Registered User mNo edit summary |
Registered User m (Undo revision 81413 by Registered User (-)) Tag: Undo |
||
(10 intermediate revisions by 2 users not shown) | |||
Line 1: | Line 1: | ||
This page aims to provide links to archived wikis. | This page aims to provide links to archived wikis. | ||
Each ecosystem release flow has its corresponding wiki. | Each STM32 MPU ecosystem release flow has its corresponding wiki. | ||
An '''ecosystem release flow''' designates all the '''ecosystem releases''' which are based on the '''same versions of the major software components''' (e.g. Linux<sup>®</sup> kernel) of the OpenSTLinux distribution (see details in the table below).<br> | An '''ecosystem release flow''' designates all the '''ecosystem releases''' which are based on the '''same versions of the major software components''' (e.g. Linux<sup>®</sup> kernel) of the OpenSTLinux distribution (see details in the table below).<br> | ||
Line 13: | Line 13: | ||
{| class="st-table" | {| class="st-table" | ||
|- | |- | ||
|style="text-align:center;" | [[File:STM32_MPU_v2_wiki_by_ST.png|center|200px|link=stm32mpuv2:Main Page]] | |||
|| STM32 MPU archived wiki for the {{Highlight|v2.''y''.''z''}} ecosystem releases | |||
|- | |||
| [[File:STM32_MPU_v1_wiki_by_ST.png|center|200px|link=stm32mpuv1:Main Page]] | | [[File:STM32_MPU_v1_wiki_by_ST.png|center|200px|link=stm32mpuv1:Main Page]] | ||
|| STM32 MPU archived wiki for the {{Highlight|v1.''y''.''z''}} ecosystem releases | || STM32 MPU archived wiki for the {{Highlight|v1.''y''.''z''}} ecosystem releases | ||
|} | |} | ||
Line 26: | Line 26: | ||
| [[Main_Page|This wiki]] | | [[Main_Page|This wiki]] | ||
| | | | ||
v3.0.0 | v3.1.0 (Nov 2021)<br> | ||
v3.0.0 (Apr 2021) | |||
| | | | ||
Linux<sup>®</sup> kernel v5.10 (LTS)<br> | Linux<sup>®</sup> kernel v5.10 (LTS)<br> | ||
Line 60: | Line 61: | ||
<noinclude> | <noinclude> | ||
[[Category:Wiki archives tab]] | [[Category:Wiki archives tab]] | ||
{{PublicationRequestId | 18177 | 2020-11-19 | {{PublicationRequestId | 18177 | 2020-11-19 }} | ||
</noinclude> | </noinclude> |
Latest revision as of 16:16, 18 July 2022
This page aims to provide links to archived wikis. Each STM32 MPU ecosystem release flow has its corresponding wiki.
An ecosystem release flow designates all the ecosystem releases which are based on the same versions of the major software components (e.g. Linux® kernel) of the OpenSTLinux distribution (see details in the table below).
Each vx flow groups together all the vx.y.z ecosystem releases, and has its own wiki.
The most recent flow is associated with this latest wiki also known as flagship wiki (whose URL is "https://wiki.st.com/stm32mpu"), while the previous flows are associated with archived wikis (whose URLs are "https://wiki.st.com/stm32mpu-ecosystem-vx").
This flagship wiki is for the v3 flow (v3.y.z ecosystem releases): if you discover the STM32 Arm® Cortex®-based MPUs, it is highly recommended to continue browsing this wiki that contains the latest major ecosystem release.
However, if you need information about any previous ecosystem releases flow, browse the associated wiki thanks to the below table:
STM32 MPU archived wiki for the v2.y.z ecosystem releases | |
STM32 MPU archived wiki for the v1.y.z ecosystem releases |
Wiki | Major ecosystem releases | Major software components (OpenSTLinux distribution) |
---|---|---|
This wiki |
v3.1.0 (Nov 2021) |
Linux® kernel v5.10 (LTS) |
Archived wiki for the v2 flow |
v2.1.0 |
Linux® kernel v5.4 (LTS) |
Archived wiki for the v1 flow |
v1.2.0 |
Linux® kernel v4.19 (LTS) |