Registered User No edit summary |
Registered User mNo edit summary |
||
(38 intermediate revisions by 7 users not shown) | |||
Line 1: | Line 1: | ||
==Open a terminal== | ==Open a terminal== | ||
Open a terminal on the host computer. | Open a terminal on the host computer. | ||
[[File: Ubuntu_terminal.png|frame|center|link=|Ubuntu terminal]] | [[File: Ubuntu_terminal.png|frame|center|link=|Ubuntu terminal]] | ||
All the commands preceded by {{PC$}} have to be executed from the host computer terminal. | All the commands preceded by {{PC$}} have to be executed from the host computer terminal. | ||
* Create your STM32MPU workspace directory on | * Create your STM32MPU workspace directory on the host computer: | ||
{{PC$}} mkdir $HOME/STM32MPU_workspace | {{PC$}} mkdir $HOME/STM32MPU_workspace | ||
{{PC$}} cd $HOME/STM32MPU_workspace | {{PC$}} cd $HOME/STM32MPU_workspace | ||
Line 10: | Line 11: | ||
* An Internet access through http and https protocols must be provided. | * An Internet access through http and https protocols must be provided. | ||
The command below | The command below enables checking for Internet access through http/https protocols: | ||
{{PC$}} wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy." | {{PC$}} wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy." | ||
If an 'OK' message is returned, the network is | If an 'OK' message is returned, the network is correctly configured.<br> | ||
In | In this case, skip the rest of this section.<br> | ||
<br> | <br> | ||
Otherwise, a proxy for http/https protocols is required.<br> | |||
The best solution to set | The best solution is to set this proxy through the shell variables http_proxy and https_proxy: | ||
{{PC$}} export http_proxy=http://''<MyProxyLogin>'':''<MyProxyPassword>''@''<MyProxyServerUrl>'':''<MyProxyPort>'' | {{PC$}} export http_proxy=http://''<MyProxyLogin>'':''<MyProxyPassword>''@''<MyProxyServerUrl>'':''<MyProxyPort>'' | ||
{{PC$}} export https_proxy=http://''<MyProxyLogin>'':''<MyProxyPassword>''@''<MyProxyServerUrl>'':''<MyProxyPort>'' | {{PC$}} export https_proxy=http://''<MyProxyLogin>'':''<MyProxyPassword>''@''<MyProxyServerUrl>'':''<MyProxyPort>'' | ||
Check again the Internet access | Check again the Internet access using the command: | ||
{{PC$}} wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy." | {{PC$}} wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy." | ||
==Install the tools== | ==Install the tools== | ||
===STM32CubeProgrammer=== | ===STM32CubeProgrammer=== | ||
* Create your STM32MPU tools directory on the host computer: | |||
* Create your STM32MPU tools directory on | |||
{{PC$}} mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools | {{PC$}} mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools | ||
{{PC$}} mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z | {{PC$}} mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z | ||
* Create a temporary directory in your STM32MPU workspace | * Create a temporary directory in your STM32MPU workspace: | ||
{{PC$}} mkdir $HOME/STM32MPU_workspace/tmp | {{PC$}} mkdir $HOME/STM32MPU_workspace/tmp | ||
* Download | * Download [https://www.st.com/en/development-tools/stm32cubeprog.html#getsoftware-scroll STM32CubeProgrammer] in the following directory<br> '''$HOME/STM32MPU_workspace/tmp''' | ||
* Uncompress the archive file to get the STM32CubeProgrammer installers | |||
STM32CubeProgrammer V2.9 recommended for {{EcosystemRelease | revision=3.1.0| range= }} | |||
STM32CubeProgrammer V2.8 recommended for {{EcosystemRelease | revision=3.0.0| range= }} | |||
* Uncompress the archive file to get the STM32CubeProgrammer installers: | |||
{{PC$}} cd $HOME/STM32MPU_workspace/tmp | {{PC$}} cd $HOME/STM32MPU_workspace/tmp | ||
{{PC$}} unzip SetupSTM32CubeProgrammer.zip | {{PC$}} unzip SetupSTM32CubeProgrammer.zip | ||
* Execute the Linux installer, which guides you through the installation process. Select "$HOME/STM32MPU-Tools/STM32CubeProgrammer-x.y.z" as | * Execute the Linux<sup>®</sup> installer, which guides you through the installation process. Select "$HOME/STM32MPU-Tools/STM32CubeProgrammer-x.y.z" as installation directory when it is requested by the installer. | ||
{{PC$}} ./SetupSTM32CubeProgrammer-x.y.z.linux | {{PC$}} ./SetupSTM32CubeProgrammer-x.y.z.linux | ||
The screenshots below have been obtained with old {{Highlight|STM32CubeProgrammer V2.7.0}}. They are provided {{Highlight| as examples}} still valid for higher version : | |||
[[File: STM32CubeProgrammer_installation_splashscreen.png|frame|center|link=|Splash screen]] | [[File: STM32CubeProgrammer_installation_splashscreen.png|frame|center|link=|Splash screen]] | ||
[[File: | [[File: STM32CubeProgrammer_installation_welcome_27.png|frame|center|link=|Welcome page]] | ||
[[File: | [[File: STM32CubeProgrammer_installation_path_25.png|frame|center|link=|Installation path]] | ||
* Add the STM32CubeProgrammer binary path to your PATH environment variable | * Add the STM32CubeProgrammer binary path to your PATH environment variable: | ||
export PATH=$HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/bin:$PATH | export PATH=$HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/bin:$PATH | ||
* Check that the STM32CubeProgrammer tool is properly installed and accessible | |||
* Go inside the binary folder: | |||
{{PC$}} cd $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/bin/ | |||
{{ReviewsComments|-- [[User:Kevin Huber|Kevin Huber]] ([[User talk:Kevin Huber|talk]]) 14:59, 13 December 2021 (CET)<br />I added this part because we are currently facing a bug if the CubeProgrammer is not launched from its binary folder. Ticket: 115167 }} | |||
* Check that the STM32CubeProgrammer tool is properly installed and accessible: | |||
{{PC$}} STM32_Programmer_CLI --h | {{PC$}} STM32_Programmer_CLI --h | ||
------------------------------------------------------------------- | ------------------------------------------------------------------- | ||
Line 55: | Line 63: | ||
===USB serial link=== | ===USB serial link=== | ||
* Install the libusb on your host computer | * Install the libusb on your host computer: | ||
{{PC$}} sudo apt-get install libusb-1.0-0 | {{PC$}} sudo apt-get install libusb-1.0-0 | ||
* To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows | * To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows: | ||
{{PC$}} cd $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/Drivers/rules | {{PC$}} cd $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/Drivers/rules | ||
{{PC$}} sudo cp *.* /etc/udev/rules.d/ | {{PC$}} sudo cp *.* /etc/udev/rules.d/ | ||
Line 65: | Line 73: | ||
{{SoftwareLicenseAgreement | distribution=OpenSTLinux}} | {{SoftwareLicenseAgreement | distribution=OpenSTLinux}} | ||
{{Warning|Only microSD cards SanDisk Class 10 and UHS Speed Class 1 are verified. Others are not recommended.}} | |||
===For {{EcosystemRelease | revision=3.1.0}}=== | |||
{{PC$}} mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0 | |||
{{PC$}} mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem- | {{PC$}} mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Starter-Package | ||
{{PC$}} mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem- | {{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Starter-Package | ||
{{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem- | * Download the [{{EcosystemRelease/Package | revision=3.1.0| package=Images package | request=url}}/{{EcosystemRelease/Package | revision=3.1.0| package=Images package | request=name}} STM32MP15-Ecosystem-v3.1.0 Starter Package] to the following directory:<br> '''$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Starter-Package''' | ||
* Download the [ | |||
* Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files | * Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files | ||
{{PC$}} tar xvf | {{PC$}} tar xvf {{EcosystemRelease/Package | revision=3.1.0| package=Images package | request=name}} | ||
<div class="mw-collapsible mw-collapsed"> | <div class="mw-collapsible mw-collapsed"> | ||
===For {{EcosystemRelease | revision=3.0.0}}=== | |||
<div class="mw-collapsible-content"> | <div class="mw-collapsible-content"> | ||
* Create your STM32MP15 Starter Package directory on | * Create your STM32MP15 Starter Package directory on the host computer: | ||
{{PC$}} mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem- | {{PC$}} mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0 | ||
{{PC$}} mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem- | {{PC$}} mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package | ||
{{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem- | {{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package | ||
* Download the [ | * Download the [{{EcosystemRelease/Package | revision=3.0.0| package=Images package | request=url}}/{{EcosystemRelease/Package | revision=3.0.0| package=Images package | request=name}} STM32MP15-Ecosystem-v3.0.0 Starter Package] to the following directory:<br> '''$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package''' | ||
* Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files | * Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files | ||
{{PC$}} tar xvf | {{PC$}} tar xvf {{EcosystemRelease/Package | revision=3.0.0| package=Images package | request=name}} | ||
</div> | |||
<noinclude> | <noinclude> | ||
{{NoIndex}} | |||
__NOTOC__ | |||
[[Category:Sub-articles]] | [[Category:Sub-articles]] | ||
{{PublicationRequestId | 19647 | 2021-04-19}} | |||
{{PublicationRequestId | | |||
</noinclude> | </noinclude> |
Latest revision as of 14:26, 28 January 2022
1. Open a terminal
Open a terminal on the host computer.

All the commands preceded by have to be executed from the host computer terminal.
- Create your STM32MPU workspace directory on the host computer:
mkdir $HOME/STM32MPU_workspace
cd $HOME/STM32MPU_workspace
2. Check the host computer Internet access
- An Internet access through http and https protocols must be provided.
The command below enables checking for Internet access through http/https protocols:
wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."
If an 'OK' message is returned, the network is correctly configured.
In this case, skip the rest of this section.
Otherwise, a proxy for http/https protocols is required.
The best solution is to set this proxy through the shell variables http_proxy and https_proxy:
export http_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>
export https_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>
Check again the Internet access using the command:
wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."
3. Install the tools
3.1. STM32CubeProgrammer
- Create your STM32MPU tools directory on the host computer:
mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools
mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z
- Create a temporary directory in your STM32MPU workspace:
mkdir $HOME/STM32MPU_workspace/tmp
- Download STM32CubeProgrammer in the following directory
$HOME/STM32MPU_workspace/tmp
STM32CubeProgrammer V2.9 recommended for ecosystem release v3.1.0
STM32CubeProgrammer V2.8 recommended for ecosystem release v3.0.0
- Uncompress the archive file to get the STM32CubeProgrammer installers:
cd $HOME/STM32MPU_workspace/tmp
unzip SetupSTM32CubeProgrammer.zip
- Execute the Linux® installer, which guides you through the installation process. Select "$HOME/STM32MPU-Tools/STM32CubeProgrammer-x.y.z" as installation directory when it is requested by the installer.
./SetupSTM32CubeProgrammer-x.y.z.linux
The screenshots below have been obtained with old STM32CubeProgrammer V2.7.0. They are provided as examples still valid for higher version :



- Add the STM32CubeProgrammer binary path to your PATH environment variable:
export PATH=$HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/bin:$PATH
- Go inside the binary folder:
cd $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/bin/
- Check that the STM32CubeProgrammer tool is properly installed and accessible:
STM32_Programmer_CLI --h
-------------------------------------------------------------------
STM32CubeProgrammer vx.y.z
-------------------------------------------------------------------
3.2. USB serial link
- Install the libusb on your host computer:
sudo apt-get install libusb-1.0-0
- To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows:
cd $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/Drivers/rules
sudo cp *.* /etc/udev/rules.d/
4. Download the image
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.
4.1. For ecosystem release v3.1.0 
mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0
mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Starter-Package
cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Starter-Package
- Download the STM32MP15-Ecosystem-v3.1.0 Starter Package to the following directory:
$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Starter-Package - Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files
tar xvf en.FLASH-stm32mp1-openstlinux-5-10-dunfell-mp1-21-11-17_tar.xz