Registered User mNo edit summary |
Registered User |
||
(11 intermediate revisions by 3 users not shown) | |||
Line 7: | Line 7: | ||
{{Warning|To use efficiently this SDK, please go through the Developer Package article relative to your STM32 microprocessor Series: [[:Category:Developer Package]]}} | {{Warning|To use efficiently this SDK, please go through the Developer Package article relative to your STM32 microprocessor Series: [[:Category:Developer Package]]}} | ||
==STM32MP15-Ecosystem- | ==STM32MP15-Ecosystem-v3.1.0 release== | ||
</noinclude> | </noinclude> | ||
* The STM32MP1 SDK is delivered through a tarball file named : ''' | * The STM32MP1 SDK is delivered through a tarball file named : '''{{EcosystemRelease/Package | revision=3.1.0 | package=SDK package | request=name}}''' | ||
<span id="Download"></span> | <span id="Download"></span> | ||
Line 16: | Line 16: | ||
{| class="st-table" | {| class="st-table" | ||
|- | |- | ||
! !!style="text-align:center;"|STM32MP1 Developer Package SDK - STM32MP15-Ecosystem- | ! !!style="text-align:center;"|STM32MP1 Developer Package SDK - STM32MP15-Ecosystem-v3.1.0 release | ||
|- | |- | ||
| Download || | | Download || | ||
You need to be logged on ''my.st.com'' before accessing the following link: <br /> | You need to be logged on ''my.st.com'' before accessing the following link: <br /> | ||
[ | [{{EcosystemRelease/Package | revision=3.1.0 | package=SDK package | request=url}}/{{EcosystemRelease/Package | revision=3.1.0 | package=SDK package | request=name}} {{EcosystemRelease/Package | revision=3.1.0 | package=SDK package | request=name}}] | ||
|- | |- | ||
| Installation || | | Installation || | ||
* Uncompress the tarball file to get the SDK installation script | * Uncompress the tarball file to get the SDK installation script | ||
$ tar xvf | {{PC$}} tar xvf {{EcosystemRelease/Package | revision=3.1.0 | package=SDK package | request=name}} | ||
* If needed, change the permissions on the SDK installation script so that it is executable | * If needed, change the permissions on the SDK installation script so that it is executable | ||
< | <div style="max-width:60em;"> | ||
$ chmod +x | {{PC$}} chmod +x {{EcosystemRelease/Package | revision=3.1.0 | package=SDK installation script | request=path}}/{{EcosystemRelease/Package | revision=3.1.0 | package=SDK installation script | request=name}} | ||
</ | </div> | ||
* Run the SDK installation script | * Run the SDK installation script | ||
** Use the ''-d <SDK installation directory absolute path>'' option to specify the absolute path to the directory in which you want to install the SDK (''<SDK installation directory>'') | ** Use the ''-d <SDK installation directory absolute path>'' option to specify the absolute path to the directory in which you want to install the SDK (''<SDK installation directory>'') | ||
** If you follow the [[Example of directory structure for Packages|proposition to organize the working directory]], it means: | ** If you follow the [[Example of directory structure for Packages|proposition to organize the working directory]], it means: | ||
< | <div style="max-width:60em;"> | ||
$ ./ | {{PC$}} ./{{EcosystemRelease/Package | revision=3.1.0 | package=SDK installation script | request=path}}/{{EcosystemRelease/Package | revision=3.1.0 | package=SDK installation script | request=name}} -d <working directory absolute path>/Developer-Package/SDK | ||
</ | </div> | ||
:* A successful installation outputs the following log: | :* A successful installation outputs the following log: | ||
<pre> | <pre style="max-width:60em;"> | ||
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version | ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17 | ||
=========================================================================================== | |||
You are about to install the SDK to "<working directory absolute path>/Developer-Package/SDK". Proceed[Y/n]? | You are about to install the SDK to "<working directory absolute path>/Developer-Package/SDK". Proceed [Y/n]? | ||
Extracting SDK.......................................................................................................done | Extracting SDK................................................................................................................................................................................................................done | ||
Setting it up...done | Setting it up...done | ||
SDK has been successfully set up and is ready to be used. | SDK has been successfully set up and is ready to be used. | ||
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. | Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. | ||
$ . | $> . <working directory absolute path>/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi | ||
</pre> | </pre> | ||
|- | |- | ||
| Release note || | | Release note || | ||
Details about the content of the SDK are available in the '''associated''' [[STM32MP15 ecosystem release note - | Details about the content of the SDK are available in the '''associated''' [[STM32MP15 ecosystem release note - v3.1.0|STM32MP15 ecosystem release note]]. | ||
[[File:Archive_box.png|25px|link=]] If you are interested in older releases, please have a look into the section [[STM32MP1_Developer_Package_-_SDK#Archives|Archives]]. | [[File:Archive_box.png|25px|link=]] If you are interested in older releases, please have a look into the section [[STM32MP1_Developer_Package_-_SDK#Archives|Archives]]. | ||
Line 57: | Line 58: | ||
* The SDK is in the ''<SDK installation directory>'': | * The SDK is in the ''<SDK installation directory>'': | ||
{{ | {{HighlightParam|<SDK installation directory>}} {{Highlight|'''SDK for OpenSTLinux distribution''': details in [[Standard SDK directory structure]] article}} | ||
├── environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi {{Highlight|'''Environment setup script''' for Developer Package}} | ├── environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi {{Highlight|'''Environment setup script''' for Developer Package}} | ||
├── site-config-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi | ├── site-config-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi | ||
Line 69: | Line 70: | ||
==Archives [[File:Archive_box.png|25px|link=]]== | ==Archives [[File:Archive_box.png|25px|link=]]== | ||
{{EcosystemFlow/Archives}} | |||
<div class="mw-collapsible mw-collapsed"> | <div class="mw-collapsible mw-collapsed"> | ||
===STM32MP15-Ecosystem- | ===STM32MP15-Ecosystem-v3.0.0 release=== | ||
<div class="mw-collapsible-content"> | <div class="mw-collapsible-content"> | ||
* The STM32MP1 SDK is delivered through a tarball file named : ''' | * The STM32MP1 SDK is delivered through a tarball file named : '''{{EcosystemRelease/Package | revision=3.0.0 | package=SDK package | request=name}}''' | ||
* Download and install the STM32MP1 SDK. | * Download and install the STM32MP1 SDK. | ||
{{SoftwareLicenseAgreement | distribution=OpenSTLinux}} | |||
{| class="st-table" | {| class="st-table" | ||
|- | |- | ||
! !!style="text-align:center;"|STM32MP1 Developer Package SDK - STM32MP15-Ecosystem- | ! !!style="text-align:center;"|STM32MP1 Developer Package SDK - STM32MP15-Ecosystem-v3.0.0 release | ||
|- | |- | ||
| Download || | | Download || | ||
You need to be logged on ''my.st.com'' before accessing the following link: <br /> | You need to be logged on ''my.st.com'' before accessing the following link: <br /> | ||
[ | [{{EcosystemRelease/Package | revision=3.0.0 | package=SDK package | request=url}}/{{EcosystemRelease/Package | revision=3.0.0 | package=SDK package | request=name}} {{EcosystemRelease/Package | revision=3.0.0 | package=SDK package | request=name}}] | ||
|- | |- | ||
| Installation || | | Installation || | ||
* Uncompress the tarball file to get the SDK installation script | * Uncompress the tarball file to get the SDK installation script | ||
$ tar xvf | {{PC$}} tar xvf {{EcosystemRelease/Package | revision=3.0.0 | package=SDK package | request=name}} | ||
* If needed, change the permissions on the SDK installation script so that it is executable | * If needed, change the permissions on the SDK installation script so that it is executable | ||
< | <div style="max-width:60em;"> | ||
$ chmod +x | {{PC$}} chmod +x {{EcosystemRelease/Package | revision=3.0.0 | package=SDK installation script | request=path}}/{{EcosystemRelease/Package | revision=3.0.0 | package=SDK installation script | request=name}} | ||
</ | </div> | ||
* Run the SDK installation script | * Run the SDK installation script | ||
** Use the ''-d <SDK installation directory absolute path>'' option to specify the absolute path to the directory in which you want to install the SDK (''<SDK installation directory>'') | ** Use the ''-d <SDK installation directory absolute path>'' option to specify the absolute path to the directory in which you want to install the SDK (''<SDK installation directory>'') | ||
** If you follow the [[Example of directory structure for Packages|proposition to organize the working directory]], it means: | ** If you follow the [[Example of directory structure for Packages|proposition to organize the working directory]], it means: | ||
< | <div style="max-width:60em;"> | ||
$ ./ | {{PC$}} ./{{EcosystemRelease/Package | revision=3.0.0 | package=SDK installation script | request=path}}/{{EcosystemRelease/Package | revision=3.0.0 | package=SDK installation script | request=name}} -d <working directory absolute path>/Developer-Package/SDK | ||
</ | </div> | ||
:* A successful installation outputs the following log: | :* A successful installation outputs the following log: | ||
<pre> | <pre style="max-width:60em;"> | ||
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version | ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 3.1-openstlinux-5.10-dunfell-mp1-21-03-31 | ||
=========================================================================================== | |||
You are about to install the SDK to "<working directory absolute path>/Developer-Package/SDK". Proceed[Y/n]? | You are about to install the SDK to "<working directory absolute path>/Developer-Package/SDK". Proceed [Y/n]? | ||
Extracting SDK.......................................................................................................done | Extracting SDK................................................................................................................................................................................................................done | ||
Setting it up...done | Setting it up...done | ||
SDK has been successfully set up and is ready to be used. | SDK has been successfully set up and is ready to be used. | ||
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. | Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. | ||
$ . | $> . <working directory absolute path>/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi | ||
</pre> | </pre> | ||
|- | |- | ||
| Release note || | | Release note || | ||
Details about the content of the SDK are available in the '''associated''' [[STM32MP15 ecosystem release note - | Details about the content of the SDK are available in the '''associated''' [[STM32MP15 ecosystem release note - v3.0.0|STM32MP15 ecosystem release note]]. | ||
[[File:Archive_box.png|25px|link=]] If you are interested in older releases, please have a look into the section [[STM32MP1_Developer_Package_-_SDK#Archives|Archives]]. | [[File:Archive_box.png|25px|link=]] If you are interested in older releases, please have a look into the section [[STM32MP1_Developer_Package_-_SDK#Archives|Archives]]. | ||
Line 121: | Line 124: | ||
* The SDK is in the ''<SDK installation directory>'': | * The SDK is in the ''<SDK installation directory>'': | ||
{{ | {{HighlightParam|<SDK installation directory>}} {{Highlight|'''SDK for OpenSTLinux distribution''': details in [[Standard SDK directory structure]] article}} | ||
├── environment-setup-cortexa7t2hf-neon-vfpv4- | ├── environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi {{Highlight|'''Environment setup script''' for Developer Package}} | ||
├── site-config-cortexa7t2hf-neon-vfpv4- | ├── site-config-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi | ||
├── {{Green|sysroots}} | ├── {{Green|sysroots}} | ||
│ ├── {{Green|cortexa7t2hf-neon-vfpv4- | │ ├── {{Green|cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi}} {{Highlight|Target sysroot (libraries, headers, and symbols)}} | ||
│ │ └── [...] | │ │ └── [...] | ||
│ └── {{Green|x86_64- | │ └── {{Green|x86_64-ostl_sdk-linux}} {{Highlight|Native sysroot (libraries, headers, and symbols)}} | ||
│ └── [...] | │ └── [...] | ||
└── version-cortexa7t2hf-neon-vfpv4- | └── version-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi | ||
</div></div> | </div></div> | ||
{{NoIndex}} | {{NoIndex}} | ||
[[Category:Sub-articles]] | [[Category:Sub-articles]] |
Latest revision as of 12:01, 15 November 2021
This article aims to give the following information:
- How to download and install the latest SDK for the STM32 microprocessor Series
- Where to find the associated release note
- Where to find the previous releases (archives)
1. STM32MP15-Ecosystem-v3.1.0 release
- The STM32MP1 SDK is delivered through a tarball file named : en.SDK-x86_64-stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17.tar.xz
- Download and install the STM32MP1 SDK.
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.
STM32MP1 Developer Package SDK - STM32MP15-Ecosystem-v3.1.0 release | |
---|---|
Download |
You need to be logged on my.st.com before accessing the following link: |
Installation |
tar xvf en.SDK-x86_64-stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17.tar.xz
chmod +x stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.sh
./stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.sh -d <working directory absolute path>/Developer-Package/SDK
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17
===========================================================================================
You are about to install the SDK to "<working directory absolute path>/Developer-Package/SDK". Proceed [Y/n]?
Extracting SDK................................................................................................................................................................................................................done
Setting it up...done
SDK has been successfully set up and is ready to be used.
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g.
$> . <working directory absolute path>/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
|
Release note |
Details about the content of the SDK are available in the associated STM32MP15 ecosystem release note.
|
- The SDK is in the <SDK installation directory>:
<SDK installation directory> SDK for OpenSTLinux distribution: details in Standard SDK directory structure article ├── environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi Environment setup script for Developer Package ├── site-config-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi ├── sysroots │ ├── cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi Target sysroot (libraries, headers, and symbols) │ │ └── [...] │ └── x86_64-ostl_sdk-linux Native sysroot (libraries, headers, and symbols) │ └── [...] └── version-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
2. Archives 
This wiki is for the v3 ecosystem releases. For information about the previous ecosystem releases, go through the Wiki archives.
2.1. STM32MP15-Ecosystem-v3.0.0 release