This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User mNo edit summary |
||
(11 intermediate revisions by 3 users not shown) | |||
Line 1: | Line 1: | ||
This module guides you | |||
The STM32MP1 Developer Package contains (for the | This module guides you through installing the STM32MP1 Developer Package to develop on Arm<sup>®</sup> Cortex<sup>®</sup>-A7.<br> | ||
{{Info|To complete this module, it is assumed a Linux PC running Ubuntu | The STM32MP1 Developer Package contains (for the Arm<sup>®</sup> Cortex<sup>®</sup>-A7) the Software Development Kit (SDK) that allows you to cross compile your own application or to rebuild the Linux<sup>®</sup> for the Arm<sup>®</sup> Cortex<sup>®</sup>-A7 kernel. | ||
{{Info|To complete this module, it is assumed a Linux PC running under Ubuntu 20.04 is used. | |||
Refer to [[PC_prerequisites]] }} | |||
<noinclude> | <noinclude> | ||
{{NoIndex}} | {{NoIndex}} | ||
[[Category:Sub-articles]] | [[Category:Sub-articles]] | ||
{{PublicationRequestId | | {{PublicationRequestId | 19652 |2021-04-19}} | ||
</noinclude> | </noinclude> |
Latest revision as of 18:32, 10 November 2021
This module guides you through installing the STM32MP1 Developer Package to develop on Arm® Cortex®-A7.
The STM32MP1 Developer Package contains (for the Arm® Cortex®-A7) the Software Development Kit (SDK) that allows you to cross compile your own application or to rebuild the Linux® for the Arm® Cortex®-A7 kernel.