This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User mNo edit summary |
||
(4 intermediate revisions by the same user not shown) | |||
Line 1: | Line 1: | ||
<noinclude> | <noinclude> | ||
This article explains how to assemble the '''STM32MP157x-DKx''' Discovery kits. It is valid for the {{Board | type=157A-DK1 | name=short}}, {{Board | type=157D-DK1 | name=short}}, {{Board | type=157C-DK2 | name=short}} and {{Board | type=157F-DK2 | name=short}} Discovery kits: the part numbers are specified in the [[STM32MP15 microprocessor#Part number codification|STM32MP15 microprocessor part numbers]] article. | |||
This article explains how to assemble the '''STM32MP157x-DKx''' Discovery kits. It is valid | |||
{{Warning|To successfully start the board, it is recommended to go through the corresponding Starter Package article: [[:Category:Starter Package]]}} | {{Warning|To successfully start the board, it is recommended to go through the corresponding Starter Package article: [[:Category:Starter Package]]}} | ||
</noinclude> | </noinclude> | ||
The STM32MP157x-DKx Discovery kits packages ( | The STM32MP157x-DKx Discovery kits packages ({{Board | type=157A-DK1 | name=short}}, {{Board | type=157D-DK1 | name=short}}, {{Board | type=157C-DK2 | name=short}} and {{Board | type=157F-DK2 | name=short}}) are delivered assembled, and contain the items listed below. A USB Type-C<sup>™</sup> cable is also included. | ||
Please note that; | Please note that; | ||
* the ''' | * the '''{{Board | type=157A-DK1 | name=short}}''' and '''{{Board | type=157D-DK1 | name=short}}''' Discovery kits neither include the "WLAN + Bluetooth" component (muRata LBEE5KL1DX), nor the MB1407 daughterboard DSI display | ||
* the ''' | * the '''{{Board | type=157C-DK2 | name=short}}''' and '''{{Board | type=157F-DK2 | name=short}}''' Discovery kits include the "WLAN + Bluetooth" component (muRata LBEE5KL1DX), and the MB1407 daughterboard DSI display | ||
{| | {| | ||
Line 16: | Line 14: | ||
! Position !! Description | ! Position !! Description | ||
|- | |- | ||
| 1 || [[MB1272]] motherboard ("WLAN + Bluetooth" component included only for the ''' | | 1 || [[MB1272]] motherboard ("WLAN + Bluetooth" component included only for the '''{{Board | type=157C-DK2 | name=short}}''' and '''{{Board | type=157F-DK2 | name=short}}''' Discovery kits) | ||
|- | |- | ||
| 2 || [[MB1407]] daughterboard DSI display (480x800 pixels): only for the ''' | | 2 || [[MB1407]] daughterboard DSI display (480x800 pixels): only for the '''{{Board | type=157C-DK2 | name=short}}''' and '''{{Board | type=157F-DK2 | name=short}}''' Discovery kits | ||
|- | |- | ||
| 3 || microSD card | | 3 || microSD card | ||
|} | |} | ||
<br clear=all> | <br clear=all> | ||
[[File: STM32MP157x-DKx_assembled.png | thumb | upright=4 | center | link= | STM32MP157x-DKx Discovery kit assembled <br> '''STM32MP157C-DK2''' shown here (picture not contractual) < | [[File: STM32MP157x-DKx_assembled.png | thumb | upright=4 | center | link= | STM32MP157x-DKx Discovery kit assembled <br> '''STM32MP157C-DK2''' Discovery kit shown here (picture not contractual)]] | ||
<noinclude> | |||
{{NoIndex}} | |||
[[Category:Sub-articles]] | |||
{{PublicationRequestId | 8427 | 2018-08-07 | AnneJ}} | |||
</noinclude> |
Latest revision as of 14:39, 13 May 2020
This article explains how to assemble the STM32MP157x-DKx Discovery kits. It is valid for the STM32MP157A-DK1 , STM32MP157D-DK1
, STM32MP157C-DK2
and STM32MP157F-DK2
Discovery kits: the part numbers are specified in the STM32MP15 microprocessor part numbers article.
The STM32MP157x-DKx Discovery kits packages (STM32MP157A-DK1 , STM32MP157D-DK1
, STM32MP157C-DK2
and STM32MP157F-DK2
) are delivered assembled, and contain the items listed below. A USB Type-C™ cable is also included.
Please note that;
- the STM32MP157A-DK1
and STM32MP157D-DK1
Discovery kits neither include the "WLAN + Bluetooth" component (muRata LBEE5KL1DX), nor the MB1407 daughterboard DSI display
- the STM32MP157C-DK2
and STM32MP157F-DK2
Discovery kits include the "WLAN + Bluetooth" component (muRata LBEE5KL1DX), and the MB1407 daughterboard DSI display
Position | Description |
---|---|
1 | MB1272 motherboard ("WLAN + Bluetooth" component included only for the STM32MP157C-DK2 ![]() ![]() |
2 | MB1407 daughterboard DSI display (480x800 pixels): only for the STM32MP157C-DK2 ![]() ![]() |
3 | microSD card |