Last edited 3 years ago

Install STM32CubeMP1 package: Difference between revisions


Revision as of 10:59, 7 October 2019

1. Overview[edit source]

This stage explains how to install the STM32Cube MP1 Package.

2. Install STM32Cube MP1 package[edit source]

  • Download STM32CubeMP1 Package v1.0.0 to the following directory:
    $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package
  • Uncompress the archive file to get the STM32CubeMP1 Package
 unzip en.stm32cubemp1_v1-0-0.zip

3. STM32Cube MP1 package structure[edit source]

The STM32Cube MP1 Package is located in your $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package directory and is named STM32Cube_FW_MP1_V1.0.0:

STM32Cube_FW_MP1_V1.0.0
├── Drivers
│   ├── BSP                          BSP drivers for the supported STM32MP1 boards
│   │   └── [...]
│   ├── CMSIS
│   │   └── [...]
│   └── STM32MP1xx_HAL_Driver        HAL drivers for the supported STM32MP1 devices
│       └── [...]
├── _htmresc
│   └── [...]
├── License.md
├── Middlewares
│   └── [...]
├── package.xml
├── Projects
│   ├── STM32CubeProjectsList.html   List of examples and applications for STM32CubeMP1 Package
│   ├── STM32MP157C-DK2              Set of examples and applications → STM32MP15 Discovery kits
│   │   └── [...]
│   └── STM32MP157C-EV1              Set of examples and applications → STM32MP15 Evaluation boards
│       └── [...]
├── Readme.md
├── Release_Notes.html               Release note for STM32CubeMP1 Package
└── Utilities
    └── [...]