This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User mNo edit summary |
||
Line 1: | Line 1: | ||
<noinclude> | <noinclude> | ||
{{ArticleApprovedVersion | Jean-ChristopheT | BernardP, GeraldB | No previous approved version | AnneJ - 08Aug'18 - 8428 | 09Aug'18}} | {{ArticleApprovedVersion | Jean-ChristopheT | BernardP, GeraldB | No previous approved version | AnneJ - 08Aug'18 - 8428 | 09Aug'18}} | ||
[[Category:Sub-articles]] | [[Category:Sub-articles]] | ||
This article presents the recommended connections to start with the '''STM32MP157x-DKx''' Discovery kits. It is valid both for the STM32MP157A-DK1 and STM32MP157C-DK2 Discovery kits: the part numbers are specified in the [[STM32MP15 microprocessor#Part number codification|STM32MP15 microprocessor part numbers]] article. | |||
This article presents the recommended connections to start with the ''' | |||
{{Warning|To successfully start the board, it is recommended to go through the corresponding Starter Package article: [[:Category:Starter Package]]}} | {{Warning|To successfully start the board, it is recommended to go through the corresponding Starter Package article: [[:Category:Starter Package]]}} | ||
</noinclude> | </noinclude> | ||
{{ | {{ | ||
ImageMap|Image: | ImageMap|Image:STM32MP157x-DKx_connections.png {{!}} thumb {{!}} 800px {{!}} center{{!}} STM32MP157x-DKx Discovery kit connections <br/> '''STM32MP157C-DK2''' shown here without the MB1407 daughterboard DSI display to avoid hiding the connections (picture is not contractual) | ||
circle | circle 278 325 39 [[#MB1272 | MB1272 motherboard: STM32MP157x 12x12, PMIC, DDR3]] | ||
rect | rect 194 357 239 400 [[#microSD | MicroSD card slot]] | ||
rect | rect 551 288 783 348 [[#USB Type-A | 2 x USB Type-A (host) → mouse, keyboard or USB driver]] | ||
rect | rect 551 355 783 413 [[#USB Type-A | 2 x USB Type-A (host) → mouse, Keyboard or USB driver]] | ||
rect | rect 493 519 543 648 [[#USB micro-B | USB micro-B (ST-LINK/V2-1) → PC virtual COM port and debug]] | ||
rect | rect 380 519 419 581 [[#Reset button | Reset button]] | ||
rect | rect 105 463 304 525 [[#Ethernet | Ethernet → Network]] | ||
rect | rect 124 411 277 450 [[#USB power | USB Type-C (power 5V-3A)]] | ||
}} | }} |
Revision as of 18:07, 6 March 2019
Template:ArticleApprovedVersion This article presents the recommended connections to start with the STM32MP157x-DKx Discovery kits. It is valid both for the STM32MP157A-DK1 and STM32MP157C-DK2 Discovery kits: the part numbers are specified in the STM32MP15 microprocessor part numbers article. Template:Warning