Last edited 2 years ago

ReviewsComments

1. Usage

The ReviewsComments template is used to store, in a page, a comment about the content (mainly, but not only, within the scope of the review process): question, disagreement, request for improvement etc. It should be added just before the line that is the object of the comment.

It puts a message box with a "pink notepad" icon in the page.

Only logged-in users who have writing permissions, can see this box. However, do not put any confidential information in the parameters of this template.

Usage:  {{ReviewsComments | <comment>}}

Where <comment> is the mandatory comment message. It is recommended that reviewers sign their comment

  • either with their MediaWiki signature plus timestamp thanks to the ~~~~ markup (replaced when saving),
  • or with their name's trigram and the week number (e.g. JCT w920 -) in the comment message.

A custom button in the Wikitext editor toolbar allows to insert a review comment (with the MediaWiki signature):

Review comment button

2. Basic examples

You type You get
Comment and MediaWiki signature supplied
{{ReviewsComments | ~~~~ - The proposed command doesn't work: please propose another version}}
Comment and trigram supplied
{{ReviewsComments | JCT w920 - The proposed command doesn't work: please propose another version}}

3. More examples

You type You get
No comment supplied, no signature supplied
{{ReviewsComments}}
No comment supplied, signature supplied
{{ReviewsComments | JCT w920 -}}
Comment supplied with a long sentence, signature supplied
{{ReviewsComments | JCT w920 - The comment is a long sentence. Lorem ipsum: isdem diebus Apollinaris Domitiani gener, paulo ante agens palatii Caesaris curam, ad Mesopotamiam missus a socero per militares numeros immodice scrutabatur, an quaedam altiora meditantis iam Galli.}}
Check that the spaces before and after the message
BEFORE{{ReviewsComments | Check spaces}}AFTER<br>
BEFORE
{{ReviewsComments | Check spaces}}
AFTER

BEFOREAFTER
BEFORE

AFTER

4. Maintenance

This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.

5. Code

No categories assignedEdit