This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage[edit source]
The Board template is used to indicate for which board(s), an article part (chapter, paragraph, table...) is valid. Per default (i.e. if this template is not used), any part of an article is valid for all boards for which the entire article is valid.
It outputs a "standardized" string that might be used to name an article part.
<type>}}Usage: {{Board | type=
- Where:
- <type> is the mandatory identifier of the board type. The possible values are (see also the part number codification for the STM32MP15 MPUs):
- 157A-EV1: STM32MP157A-EV1 Evaluation board
- 157C-EV1: STM32MP157C-EV1 Evaluation board
- 157x-EV1: any of the previous two
- 157A-DK1: STM32MP157A-DK1 Discovery kit
- 157C-DK2: STM32MP157C-DK2 Discovery kit
- 157x-DKx: any of the previous two
Clicking on the icon displays the article about the board (e.g. STM32MP157X-DKX - hardware description).
2. Basic examples[edit source]
You type | You get |
---|---|
STM32MP157C-EV1 Evaluation board
{{Board | type=157C-EV1}}
|
|
STM32MP157C-DK2 Discovery kit
{{Board | type=157C-DK2}}
|
3. More examples[edit source]
4. Code[edit source]
STM32MP unknown board type identifier