Last edited 4 years ago

How to create your own machine

Template:ArticleMainWriter Template:ArticleApprovedVersion


1 Introduction[edit source]

For your own needs, you can add in the Yocto project a new machine reflecting your own board and your own features.
This article is reserved to Yocto experts or at least guys who have already practiced with the Yocto environmment.

This section describes how to add and configure machine that is similar to those that the OpenSTLinux Distribution Package already supports.
This customer machine is associated to STM32CubeMX tool which provides DeviceTree files per component (tf-a, u-boot and kernel).

We suppose here that all the stuff described below is done inside an existing STM32MP BSP layer 'addons'.
For reminder this addons layer is deployed here in our delivery : <path of OpenSTLinux distribution delivery>/meta-st/meta-st-stm32mp-addons/

2 Generate devicetree[edit source]

The principle is that the user generates devicetree files from the STM32CubeMX tool.
With the STM32CubeMX tool, the user browses inside the OpenSTLinux distribution file system until “mx” folder located into STM32MP BSP layer addons : <path of OpenSTLinux distribution delivery>/meta-st/meta-st-stm32mp-addons/mx/

  • 3 sub-folders are created and populated with generated devicetree files :
    • <ProjectName>/kernel
    • <ProjectName>/u-boot
    • <ProjectName>/tf-a

Where <ProjectName> is the “STM32CubeMX user project name”

Each directory of <ProjectName> contains devicetree files associated to the component directory, here: kernel, u-boot and tf-a (Trusted Firmware-A).
Please refer to these pages for more details on this tool and its usage :


3 Create a custom machine[edit source]

Create a machine based on the one provided by ST and align some environment variables with the content of mx/<ProjectName> sub-folders

3.1 Create the new machine[edit source]

  $> cd <path of OpenSTLinux distribution delivery>/meta-st/meta-st-stm32mp-addons/conf/machine
  $> cp stm32mp1-mx.conf stm32mp1-<ProjectName>.conf

3.2 Edit the new machine file: stm32mp1-<ProjectName>.conf[edit source]

 # Assign CubeMX Board DT and project name
 CUBEMX_DTB = "stm32mp157c-<ProjectName>-mx"
 CUBEMX_PROJECT = "<ProjectName>"

CUBEMX_PROJECT is the path of the directory in which the machine must find the package directory, here 'MyProjectName' for a path corresponding to mx/MyProjectName.

4 Miscellaneous[edit source]

4.1 MACHINEOVERRIDES regular expression[edit source]

In each customer machine we retrieve this line:

MACHINEOVERRIDES .= ":stm32mpcommonmx"

A regular expression that resolves to one or more target machines with which a recipe is compatible.


The impact in the build environment is that recipes can now do things conditionally only on the builds for all mx specific machines: stm32mpcommonmx
It is very useful in some existing recipes to keep the compatibility for all stm32mp1-<ProjectName>.conf machines.
For instance use it like this (as it is done in the recipe <path of OpenSTLinux distribution delivery>/meta-st/meta-st-stm32mp-addons/recipes-bsp/alsa/alsa-state-stm32mp1.bbappend):

SRC_URI_append_stm32mpcommonmx

The append will be applied for all machines (all stm32mp1-<ProjectName>.conf) which include MACHINEOVERRIDES .= ":stm32mpcommonmx"

So it avoids to create an append file by customer machine.

4.2 STM32CubeMX class[edit source]

A dedicated class is provided here :

<STM32MP BSP layer addons>/classes/cubemx-stm32mp.bbclass

The main goal of this class is to manage any change done by the customer in sub folders mx/<ProjectName>/...

So if a devicetree file is updated for one or more of components, this change will be taken into account automatically during the next compilation done in the Distribution Package.

5 Compile your image with the yocto build process[edit source]

 $> cd <path of yocto delivery>
 (directory which contains meta-st, openembedded-core, meta-openembedded)
$> MACHINE=stm32mp1-<ProjectName> DISTRO=openstlinux-weston source meta-st/script/envsetup.sh Accept the term of EULA (if you agree with)
$> bitbake st-image-weston The generated images are available on build-openstlinuxweston-stm32mp1-<ProjectName>/tmp-glibc/deploy/images/stm32mp1-<ProjectName>