Modify, rebuild and reload a firmware

Revision as of 18:48, 13 February 2020 by Registered User

1. Overview[edit source]

This stage explains how to modify, rebuild and reload a STM32MP1 Arm® Cortex®-M4 coprocessor firmware.

It proposes to customize the STM32MP1 Cube Package application example OpenAMP_TTY_Echo using STM32CubeIDE.

2. Disconnect the minicom console[edit source]

  • If minicom is already opened, please disconnect it to use the STM32CubeIDE built in serial console.
 Ctrl + A then Q

3. Open STM32CubeIDE[edit source]

  • Start STM32CubeIDE
STM32CubeIDE Starter Screen
  • Choose a workspace ( default is fine)
  • Notice information provided in the Information Center page and close it. ( you can open it later on)
STM32CubeIDE Information Center Page
  • You come into your workspace projet view
STM32CubeIDE Project View

4. Check connection to Serial Console[edit source]

  • STM32CubeIDE require to be connected to Linux running on MP1 though serial connection

This connexion is automatically detected and configured since you have put cable on ST-Link port and board has booted.

  • You can check you can get linux log and prompt by clicking on the STM32 butterfly button :
STM32CubeIDE Serial Console button
  • Connection is ok if Linux log or prompt are displayed in the console windows.
STM32CubeIDE Linux Prompt

5. Import an existing example in STM32CubeIDE[edit source]

  • Open the import screen File > Import... and select Existing Project into Workspace
STM32CubeIDE import screen
  • Browse and select OpenAMP_TTY_echo application example :

$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Developer-Package/STM32Cube_FW_MP1_V1.2.0/Projects/{{{board_type}}}/Applications/OpenAMP/OpenAMP_TTY_echo/STM32CubeIDE /* For ecosystem release v1.2.0 More info.png */$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.1.0/Developer-Package/STM32Cube_FW_MP1_V1.1.0/Projects/{{{board_type}}}/Applications/OpenAMP/OpenAMP_TTY_echo/SW4STM32 /* For ecosystem release v1.1.0 More info.png */ $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/{{{board_type}}}/Applications/OpenAMP/OpenAMP_TTY_echo/SW4STM32 /* For ecosystem release v1.0.0 More info.png */

  • STM32CubeIDE brings a new project structure for dual core chip such as STM32MP1. A top level project contain sub-projects for each core.
  • Here OpenAMP_TTY_echo top project contains OpenAMP_TTY_echo_CM4 sub project. Keep the 2 projects selected and click on "finish".
STM32CubeIDE project selection
  • The OpenAMP_TTY_echo project is open and you can browse inside using the left pan
OpenAMP_TTY_echo project structure

6. Build the firmware[edit source]

  • Select project OpenAMP_TTY_Echo_CM4 and click the build button (the little hammer in the toolbar)
STM32CubeIDE build the project
  • Build is finished with no error
STM32CubeIDE build finished with no error

7. Start Debug Session[edit source]

Your board might be connected to the PC by ethernet, either using RJ45 (point to point or VLAN) or USB0 EthernetOverUSB gadget ( point to point connection with PC with TypeA-TypeC cable). Screenshot below use the second solution. STM32CubeIDE should automatically detect the board Inet address and display it in the Serial Target widget status window in bottom right part of the screen.

STM32Cube Serial Target widget status


  • Select your OpenAMP_TTY_echo_CM4 project
  • Right click on Debug As > Debug configurations... to open the Debug Configurations panel
  • If not already created, create your debug configuration by double clicking on STM32 Cortex-M C/C++ Application and open "Debugger" pane.
Select Production mode in Startup pane of Debug Configuration
  • Check IP addess is correctly filled (1). Else you can force detection using button on the right (2).
  • Make sure the "Thru Linux core (production mode)" is selected (3)
  • When configuration is ok, the "Debug" button (5) turn to active and you can launch the debug session. Else error message appears in area (4).
The debug in production mode' adds the cortex-M firmware transfer to the embedded Linux. This means also in case of network usage some specific pop-up appearing: 
  • the SSH Password is to complete: the default one is root.
SSH password popup
  • the RSA key is to be approved.
RSA key popup

After, download of the firmware SW4STM32 will start it and switch into Debug Perspective. You can then use all features of the debugger.

For further information and support on new MPU feature in SW4STM32, refer to Help menu of SW4STM32 "Micro Processor Unit (MPU) Family - MCU support "

8. Test the firmware[edit source]

The OpenAMP_TTY_echo firmware do the following:

  • CPU2(CM4) initialize OpenAMP MW which initializes/configures IPCC peripheral through HAL and setup openamp-rpmsg framework infrastructure
  • CPU2(CM4) creates 2 rpmsg channels for 2 virtual UART instances UART0 and UART1
  • CPU2(CM4) is waiting for messages from CPU1(CA7) on these both channels
  • When CPU2(CM4) receives a message on 1 Virtual UART instance/rpmsg channel, it sends the message back to CPU1(CA7) on the same Virtual UART instance

If you have used SW4STM32 to load and start the firmware you should reopen the serial console.

  • Initialize the ttyRPMSG0 configuration
 stty -onlcr -echo -F /dev/ttyRPMSG0
  • Read constantly the ttyRPMSG0 channel in background
 cat /dev/ttyRPMSG0 &
  • Send a message on one ttyRPMSG0 channel and recieve the echo on the same ttyRPMSG0 channel
 echo "Hello Virtual UART0" > /dev/ttyRPMSG0
Hello Virtual UART0
  • You can perform the same steps with the ttyRPMSG1 channel


  • After playing a while you can stop the firmware
 echo stop > /sys/class/remoteproc/remoteproc0/state
  • And terminate the SW4STM32 debug session

9. Modify the firmware[edit source]

The original firmware example receives a message for the host on one channel end sent back the same message to the host on the same channel.
As this is not so obvious on which channel the message is received, we propose to modify the firmware in order to add an indication to know what is the channel that is receiving the message.
Please modify main.c original code as follow:

File:SW4STM32 workspace project modification.png
SW4STM32 main.c file modification
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {

    OPENAMP_check_for_message();

    /* USER CODE END WHILE */
    if (VirtUart0RxMsg) {
      char msg_to_transmit[MAX_BUFFER_SIZE];
      int msg_size = 0;
      VirtUart0RxMsg = RESET;

      msg_size = snprintf(msg_to_transmit, MAX_BUFFER_SIZE, "Channel RPMSG0: ");
      msg_size += snprintf(msg_to_transmit + msg_size, MAX_BUFFER_SIZE, "%s\n", VirtUart0ChannelBuffRx);
      log_info("size of the message to transmit = %d bytes\n", msg_size);
      VIRT_UART_Transmit(&huart0, (uint8_t*)msg_to_transmit, msg_size);
    }

    if (VirtUart1RxMsg) {
      char msg_to_transmit[MAX_BUFFER_SIZE];
      uint16_t msg_size = 0;
      VirtUart1RxMsg = RESET;

      msg_size = snprintf(msg_to_transmit, MAX_BUFFER_SIZE, "Channel RPMSG1: ");
      msg_size += snprintf(msg_to_transmit + msg_size, MAX_BUFFER_SIZE, "%s\n", VirtUart1ChannelBuffRx);
      log_info("size of the message to transmit = %d bytes\n", msg_size);
      VIRT_UART_Transmit(&huart1, (uint8_t*)msg_to_transmit, msg_size);
    }
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
  • Save your modifications

10. Rebuild, reload and test the modified firmware[edit source]

10.1. Rebuild[edit source]

  • Click the build button (the little hammer in the toolbar)
  • Wait the end of the build

10.2. Reload and start[edit source]

Just relaunch the debug session but reply "No" to following popup in order to force load of the updated firmware.

File:Force Load of the updated binary.png
Force Load of the updated firmware

10.3. Test[edit source]

  • Initialize the ttyRPMSG0 and ttyRPMSG1 configurations
 stty -onlcr -echo -F /dev/ttyRPMSG0
 stty -onlcr -echo -F /dev/ttyRPMSG1
  • Read constantly the ttyRPMSG0 and ttyRPMSG1 channels in background
 cat /dev/ttyRPMSG0 &
 cat /dev/ttyRPMSG1 &
  • Send a message on one ttyRPMSG0 channel and check the echo log
 echo "Hello Virtual UART0" > /dev/ttyRPMSG0
Channel RPMSG0: Hello Virtual UART0
  • Send a message on one ttyRPMSG1 channel and check the echo log
 echo "Hello Virtual UART1" > /dev/ttyRPMSG1
Channel RPMSG1: Hello Virtual UART1


Info white.png Information
When the firmware is running, you can output log from the firmware by using the following command:
cat /sys/kernel/debug/remoteproc/remoteproc0/trace0


  • After playing a while you can stop the firmware
 echo stop > /sys/class/remoteproc/remoteproc0/state
  • And terminate the SW4STM32 debug session