This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage
The Green template is used to color text in pages, with the "classic orange" (█) color.
Usage: {{Orange|<text to color>}}
Where <text to color> is the text to format in orange. If this template is called with no text, the hexadecimal code of the color is returned.
2. Basic examples
You type | You get |
---|---|
Coloring text in "classic" orange
This is a {{Orange|"classic" color: orange: █}} |
This is a Classic color: orange: █ |
Getting the hexadecimal code of the color
{{Orange}} is the hexadecimal code of the "classic" orange. |
#FFA500 is the hexadecimal code of the "classic" orange. |
3. More examples
You type | You get |
---|---|
Orange and bold
This is a {{Orange|'''"classic"'''}} color: '''{{Orange|orange: █}}''' |
This is a "classic" color: orange █ |
Orange and italic
This is a {{Orange|''"classic"''}} color: ''{{Orange|orange: █}}'' |
This is a "classic" color: orange: █ |
4. Code
#FFA500