This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage[edit source]
This template is used to indicate the source of any file used in this user guide.
It takes as first input parameter a string that identifies the source of the file. The possible values are:
- "Digital Assets Library": the file source is in STMicroelectronics Digital Assets Library (intranet - restricted access). Then, the second input parameter is the number of the document in this Library
- {{FileSource | Digital Assets Library | 7331}}
- "User guide": the file source is in STMicroelectronics user guide files library (intranet - restricted access). Then, the second parameter is the relative path of the file source from the user guide files library root directory
- {{FileSource | User guide | Boards/STM32MP157X-DKX.ppt}}
- "Training": the file source is in STMicroelectronics training files library (intranet - restricted access). Then, the second parameter is the relative path of the file source from the training files library root directory
- {{FileSource | Training | STM32MP15-Software-%20Software%20architecture.pptx}}
- "UML diagram": the file source is in STMicroelectronics UML diagrams' Git repository (intranet - restricted access). Then, the second parameter is the relative path of the UML diagram from the UML diagrams' Git repository root directory
- {{FileSource | UML diagram | timers/quadrature_x4_encoding.txt}}
- "Internet": the file source is Internet. Then, the second parameter is the URL of the file source. Optionally, a third parameter gives a link text.
- {{FileSource | Internet | http://www.openembedded.org/}}
- {{FileSource | Internet | http://www.openembedded.org/ | OpenEmbedded}}
- "NA": the file is self-contained (to modify the file, it is enough to download it). "NA" means "not applicable". Optionally, a second parameter gives a comment.
- {{FileSource | NA}}
- {{FileSource | NA | (archive file)}}
If the first input parameter contains any other string (or no string), then, the file source is considered as not yet filled:
- {{FileSource}}
- {{FileSource | Unknown value | Ignored field}}
2. Example[edit source]
Source → exists |
Source → STMicroelectronics intranet |
Source → STMicroelectronics intranet |
Source → STMicroelectronics intranet |
Source → STMicroelectronics intranet |
Source → OpenEmbedded |
Source → http://www.openembedded.org/ |
Source → not applicable |
Source → not applicable (archive file) |
Source → not yet filled |
Source → not yet filled |
3. Code[edit source]
Source → not yet filled |