STM32MP15 Discovery kits - starting for the first time

Revision as of 18:05, 9 January 2019 by deleted>Frq08988
(diff) ← Older revision | Latest revision (diff) | Newer revision → (diff)

Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion

This article aims to present how to configure and start for the first time a STM32MP15 Discovery kit that has just been flashed.

Warning white.png Warning
For assistance with starting up the boards, it is recommended to go through the related Starter Package articles: Category:Starter Package


Now that the image is flashed on the STM32MP15 Discovery kit, let's finalize the system configuration:

  • Step 1: check the configuration of the switches
    • The figure below shows the position of the boot switches in order to boot from the microSD card.
  • Step 2: (optional) connect a USB keyboard and/or a USB mouse (not provided) using the USB type A ports (3 and 4)
  • Step 3: (optional) connect an Ethernet cable (not provided) to the dedicated connector (7)


MB1272 motherboard: STM32MP157x 12x12,  PMIC,  DDR3MicroSD card slot2 x USB Type-A (host) → mouse,  keyboard or USB driver2 x USB Type-A (host) → mouse,  Keyboard or USB driverUSB micro-B (ST-LINK/V2-1) → PC virtual COM port and debugReset buttonEthernet → NetworkUSB Type-C (power 5V-3A)
STM32MP157x-DKx Discovery kit connections

STM32MP157C-DK2 shown here without the MB1407 daughterboard DSI display to avoid hiding the connections (picture is not contractual)



  • Step 4: check that the microSD card is inserted into the dedicated slot (2)
  • Step 5: connect the provided power supply (5 V, 3 A) to the USB type C connector (8)
  • Step 6: (optional) connect the ST-Link V2.1 USB micro-B port (5) to a host PC that runs a Terminal program with STLink V2.1 virtual port (e.g. Minicom on Ubuntu Linux PC or Tera Term on Windows PC)
  • Step 7: (optional) connect a HDMI monitor (or TV) to the HDMI connector. This option is particularly useful for the STM32MP157X-DK1 Discovery kit that does not include any DSI display daughterboard

File:STM32MP157X-DKX HDMI.png

  • Step 8: press the reset button (6) to reset the board

The board boots and the system will be available after few seconds.