This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage
Template "ArticleBasedOnModel" must be used to identified on which model the article in based. Should be used in lot of articles. Required position is on the top of article.
- {{ArticleBasedOnModel|Model used to create the article}}
2. Example
This article is based on model Model used to create the article. It must follow it as much as possible. |
3. Code
This article is based on model {{{1}}}. It must follow it as much as possible. |