This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User (Merge articles) |
||
Line 1: | Line 1: | ||
<noinclude> | <noinclude> | ||
==Usage== | ==Usage== | ||
The [[Template:U-Boot$|U-Boot$]] template is used '''to prefix a command that must be executed on the U-Boot console, with a U-Boot-specific prompt'''. | The [[Template:U-Boot$|U-Boot$]] template is used '''to prefix a command that must be executed on the U-Boot console, with a U-Boot-specific prompt'''.<br> | ||
Thanks to the <code>u-boot-prompt</code> class defined in [[MediaWiki:Common.css]], a double (or triple) click to select the command doesn't select the prompt. | |||
Usage: <nowiki>{{</nowiki>U-Boot$}} | Usage: <nowiki>{{</nowiki>U-Boot$}} | ||
Line 9: | Line 10: | ||
! You type !! You get | ! You type !! You get | ||
|- | |- | ||
| <code> | | <code>help env</code> command executed on the U-Boot console | ||
<pre style="white-space: pre-wrap;"> | <pre style="white-space: pre-wrap;"> | ||
{{U-Boot$}} | {{U-Boot$}} help env<br> | ||
env - environment handling commands | |||
</pre> | </pre> | ||
| | | | ||
{{U-Boot$}} | {{U-Boot$}} help env<br> | ||
env - environment handling commands | |||
|} | |} | ||
==More examples== | |||
{| class="st-table" | |||
! You type !! You get | |||
|- | |||
| 2 commands executed on the U-Boot console and preformatted text block (space at the beginning of each line) | |||
<pre style="white-space: pre-wrap;"> | |||
{{U-Boot$}} help env | |||
env - environment handling commands | |||
{{U-Boot$}} env default -a | |||
</pre> | |||
| | |||
{{U-Boot$}} help env | |||
env - environment handling commands | |||
{{U-Boot$}} env default -a | |||
|- | |||
| Command executed on the U-Boot console and preformatted text block (space at the beginning of each line) | |||
<pre style="white-space: pre-wrap;"> | |||
{{U-Boot$}} help env | |||
env - environment handling commands | |||
</pre> | |||
| | |||
{{U-Boot$}} help env | |||
env - environment handling commands | |||
|- | |||
| Long command executed on the U-Boot console and preformatted text block (space at the beginning of each line) | |||
<pre style="white-space: pre-wrap;"> | |||
{{U-Boot$}} this is a so long command executed on the U-Boot console that a horizontal scrolling bar is needed | |||
</pre> | |||
| style="max-width:30em;" | | |||
{{U-Boot$}} this is a so long command executed on the U-Boot console that a horizontal scrolling bar is needed | |||
|- | |||
| Template used within another public message box template | |||
<pre style="white-space: pre-wrap;"> | |||
{{Info | | |||
Message before the command | |||
{{U-Boot$}} help env | |||
env - environment handling commands | |||
Message after the command | |||
}} | |||
</pre> | |||
| | |||
{{Info | | |||
Message before the command | |||
{{U-Boot$}} help env | |||
env - environment handling commands | |||
Message after the command | |||
}} | |||
|- | |||
| Template used within another protected message box template | |||
<pre style="white-space: pre-wrap;"> | |||
{{InternalInfo | | |||
Message before the command | |||
{{U-Boot$}} help env | |||
env - environment handling commands | |||
Message after the command | |||
}} | |||
</pre> | |||
| | |||
{{InternalInfo | | |||
Message before the command | |||
{{U-Boot$}} help env | |||
env - environment handling commands | |||
Message after the command | |||
}} | |||
|} | |||
==Maintenance== | |||
This template is a template common to all ST wikis. <br> | |||
Modifications must be done into the [[stwikimodel:Template:U-Boot$|WikiModel]]. They must be reviewed by all ST wikis maintainers.<br> | |||
When approved, the template can be pushed/merged towards all ST wikis. | |||
==Code== | ==Code== | ||
</noinclude> | </noinclude><span class{{=}}"u-boot-prompt"></span> |
Latest revision as of 16:24, 4 October 2022
1. Usage[edit source]
The U-Boot$ template is used to prefix a command that must be executed on the U-Boot console, with a U-Boot-specific prompt.
Thanks to the u-boot-prompt
class defined in MediaWiki:Common.css, a double (or triple) click to select the command doesn't select the prompt.
U-Boot$}}Usage: {{
2. Basic examples[edit source]
You type | You get |
---|---|
help env command executed on the U-Boot console
U-Boot$}} help env<br> env - environment handling commands{{ |
help env |
3. More examples[edit source]
You type | You get |
---|---|
2 commands executed on the U-Boot console and preformatted text block (space at the beginning of each line)
U-Boot$}} help env env - environment handling commands {{U-Boot$}} env default -a{{ |
help env
env - environment handling commands
env default -a
|
Command executed on the U-Boot console and preformatted text block (space at the beginning of each line)
U-Boot$}} help env env - environment handling commands{{ |
help env
env - environment handling commands
|
Long command executed on the U-Boot console and preformatted text block (space at the beginning of each line)
U-Boot$}} this is a so long command executed on the U-Boot console that a horizontal scrolling bar is needed{{ |
U-Boot console that a horizontal scrolling bar is neededthis is a so long command executed on the |
Template used within another public message box template
U-Boot$}} help env env - environment handling commands Message after the command }}{{Info | Message before the command {{ |
|
Template used within another protected message box template
U-Boot$}} help env env - environment handling commands Message after the command }}{{InternalInfo | Message before the command {{ |
4. Maintenance[edit source]
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.
5. Code[edit source]