Last edited 3 years ago

Template:STYellow: Difference between revisions


Latest revision as of 18:01, 7 October 2021

1. Usage

The STYellow template is used to color text in pages, with the STMicroelectronics corporate primary color shade of yellow (█).

Where:

Usage:  {{STYellow|<text to color>|tint=<tint>}}
  • <text to color> is the text to format in yellow. If this template is called with no text, the hexadecimal code of the color is returned.
  • <tint> is the tint of the color expressed in percentage. If tint is not set then the original color is used (tint = 100%). The possible value are:
    • 75: 75% of the original color tint
    • 50: 50% of the original color tint
    • 25: 25% of the original color tint

2. Basic examples

You type You get
Coloring text in yellow
This is a {{STYellow|STMicroelectronics corporate color: shade of yellow: █}}

This is a STMicroelectronics corporate color: shade of yellow: █

Coloring text in 75% tint of yellow
This is a {{STYellow|STMicroelectronics corporate color: 75% tint of yellow: █ | tint=75}}

This is a STMicroelectronics corporate color: 75% tint of yellow: █

Coloring text in 50% tint of yellow
This is a {{STYellow|STMicroelectronics corporate color: 50% tint of yellow: █ | tint=50}}

This is a STMicroelectronics corporate color: 50% tint of yellow: █

Coloring text in 25% tint of yellow
This is a {{STYellow|STMicroelectronics corporate color: 25% tint of yellow: █ | tint=25}}

This is a STMicroelectronics corporate color: 25% tint of yellow: █

Getting the hexadecimal code of the color
{{STYellow}} is the hexadecimal code of STMicroelectronics yellow.

#FFD200 is the hexadecimal code of STMicroelectronics yellow.

Getting the hexadecimal code of the 75% tint of the color
{{STYellow | tint=75}} is the hexadecimal code of STMicroelectronics 75% tint of yellow.

#FFD200 is the hexadecimal code of STMicroelectronics 75% tint of yellow.

Getting the hexadecimal code of the 50% tint of the color
{{STYellow | tint=50}} is the hexadecimal code of STMicroelectronics 50% tint of yellow.

#FFD200 is the hexadecimal code of STMicroelectronics 50% tint of yellow.

Getting the hexadecimal code of the 25% tint of the color
{{STYellow | tint=25}} is the hexadecimal code of STMicroelectronics 25% tint of yellow.

#FFD200 is the hexadecimal code of STMicroelectronics 25% tint of yellow.

3. More examples

You type You get
yellow and bold
This is a {{STYellow|'''STMicroelectronics'''}} corporate color: '''{{STYellow|shade of yellow: █}}'''

This is a STMicroelectronics corporate color: shade of yellow: █

yellow and italic
This is a {{STYellow|''STMicroelectronics''}} corporate color: ''{{STYellow|shade of yellow: █}}''

This is a STMicroelectronics corporate color: shade of yellow: █

4. Maintenance

This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.

5. Code

#FFD200

No categories assignedEdit