This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User |
||
| (9 intermediate revisions by one other user not shown) | |||
| Line 6: | Line 6: | ||
{{Warning|For more specific information, go through the Distribution Package article relative to your STM32 microprocessors Series: [[:Category:Distribution Package]]}} | {{Warning|For more specific information, go through the Distribution Package article relative to your STM32 microprocessors Series: [[:Category:Distribution Package]]}} | ||
==STM32MP15-Ecosystem-v1. | ==STM32MP15-Ecosystem-v1.2.0 release== | ||
<onlyinclude> | <onlyinclude> | ||
* The STM32MP1 OpenSTLinux distribution is delivered through a manifest repository location and a manifest revision ('''openstlinux-20-02-19'''). | |||
* The installation relies on the ''repo'' command. In case the Repo tool (a Google-built repository management tool that runs on top of Git) is not yet installed and configured on the host PC, refer to the [[PC prerequisites]] article. | |||
* The OpenSTLinux distribution is massively using open source software (OSS) packages that are downloaded from a variety of open source repositories; so it is required that the IT infrastructure proxies do not forbid such accesses. If some proxy-related issues are suspected, refer to the [[How to avoid proxy issues]] article. | |||
* Install the STM32MP1 OpenSTLinux distribution | |||
{| class="st-table" | |||
|- | |||
! !! style="text-align:center;" |STM32MP1 Distribution Package OpenSTLinux distribution - STM32MP15-Ecosystem-v1.2.0 release | |||
|- | |||
| Installation || <span id="Download"></span> | |||
* Go to the host PC directory where to install the Distribution Package (''<Distribution Package installation directory>''). Example, if following the [[Example of directory structure for Packages|proposition to organize the working directory]]: | |||
$ cd <working directory path>/Distribution-Package | |||
* Create the OpenSTLinux distribution installation sub-directory: | |||
<pre> | |||
$ mkdir openstlinux-20-02-19 | |||
$ cd openstlinux-20-02-19 | |||
</pre> | |||
* Initialize repo in the current directory (More details on 'repo init' [https://source.android.com/setup/develop/repo#init here]). | |||
{{Highlight| For Ubuntu 16.04 you should use the legacy repo, procedure to install [https://source.android.com/setup/build/downloading#old-repo-python2 here]}} | |||
<pre> | |||
$ repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-20-02-19 | |||
</pre> | |||
'''Note:''' "ERROR 404" may appear during "repo init" command without any impact on the process <br> | |||
* Synchronize the local project directories with the remote repositories specified in the manifest (more details on 'repo sync' [https://source.android.com/setup/develop/repo#sync here])<br> | |||
<pre> | |||
$ repo sync | |||
</pre> | |||
'''Note:''' ''Distribution package'' needs around 140MB to be installed (and around 25GB once ''distribution package'' is compiled).<br> | |||
|- | |||
| Release note || | |||
Details about the content of this software package are available in the '''associated''' [[STM32MP15 ecosystem release note - v1.2.0|STM32MP15 ecosystem release note]]. | |||
[[File:Archive_box.png|25px|link=]] If interested in previous releases, go through the [[STM32MP1_Distribution_Package_-_OpenSTLinux_distribution#Archives| archives]] of the ecosystem release note. | |||
|} | |||
* The '''OpenSTLinux distribution installation directory''' is in the ''<Distribution Package installation directory>, and is named ''openstlinux-20-02-19'': | |||
{{Green|openstlinux-20-02-19}} {{Highlight|OpenSTLinux distribution}} | |||
├── {{Green|layers}} | |||
│ ├── {{Green|meta-openembedded}} {{Highlight|Collection of layers for the OpenEmbedded-Core universe ([[OpenEmbedded]] standard)}} | |||
│ ├── {{Green|meta-qt5}} {{Highlight|QT5 layer for OpenEmbedded (standard)}} | |||
│ ├── {{Green|meta-st}} | |||
│ │ ├── {{Green|meta-st-openstlinux}} {{Highlight|STMicroelectronics layer that contains the frameworks and images settings for the OpenSTLinux distribution}} | |||
│ │ ├── {{Green|meta-st-stm32mp}} {{Highlight|STMicroelectronics layer that contains the description of the BSP for the STM32 MPU devices}} | |||
│ │ │ ├── {{Green|recipes-bsp}} | |||
│ │ │ │ ├── {{Green|alsa}} {{Highlight|Recipes for ALSA control configuration}} | |||
│ │ │ │ ├── {{Green|drivers}} {{Highlight|Recipes for Vivante GCNANO GPU kernel drivers}} | |||
│ │ │ │ ├── {{Green|trusted-firmware-a}} {{Highlight|Recipes for TF-A}} | |||
│ │ │ │ └── {{Green|u-boot}} {{Highlight|Recipes for U-Boot}} | |||
│ │ │ ├── {{Green|recipes-extended}} | |||
│ │ │ │ ├── {{Green|linux-examples}} {{Highlight|Recipes for Linux examples for STM32 MPU devices}} | |||
│ │ │ │ ├── {{Green|m4coredump}} {{Highlight|Recipes for script to manage coredump of cortexM4}} | |||
│ │ │ │ └── {{Green|m4projects}} {{Highlight|Recipes for firmware examples for Cortex M4}} | |||
│ │ │ ├── {{Green|recipes-graphics}} | |||
│ │ │ │ ├── {{Green|gcnano-userland}} {{Highlight|Recipes for Vivante libraries OpenGL ES, OpenVG and EGL (multi backend)}} | |||
│ │ │ │ └── [...] | |||
│ │ │ ├── {{Green|recipes-kernel}} | |||
│ │ │ │ ├── {{Green|linux}} {{Highlight|Recipes for Linux kernel}} | |||
│ │ │ │ └── {{Green|linux-firmware}} {{Highlight|Recipes for Linux firmwares (example, Bluetooth firmware)}} | |||
│ │ │ ├── {{Green|recipes-security}} | |||
│ │ │ │ └── {{Green|optee}} {{Highlight|Recipes for OPTEE}} | |||
│ │ │ ├── {{Green|recipes-st}} | |||
│ │ │ │ └── {{Green|images}} {{Highlight|Recipes for the ''bootfs'' and ''userfs'' partitions binaries}} | |||
│ │ │ └── [...] | |||
│ │ ├── {{Green|meta-st-stm32mp-addons}} {{Highlight|STMicroelectronics layer that helps managing the STM32CubeMX integration}} | |||
│ │ └── {{Green|scripts}} | |||
│ │ ├── envsetup.sh {{Highlight|'''Environment setup script''' for Distribution Package}} | |||
│ │ └── [...] | |||
│ ├── {{Green|meta-timesys}} {{Highlight|Timesys layer for OpenEmbedded (standard)}} | |||
│ └── {{Green|openembedded-core}} {{Highlight|Core metadata for current versions of [[OpenEmbedded]] (standard)}} | |||
{{InternalInfo| Additional layer for internal usage | |||
└── st-hands-on STMicroelectronics layer that contains the reference source code for the hands-on | |||
}} | |||
</onlyinclude> | |||
==Archives [[File:Archive_box.png|25px|link=]]== | |||
<div class="mw-collapsible mw-collapsed"> | |||
===STM32MP15-Ecosystem-v1.1.0 release=== | |||
<div class="mw-collapsible-content"> | |||
* The STM32MP1 OpenSTLinux distribution is delivered through a manifest repository location and a manifest revision ('''openstlinux-4.19-thud-mp1-19-10-09'''). | * The STM32MP1 OpenSTLinux distribution is delivered through a manifest repository location and a manifest revision ('''openstlinux-4.19-thud-mp1-19-10-09'''). | ||
* The installation relies on the ''repo'' command. In case the Repo tool (a Google-built repository management tool that runs on top of Git) is not yet installed and configured on the host PC, refer to the [[PC prerequisites]] article. | * The installation relies on the ''repo'' command. In case the Repo tool (a Google-built repository management tool that runs on top of Git) is not yet installed and configured on the host PC, refer to the [[PC prerequisites]] article. | ||
| Line 87: | Line 173: | ||
└── st-hands-on STMicroelectronics layer that contains the reference source code for the hands-on | └── st-hands-on STMicroelectronics layer that contains the reference source code for the hands-on | ||
}} | }} | ||
</ | </div></div> | ||
<div class="mw-collapsible mw-collapsed"> | <div class="mw-collapsible mw-collapsed"> | ||
===STM32MP15-Ecosystem-v1.0.0 release=== | ===STM32MP15-Ecosystem-v1.0.0 release=== | ||
Latest revision as of 10:44, 20 February 2020
This article aims to give the following information:
- How to download and install the latest OpenSTLinux distribution for the STM32 microprocessors Series
- Where to find the associated release note
- Where to find the previous releases (archives)
1. STM32MP15-Ecosystem-v1.2.0 release[edit source]
- The STM32MP1 OpenSTLinux distribution is delivered through a manifest repository location and a manifest revision (openstlinux-20-02-19).
- The installation relies on the repo command. In case the Repo tool (a Google-built repository management tool that runs on top of Git) is not yet installed and configured on the host PC, refer to the PC prerequisites article.
- The OpenSTLinux distribution is massively using open source software (OSS) packages that are downloaded from a variety of open source repositories; so it is required that the IT infrastructure proxies do not forbid such accesses. If some proxy-related issues are suspected, refer to the How to avoid proxy issues article.
- Install the STM32MP1 OpenSTLinux distribution
| STM32MP1 Distribution Package OpenSTLinux distribution - STM32MP15-Ecosystem-v1.2.0 release | |
|---|---|
| Installation |
$ cd <working directory path>/Distribution-Package
$ mkdir openstlinux-20-02-19
$ cd openstlinux-20-02-19
For Ubuntu 16.04 you should use the legacy repo, procedure to install here $ repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-20-02-19
Note: "ERROR 404" may appear during "repo init" command without any impact on the process
$ repo sync
Note: Distribution package needs around 140MB to be installed (and around 25GB once distribution package is compiled). |
| Release note |
Details about the content of this software package are available in the associated STM32MP15 ecosystem release note.
|
- The OpenSTLinux distribution installation directory is in the <Distribution Package installation directory>, and is named openstlinux-20-02-19:
openstlinux-20-02-19 OpenSTLinux distribution ├── layers │ ├── meta-openembedded Collection of layers for the OpenEmbedded-Core universe (OpenEmbedded standard) │ ├── meta-qt5 QT5 layer for OpenEmbedded (standard) │ ├── meta-st │ │ ├── meta-st-openstlinux STMicroelectronics layer that contains the frameworks and images settings for the OpenSTLinux distribution │ │ ├── meta-st-stm32mp STMicroelectronics layer that contains the description of the BSP for the STM32 MPU devices │ │ │ ├── recipes-bsp │ │ │ │ ├── alsa Recipes for ALSA control configuration │ │ │ │ ├── drivers Recipes for Vivante GCNANO GPU kernel drivers │ │ │ │ ├── trusted-firmware-a Recipes for TF-A │ │ │ │ └── u-boot Recipes for U-Boot │ │ │ ├── recipes-extended │ │ │ │ ├── linux-examples Recipes for Linux examples for STM32 MPU devices │ │ │ │ ├── m4coredump Recipes for script to manage coredump of cortexM4 │ │ │ │ └── m4projects Recipes for firmware examples for Cortex M4 │ │ │ ├── recipes-graphics │ │ │ │ ├── gcnano-userland Recipes for Vivante libraries OpenGL ES, OpenVG and EGL (multi backend) │ │ │ │ └── [...] │ │ │ ├── recipes-kernel │ │ │ │ ├── linux Recipes for Linux kernel │ │ │ │ └── linux-firmware Recipes for Linux firmwares (example, Bluetooth firmware) │ │ │ ├── recipes-security │ │ │ │ └── optee Recipes for OPTEE │ │ │ ├── recipes-st │ │ │ │ └── images Recipes for the bootfs and userfs partitions binaries │ │ │ └── [...] │ │ ├── meta-st-stm32mp-addons STMicroelectronics layer that helps managing the STM32CubeMX integration │ │ └── scripts │ │ ├── envsetup.sh Environment setup script for Distribution Package │ │ └── [...] │ ├── meta-timesys Timesys layer for OpenEmbedded (standard) │ └── openembedded-core Core metadata for current versions of OpenEmbedded (standard)
2. Archives
[edit source]
Expand
2.1. STM32MP15-Ecosystem-v1.1.0 release[edit source]
Expand