This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User No edit summary |
||
Line 1: | Line 1: | ||
<noinclude> | <noinclude> | ||
This article aims to present how to assemble the '''STM32MP157x-EV1''' Evaluation boards. It is valid both for the STM32MP157A-EV1 and STM32MP157C-EV1 Evaluation boards: the part numbers are specified in the [[STM32MP15 microprocessor#Part number codification|STM32MP15 microprocessor part numbers]] article. | This article aims to present how to assemble the '''STM32MP157x-EV1''' Evaluation boards. It is valid both for the STM32MP157A-EV1 and STM32MP157C-EV1 Evaluation boards: the part numbers are specified in the [[STM32MP15 microprocessor#Part number codification|STM32MP15 microprocessor part numbers]] article. | ||
{{Warning|To start efficiently the board, it's recommended to go through its Starter Package article: [[:Category:Starter Package]]}} | {{Warning|To start efficiently the board, it's recommended to go through its Starter Package article: [[:Category:Starter Package]]}} | ||
Line 32: | Line 30: | ||
[[File: STM32MP157x-EV1_assembled.png | thumb | upright=4 | center | link= | STM32MP157x-EV1 Evaluation board assembled <br> '''STM32MP157A-EV1''' shown here (picture is not contractual)]] | [[File: STM32MP157x-EV1_assembled.png | thumb | upright=4 | center | link= | STM32MP157x-EV1 Evaluation board assembled <br> '''STM32MP157A-EV1''' shown here (picture is not contractual)]] | ||
<noinclude> | |||
[[Category:Sub-articles]] | |||
{{PublicationRequestId | 7572 | 2018-06-19 | AlainF}} | |||
</noinclude> |
Latest revision as of 15:18, 31 January 2020
This article aims to present how to assemble the STM32MP157x-EV1 Evaluation boards. It is valid both for the STM32MP157A-EV1 and STM32MP157C-EV1 Evaluation boards: the part numbers are specified in the STM32MP15 microprocessor part numbers article.
The STM32MP157x-EV1 Evaluation boards packages (STM32MP157A-EV1 and STM32MP157C-EV1) include all the items listed below.
Position | Description |
---|---|
1 | MB1262 motherboard |
2 | MB1263 daughterboard |
3 | MB1230 DSI 720p display |
4 | MB1379 daughterboard camera |
5 | microSD card |
6 | Power supply block (5V, 3A) |
The following figures explain how to assemble these different items to get the STM32MP157x-EV1 Evaluation boards.