This article is a tutorial on how to use NanoEdge™ AI Studio to create a multi-state vibrations classifier running on the SensorTile.box PRO with multi-sensors and wireless connectivity development kit (STEVAL-MKBOXPRO).
This tutorial shows you how to program the SensorTile.box PRO for datalogging; how to use NanoEdge™ AI Studio to collect data, label data, find the best algorithm, run the Emulator, generate the library files for deployment; how to use STM32CubeIDE to modify codes, build the project, program the SensorTile.box PRO; and finally run the classifier on SensorTile.box PRO. The main process of this tutorial is shown in the flowchart below:
1. Prerequisites
1.1. Hardware
- An STEVAL-MKBOXPRO development kit board,
- One USB-C cable (to connect the SensorTile.box PRO to PC),
- A Windows® powered laptop/PC (Windows® 7, 8, or 10),
- A multi-speed USB powered fan (can be ordered from this link), which has three speed mode: low, medium and high.
1.2. Software
1.2.1. Source Code
- A firmware package
stwin-fan-classifier-wiki-package.zip
is ready to download from st.com, please TODO: download the zip file here. The package includes:
- Project source code in subfolder
STEVAL-MKBOXPRO_LSM6DSV16X
- Two Pre-compiled binary files in subfolder
Binary
:
SensorTile_Fan_Classifier-datalog.bin
for dataloggingSensorTile_Fan_Classifier-detection.bin
for detection
- Library files generated by NanoEdge™ AI Studio in subfolder
libneai_sensortile-fan-nclassifier.zip
- Project source code in subfolder
1.2.2. NanoEdge™ AI Studio
- NanoEdge™ AI Studio is a new Machine Learning (ML) technology to bring true innovation easily to the end-users. In just a few steps, developers can create an optimal ML library for their project, based on a minimal amount of data.
- Download NanoEdge™ AI Studio as a free trial version for the STMicroelectronics boards.
- After registration, you will receive the license key in your registered email, which will be used to active NanoEdge™ AI Studio when you launch it for the first time.
1.2.3. STM32CubeIDE
- STM32CubeIDE is an all-in-one multi-OS development tool, which is part of the STM32Cube software ecosystem. It is an advanced C/C++ development platform with peripheral configuration, code generation, code compilation, and debug features for STM32 microcontrollers and microprocessors.
- Download STM32CubeIDE from st.com
1.2.4. Tera Term
- Tera Term is an open-source and freely available software terminal emulator, which is used to display the classification results.
- Users can download and install the latest version available from Tera Term.
2. Program SensorTile.box PRO for datalogging
The first step is to connect the SensorTile.box PRO to your PC and program it for datalogging mode with the provided binary file.
2.1. Board connection
There is a single connection to make on the SensorTile.box PRO, as shown in the picture:
- Plug the USB cable ‘C’ side into the SensorTile.box PRO
- Plug the SensorTile USB cable into PC
2.2. Program SensorTile.box PRO using binary file
The easiest way to program the SensorTile.box PRO is using the STM32CubeProgrammer. Once you have the pre-built binary file on your local disk, use CubeProgrammer to flash it to SensorTile.box PRO:
- On SensorTile, slide the power button to OFF position
- Press and hold button 2 and slide the power button to ON position
- Launch CubeProgrammer and select USB from the dropdown menu
- Refresh the Port
- Connect using USB
- Under the Erasing & Programming tab, press Browse and select the SensorTile_Fan_Classifier-datalog.elf binary file
- Click Start Programming
You will see a success prompt once programming is complete. Then, close CubeProgrammer.
3. Create an n-Class Classification Project in NanoEdge™ AI Studio
In this step, we will create an n-Class classification project in NanoEdge™ AI Studio, and configure the project settings.
Open NanoEdge™ AI Studio on PC, you should see the welcome interface below and then follow the steps:
- Click on n-Class Classification to choose it as project type.
- Click on CREATE NEW PROJECT to create the project.
You should see the Project settings page as below:
- Give the project a name, e.g. SensorTile-Fan-nClassifier
- Add a brief description for the project.
- Leave the Max RAM as default.
- Choose No Flash limit
- Choose STEVAL-MKBOXPRO for Target. On the target selection screen, scroll down to STM32U5 series, select STEVAL-MKBOXPRO, and click Confirm.
- Choose Accelerometer 3 axes for Sensor type.
- Finally, click on NEXT to go to the next step.
4. Datalogging in NanoEdge™ AI Studio
In this step, we will alter the speed of the fan by pressing the button on the back, as well as applying clog to the fan to collect data for seven (7) classes: stop, low speed, medium speed, high speed, low speed clogged, medium speed clogged and high speed clogged.
4.1. Hardware Setup before datalogging
Before starting datalogging, it is recommended to disconnect SensorTile.box PRO from the PC and power cycle the board.
- Slide the Power switch to OFF position
- Stick the SensorTile on top of the fan with double-sided tape (or use normal tape to make a ring as double-sided tape)
- Connect the USB Cable and slide the Power switch to ON position
- Plug the USB cable of the fan into PC or USB charger. Leave the fan in stop mode
4.2. Start Datalogging
Next, we will use the programmed SensorTile and NanoEdge™ AI Studio to collect the data for each class via USB streaming. Go back to NanoEdge™ AI Studio, once the project was created, you should see the window as shown below:
- Click on ADD SIGNAL to open the "Import signal" window.
- In the pop-up window, choose FROM SERIAL (USB) as Type of signal source.
- In the next window, select your Serial / COM port. Refresh if needed.
- Select 115200 for Baudrate
- Check the box to define Max lines of 100 signals. By doing this, the data logger will automatically stop when 100 lines of signal are collected.
- Give a class name, e.g. "stop", which will be used to shown as classification result later.
- Make sure the fan is initially turned off. Then click on the START/STOP button to start data logging. The real-time data and plotting will be shown.
- Once 100 lines of signal are collected, the data logger will stop. click on CONTINUE to the next step.
- You can preview the collected data. If no problem, click on IMPORT to finish datalogging for this class.
- Repeat step 1-9 to add all classes
- Press the button on the back the fan to switch its speed between low, medium and high
- Use a sticky note or a notebook (stick the sticky note or put the notebook closely at the front side of the fan) to clog the fan for clogged classes.
- You should finally have 7 classes in total, including stop, low speed, medium speed, high speed, low speed clogged, medium speed clogged and high speed clogged. The final result is shown below and you are ready for next step.
5. Benchmarking in NanoEdge™ AI Studio
In this step, we will use NanoEdge™ AI Studio to quickly and automatically find the optimized algorithm for our use case.
After collecting the data for all classes, click on "Benchmark" in NanoEdge™ AI Studio. You should see the welcome interface as shown below:
- Click on RUN NEW BENCHMARK
- A "Select your Class" window will pop up. Select All classes and click on START.
- Then the Studio will start the benchmarking, you should see the window below:
- This area shows the benchmark status and it's timestamp
- Notable information and events such as benchmark status, search speed per thread, and new libraries found
- Elapsed time and number of libraries tested
- Performance indicators: Higher balanced accuracy and confidence level are better, while lower RAM and Flash sizes are better
- Graph shows the evolution of the performance indicators over time, as thousands of candidate libraries are tested.
- This area contains control buttons:
- You can pause the benchmark and resume later
- You can stop the benchmark when the desired performance is reached
- Once you are satisfied with the performance during the library selection process, click on the "STOP" button to end the benchmarking. The optimized algorithm will be selected for deployment later. You should see the details of this benchmark as below:
6. Validation in NanoEdge™ AI Studio
The validation screen is used to summarize any selected benchmark or to compare the metrics of two benchmarks. Click on "Validation" in NanoEdge™ AI Studio to open the validation interface:
7. Emulator in NanoEdge™ AI Studio
In this step, we will use the Emulator in NanoEdge™ AI Studio to verify the selected library before we generate and deploy the library files on STWIN.
After finish the benchmarking, click on "Emulator" in NanoEdge™ AI Studio to open the Emulator interface.
- Click on the INITIALIZE EMULATOR button to open the Emulator, and click on FROM SERIAL(USB) tab. Then the process is similar to datalogging step as shown below:
- Select Serial data as we did in datalogging step.
- Select the same COM port
- Select the same Baudrate.
- Get the fan ready in any mode, and click on the "START/STOP" button. The real-time classification result should be shown in the Live Repartition as blue bar.
- Switch between different speeds, and add clogs. Check the classification results.
- Click on the "START/STOP" button to stop the emulation.
- If the classification results are not accurate, you should go back to datalogging step to start over the datalogging and benchmarking process.
- Otherwise you can go to the next step to generate the library files for deployment.
8. Deployment in NanoEdge™ AI Studio
In this step, we will generate the library files using NanoEdge™ AI Studio.
8.1. Generate library files in NanoEdge™ AI Studio
When you finish the Emulator, click on "Deployment" in NanoEdge™ AI Studio to open the Deploy interface for library generation.
- If you have multiple benchmarks, choose the one you want to compile. Otherwise, leave it default.
- Check the box for
Float abi
to enable the hardware FPU operations. - Click on the COMPILE LIBRARY button, and there will be a pop-up window as shown below:
- Click Get Library and fill the survey or press skip, then there will be another pop-up window letting you to choose a local directory to save the libraries.
- Locate to a local directory you prefer, rename the file as you want, then click on Save.
- Go to the directory you chose, make sure the file
libneai_*.zip
is successfully saved there, extract the file, and you are ready for the next step.
8.2. Library files explanation
The NanoEdge AI static library for classification is the code that contains an AI model (for example, as a bundle of signal treatment, machine learning model, optimally tuned hyperparameters, etc.) designed to identify a sensor pattern in a class. All classes are defined by the user in NanoEdge™ AI Studio and are used during the training process of the AI model.
After the zip file is extracted, you should find these folders and files included:
There are three files we will need for next step: libneai.a
, knowledge.h
and NanoEdgeAI.h
.
libneai.a
is the C/C++ static library for the classifier.knowledge.h
is the header file that contains the knowledge buffer declaration.NanoEdgeAI.h
is the header file that contains function prototypes and sample declarations. An example of the code is shown below:
9. Program STWIN for Detection
In this step, we will add the library files into the project, import the project into STM32CubeIDE, modify the source code, then program the SensorTile.box PRO for detection.
- Replace the old library files by the new ones
- Go to the library folder, copy the file
libneai.a
- Go to the project folder
..\STEVAL-MKBOXPRO_LSM6DSV16X\Core\Src
, paste the file here, and click on Replace the file in the destination in the pop-up window. - Go back to the library folder, copy the files
knowledge.h
andNanoEdgeAI.h
. - Go back to the project folder
..\STEVAL-MKBOXPRO_LSM6DSV16X\Core\Inc
, paste the files here, and click on Replace the files in the destination in the pop-up window.
- Go to the library folder, copy the file
- Import project into STM32CubeIDE workspace
- Open STM32CubeIDE on your PC, create or choose a workspace and click Launch to launch your workspace.
- In the menu bar, click File -> Import...
- In the pop-up window, select Existing Projects into Workspace, and click Next, as shown below:
- In the next interface, click Browse..., find the project folder where you saved and then click Select Folder, then click Finish and wait for the project to be imported, as shown in the picture below:
- Build Project and Program the STWIN
- In STM32CubeIDE, unfold the project in Project Explorer, find
..\Core\Src\main.c
and..\Core\Inc\NanoEdgeAI.h
. Double click on the two files separately to open them in the Editor, as shown below:
- In STM32CubeIDE, unfold the project in Project Explorer, find
- In
main.c
, go to line 48 to find#define NEAI_MODE
. Change the value to "1" if it is not, as shown below:
- In
- Then go to
NanoEdgeAI.h
, find the buffer declarations in the commented part underneath, select the codes of "buffer for mapping class id to class name", line 84 to 93const char *id2class[CLASS_NUMBER + 1]
. Right click and choose "Copy" or simply pressCtrl+C
on the keyboard to copy the codes:
- Then go to
- Go back to
main.c
, paste the copied codes belowfloat output_class_buffer[CLASS_NUMBER];
to replace the existing declarations. As shown below:
- Go back to
- Press
CTRL + S
to save the changes. - Click on the “hammer” button to build the project:
- After built successfully, you should see
Build Finished. 0 errors, 0 warnings. (took 2s.866ms)
in the console. - There is a Debug folder generated, in which you can find the STEVAL-MKBOXPRO_LSM6DSV16X.elf binary file that we will use for next step
- Press
- Replace the old library files by the new ones
- Once you have generated the binary, use CubeProgrammer to flash it to SensorTile
- On SensorTile, slide the power button to OFF position
- Once you have generated the binary, use CubeProgrammer to flash it to SensorTile
- Press and hold button 2 and slide the power button to ON position
- Launch CubeProgrammer and select USB from the dropdown menu
- Refresh the Port
- Connect using USB
- Under the Erasing & Programming tab, press Browse and select the binary file we just built, which can be found in this path:
- Click Start Programming
..\STEVAL-MKBOXPRO_LSM6DSV16X\Debug\ STEVAL-MKBOXPRO_LSM6DSV16X.elf
Close CubeProgrammer once you see a success prompt indicating that programming is complete.
10. Run the Classifier on STWIN
In this step, we will run the fan classifier on STWIN and use Tera Term to display the classification results.
- Once the STWIN is successfully programmed for detection, you can open the Tera Term on PC.
- In Tera Term's menu bar, click on Setup -> Terminal.... In the New-line setting, change Receive to AUTO, and Transmit to CR:
- Go back to Tera Term's menu bar, click on Setup -> Serial port.... The serial port setup window will pop up as shown below:
- Select the same COM port as we did in datalogging step for datalogging.
- Select the Baudrate value "115200" for Speed.
- Leave other settings as default, and click on New open.
- Get the fan ready and make sure STWIN is firmly attached at the top of the fan. The classification results will show in the interface, along with the probability of each class, as shown below:
11. Resources
- Firmware Package - Project source code and pre-compiled binary files
- NanoEdge™ AI Studio wiki
- NanoEdge™ AI Library for n-class classification (nCC) wiki
- UM2777 - How to use the STEVAL-STWINKT1B SensorTile Wireless Industrial Node for condition monitoring and predictive maintenance applications
- UM2237 STM32CubeProgrammer software description
- UM2609 STM32CubeIDE user guide
- How to troubleshoot common NanoEdge AI Studio installation / activation problems