This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Track the most recent changes to the wiki on this page.
List of abbreviations:
- N
- This edit created a new page (also see list of new pages)
- m
- This is a minor edit
- b
- This edit was performed by a bot
- (±123)
- The page size changed by this number of bytes
26 September 2024
N 16:07 | STM32WB0 Bluetooth® Low Energy AOA feature diffhist +21,235 Registered User (Created page with "{{DISPLAYTITLE:STM32WB0 Bluetooth® Low Energy AOA feature}} The STM32WB09, STM32WB05 MCUs support the Bluetooth LE Direction Finding angle of arrival (AoA) and angle of departure (AoD) feature. This document provides the key concepts related to the Bluetooth LE Direction Finding and some information about how these featurec could be supported in the context of STM32WB09, STM32WB05 MCUs. == Introduction == Bluetooth Core Specification v5.1 introduced Direction findin...") |
|
N 15:49 | STM32WB0 Bluetooth® LE network coprocessor (NCP) framework 2 changes history +28,675 [Registered User (2×)] | |||
|
15:49 (cur | prev) +26 Registered User (Changed categories.) | ||||
N |
|
15:39 (cur | prev) +28,649 Registered User (Added page for STM32WB0 NCP) Tag: 2017 source edit |
15:24 | Category:STM32WB0 Bluetooth LE Features diffhist +28,726 Registered User (→STM32WB0 Bluetooth® LE network coprocessor (NCP) framework: new section) |
25 September 2024
N 14:57 | STM32WB0 SW Package and Tools diffhist +195 Registered User (Created page with "In this category you can find various project which can help you 40 {{PublicationRequestId | Auto | | Automatic approval based on the “Category model” article}}") |
N 14:57 | STM32WB0 Devices Features diffhist +195 Registered User (Created page with "In this category you can find various project which can help you 35 {{PublicationRequestId | Auto | | Automatic approval based on the “Category model” article}}") |
N 14:56 | STM32WB0 Bluetooth LE Features diffhist +195 Registered User (Created page with "In this category you can find various project which can help you 30 {{PublicationRequestId | Auto | | Automatic approval based on the “Category model” article}}") |
N 14:54 | Applications and Profiles diffhist +195 Registered User (Created page with "In this category you can find various project which can help you 20 {{PublicationRequestId | Auto | | Automatic approval based on the “Category model” article}}") |
N 13:06 | Connectivity:STM32WB Zigbee memory requirements diffhist +35,906 Registered User (Created page with " {{DISPLAYTITLE:STM32WB-WBA Zigbee memory requirements}} ==Introduction== The Zigbee stack is a software component designed to enable Zigbee communication on the STM32WB/WBA microcontroller. Like any software, the Zigbee stack requires memory to operate. There are two main types of memory that are relevant to the stack: '''RAM''' and '''Flash''' memory.<br> '''RAM''' (Random Access Memory) is a type of volatile memory that is used for temporary storage of data and prog...") |
23 September 2024
N 14:40 | Security:Secure Boot for for STM32N6 diffhist +68 Registered User (Created page with " <noinclude> 30 </noinclude>") |
N 14:39 | Security:Secure storage-SAES key wrapping for STM32N6 diffhist +68 Registered User (Created page with " <noinclude> 25 </noinclude>") |
N 14:39 | Security:Product state for STM32N6 diffhist +68 Registered User (Created page with " <noinclude> 20 </noinclude>") |
N 14:36 | Security:BootRom for STM32N6 diffhist +68 Registered User (Created page with " <noinclude> 20 </noinclude>") |
N 14:34 | Security:SSP RSSe for STM32N6 diffhist +66 Registered User (Created page with " <noinclude> 20 </noinclude>") |
N 14:02 | Connectivity:STM32WB-WBA Zigbee memory requirements backend diffhist +37,420 Registered User (Created page with " {{DISPLAYTITLE:STM32WB-WBA Zigbee memory requirements}} ==Introduction== The Zigbee stack is a software component designed to enable Zigbee communication on the STM32WB/WBA microcontroller. Like any software, the Zigbee stack requires memory to operate. There are two main types of memory that are relevant to the stack: '''RAM''' and '''Flash''' memory.<br> '''RAM''' (Random Access Memory) is a type of volatile memory that is used for temporary storage of data and prog...") |
N 14:00 | Security:OEMiRoT for STM32N6 diffhist +22,824 Registered User (Created page with "This article gives an overview of the OEMiRoT solution integrated in STM32H7R. The chapter About hardware highlights the main differences with STM32H7S with an impact on the secure boot solutions. Except these differences this article is very similar to OEMiRoT OEMuRoT for STM32H7S '''List of applicable products:''' {| class="wikitable centre" style="width:100%;" |- ! scope=c...") |
N 13:58 | Security:Security features on STM32N6 MCUs diffhist +5,529 Registered User (Created page with "__NOTOC__ This article contains an overview of the security features<ref>Security acronyms and definitions</ref> available on STM32U0 MCUs. The table below contains detailed information based on the different product lines. {| |- ! Security features embedded on: !! 100px !! 100px!! 100px |- |#Secure Boot and Firmware Update|'''Secure B...") |
N 13:57 | Category:Security with STM32N6 diffhist +96 Registered User (Created page with "{{Security:Security features on STM32U0 MCUs}} <noinclude> 10 </noinclude>") |
N 13:54 | Category:STM32N6 diffhist +436 Registered User (Created page with "Please click on '''''Security with STM32U0''''' to access specific STM32U0 security features or on '''''Getting started with STM32U0 security''''' for useful examples <br><br><br> <imagemap> File:top_page_security_STM32U0.png|400px|center rect 0 0 1400 460 Category:Security with STM32U0 rect 0 467 1400 930 Category:Getting started with STM32U0 security desc none </imagemap> <noinclude> 10 </noinclude>") |
N 09:30 | Security:How to install a trusted application on STM32N6 MCUs diffhist +2,551 Registered User (Created page with "<big><big><big>''How to install a trusted application on STM32N6 MCUs''</big></big></big><br> <big><big>'''Literature'''</big></big><br> * [https://www.st.com/resource/en/user_manual/dm00403500.pdf UM2237] STM32CubeProgrammer software description * [https://www.st.com/resource/en/application_note/dm00413494-secure-programming-using-stm32cubeprogrammer-stmicroelectronics.pdf AN5054] Secure programming using STM32CubeProgrammer <big><big>'''Target description'''</big>...") |