This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Click here for Bluetooth® Low Energy Overview
1. Introduction
Many STM32WBA & STM32WB Bluetooth® Low Energy examples are provided within:
- The STM32CubeWBA MCU Package[1] running on STM32WBA Series MCUs.
- The STM32CubeWB MCU Package[2] running on STM32WBA Series MCUs.
Additionally to official examples, many examples are provided to an STMicroelectronics GitHub organization for unofficial STM32 projects (STM32 Hotspot[3]) These materials are contributed by ST’s STM32 experts on an informal basis and may bring added value to users looking for additional STM32 software resources coming from a trusted source.
2. STM32WBA Bluetooth® LE applications on STM32 Hotspot
The following Bluetooth® LE applications are delivered as source code
- To build and install them, follow the steps described in Bluetooth® LE Build and Install Application page
Application | Description | |
---|---|---|
Web Bluetooth® LE | STM32WBA Web Interface | Web Bluetooth® Application to support STM32WBA BLE Applications |
Operating System | FreeRTOS | P2P Server & Client example done with FreeRTOS OS |
Bluetooth® LE Medical System | Blood Pressure | Application supporting the Blood Pressure Sensor |
Bluetooth® LE Sport System | Running Speed & Cadence | Application supporting the RSC Sensor |
Bluetooth® LE Secure Application | TF-M Door Lock | This project illustrates how to create a BLE Secure Application in a TrustZoned environment running the TF-M |
Bluetooth® LE Demonstration | ANCS & AMS | Apple Notification Center and Media Services (ANCS & AMS) as specified by Apple |
Long Range Connection | Application to extend BLE range up to 1,6 km or more |
3. STM32WB Bluetooth® LE applications on STM32 Hotspot
The following Bluetooth® LE applications are delivered as source code
- To build and install them, follow the steps described in Bluetooth® LE Build and Install Application page
Application | Description | |
---|---|---|
Web Bluetooth® LE | Web Interface | Web Bluetooth® Application to support STM32WBA BLE Applications |
Bluetooth® LE Medical System | Health Thermometer | Application supporting the Health Thermometer Sensor with STM32WB1M Discovery Kit |
Bluetooth® LE System | Standby | Standby Example on STM32WB Nucleo |
FUS Command Line | Demonstrate how to interact with Firmware Upgrade Service using FUS commands in order to delete and upgrade the current Wireless Stack, switch between FUS and Wireless Stack. | |
Bluetooth® LE Features | Privacy | Demonstrate advertising with a Resolvable Private Address |
Connection Oriented Channel | allow to exchange data at L2CAP level without GATT layer | |
Bluetooth® LE Demonstration | Multi-links Connection | Demonstrate multilink communication between a STM32WB5MM-DK board and up to 8 smartphones |
MIDI Player | Apple MIDI over BLE | |
Interoperability Program | Verify BLE behavior different smartphone | |
AI Motion Sense | Motion sensing application to recognize human activities using machine learning | |
Motor Control | Wireless moteur remote control with X-CUBE-MCSDK v5 | |
HID Selfie | This application is designed to help you send keycodes for both generic and multimedia keyboards to your device |
4. References