This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1 Delta between 1.11.0 and 1.11.2
ID | Summary |
---|---|
140972 | STM32CubeIDE installations were corrupted when using the Eclipse Marketplace, the Toolchain Manager, and downloading OpenSTLinux packages. This patch v1.11.2 fixes this issue. |
140569 | With STM32CubeIDE v1.11.0, some code about the FreeRTOS™ support was removed for the STM32F4. This patch v1.11.2 fixes this issue. |
2 Fixed issues
ID | Summary |
---|---|
73456 74149 |
Fixed issue with SFR view – incorrect values during search and filters will show child nodes. |
85064 | Some macOS® versions report installation image corruption or that the image cannot be opened because the developer cannot be verified. The work-around is to execute the following command:
xattr -c /Applications/STM32CubeIDE.app |
123405 | Fixed issue with SWV bandwidth performance with ST-LINK GDB server. |
124770 | There are multiple CM0+ pre-compiled stacks with different memory size requirements. It is consequently up to the user to update the linker script to reflect the memory split between the CM4 and CM0+ core. |
130208 | Fixed issues with selecting text in Linker script editor and solved dark theme issues. |
131836 | ST-LINK GDB server can now abort debug launch when STM32CubeProgrammer fails to perform the flash download. |
134020 | RAM linker script for STM32H7B0xB device has only 128K RAM. |
134147 | ST-LINK GDB server dead-lock in persistent mode after a few GDB-client connections. |
134674 | The Build Analyzer "Memory Regions"-tab has an error in the "End Address" column. |
135591 | OpenOCD – Shared ST-LINK option persistent when switching script generation method. |
136427 | Fixed the issue with SWV ITM Console going black. |
3 Known issues
The known issues are split into general, OS-specific, and target-specific issues.
3.1 General issues
ID | Summary |
---|---|
59435 | Having a space or non-ASCII character in the project/workspace path or installation path is not fully supported. |
63624 | Some STM32CubeMX pop-up dialogs are not opened in front of the STM32CubeIDE workbench on all OS's. |
68184 | Hierarchical projects cannot be imported with the option Copy into workspace. |
68440 | Hierarchical projects cannot be renamed. |
89454 | Restart configuration only works for flash memory projects and not for RAM projects. Program Counter register is not set correctly. Manual work-around: In Restart configuration, manually set PC to the ResetHandler() in RAM: set $pc = 0x20000xxx. |
109764 | FreeRTOS™ kernel-aware debugging: Full stack traces off all tasks do not work if configUSE_PORT_OPTIMISED_TASK_SELECTION 1 |
115928 | Editing live expressions while target is running does not work with SEGGER J-Link. |
124062 | GCC-10 is more strict with respect to declaration of global variables in header files. Read the GCC-10 porting guide. |
133183 | STM32CubeIDE cannot debug using FreeRTOS aware with J-LINK.
Work-arounds, if: Reset strategy == Connect under reset, requires Initialization commands: info threads info threads thread 2 Work-arounds, if: Reset strategy == None (attach mode), requires Initialization commands: info threads info threads thread 2 stepi |
3.2 OS-specific issues
3.2.1 Linux®
ID | Summary |
---|---|
139617 | The CAD view in the ioc-editor may not render. A restart of STM32CubeIDE is required. |
3.3 Target-specific issues
3.3.1 STM32H7
ID | Summary |
---|---|
73552 | Serial Wire Viewer configuration is not reset for STM32H7 devices on the next launch if it was terminated with record active when using ST-LINK GDB server. |
79658 | ST-LINK GDB server reports being suspended on address: 0x05F0001 when debugging STM32H7 dual-core devices and the core under debug goes to sleep. |
81763 | OpenOCD does not support debugging STM32H7 dual-core devices when the core under debug goes to sleep. |
3.3.2 STM32MP1
ID | Summary |
---|---|
73895 | Debugging in production mode requires a network connection. If STM32CubeIDE is configured to use a network proxy, then the IP address of the STM32MP1 board needs to be added to the "Proxy bypass" list. |
73896 | The synchronization check between the IP-address entered in launch configuration and the IP-address of the target does not abort the launch in case of mismatch. |