This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies."Display units" is a declarative predefined property to define units of display for numeric typed properties and is provided by Semantic MediaWiki. A comma-separated list allows to describe units or formats to be used for the display. This property is pre-deployed (also known as special property) and comes with additional administrative privileges but can be used just like any other user-defined property.