Approved version. Approved on: 16:26, 12 October 2021
Difference between revisions of "Yavta"
[unchecked revision] | [quality revision] |
m
|
m
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
1 Overview[edit]
Yavta stands for "Yet Another V4L2 Test Application". This is a test application based on V4L2 Linux® kernel interface that allows testing, debugging and controlling camera subsystem.
![]() |
Yavta is only available in STM32MP1 Distribution Package weston image |
2 How to use Yavta[edit]
/usr/sbin # yavta --help Usage: yavta [options] device Supported options: -c, --capture[=nframes] Capture frames -C, --check-overrun Verify dequeued frames for buffer overrun -d, --delay Delay (in ms) before requeuing buffers -D, --display Display frames -f, --format format Set the video format -F, --file[=name] Read/write frames from/to disk For video capture devices, the first '#' character in the file name is expanded to the frame sequence number. The default file name is 'frame-#.bin'. -h, --help Show this help screen -i, --input input Select the video input -I, --fill-frames Fill frames with check pattern before queuing them -l, --list-controls List available controls -n, --nbufs n Set the number of video buffers -p, --pause Pause before starting the video stream -q, --quality n MJPEG quality (0-100) -r, --get-control ctrl Get control 'ctrl' -R, --realtime=[priority] Enable realtime RR scheduling -s, --size WxH Set the frame size -t, --time-per-frame num/denom Set the time per frame (eg. 1/25 = 25 fps) -u, --userptr Use the user pointers streaming method -w, --set-control 'ctrl value' Set control 'ctrl' to 'value' --enum-formats Enumerate formats --enum-inputs Enumerate inputs --no-query Don't query capabilities on open --offset User pointer buffer offset from page start --requeue-last Requeue the last buffers before streamoff --skip n Skip the first n frames --sleep-forever Sleep forever after configuring the device --stride value Line stride in bytes
3 Examples[edit]
- Getting supported controls/formats/resolutions:
yavta -l --enum-formats --enum-inputs /dev/video0
Device /dev/video0 opened. Device `STM32 Camera Memory Interface' on `platform:dcmi' is a video capture device. --- Image Processing Controls (class 0x009f0001) --- control 0x009f0903 `Test Pattern' min 0 max 1 step 1 default 0 current 1. 1 control found. - Available formats: Format 0: RGB565 (50424752) Type: Video capture (1) Name: 16-bit RGB 5-6-5 Frame size: 640x480 () Frame size: 320x240 () Frame size: 160x120 () - Available inputs: Input 0: Camera. Video format: RGB565 (50424752) 160x120 (stride 320) buffer size 38400
- Capturing 10 frames on the disk (default format/resolution):
yavta -F /dev/video0 --capture=10
/usr/sbin # yavta -F /dev/video0 --capture=10 Device /dev/video0 opened. Device `STM32 Camera Memory Interface' on `platform:dcmi' is a video capture device. Video format: RGB565 (50424752) 160x120 (stride 320) buffer size 38400 8 buffers requested. length: 38400 offset: 0 Buffer 0 mapped at address 0xc0710000. length: 38400 offset: 40960 Buffer 1 mapped at address 0xc0720000. length: 38400 offset: 81920 Buffer 2 mapped at address 0xc0730000. length: 38400 offset: 122880 Buffer 3 mapped at address 0xc0740000. length: 38400 offset: 163840 Buffer 4 mapped at address 0xc0750000. length: 38400 offset: 204800 Buffer 5 mapped at address 0xc0760000. length: 38400 offset: 245760 Buffer 6 mapped at address 0xc0770000. length: 38400 offset: 286720 Buffer 7 mapped at address 0xc0780000. 0 (0) [-] 0 38400 bytes 1378.374325 1378.374535 17.819 fps 1 (1) [-] 1 38400 bytes 1378.407623 1378.407822 30.032 fps 2 (2) [-] 2 38400 bytes 1378.440939 1378.441111 30.016 fps 3 (3) [-] 3 38400 bytes 1378.474288 1378.474450 29.986 fps 4 (4) [-] 4 38400 bytes 1378.507624 1378.507827 29.998 fps 5 (5) [-] 5 38400 bytes 1378.540989 1378.541196 29.972 fps 6 (6) [-] 6 38400 bytes 1378.574288 1378.574489 30.031 fps 7 (7) [-] 7 38400 bytes 1378.607624 1378.607827 29.998 fps 8 (0) [-] 8 38400 bytes 1378.640959 1378.641162 29.999 fps 9 (1) [-] 9 38400 bytes 1378.674288 1378.674488 30.004 fps Captured 10 frames in 0.356282 seconds (28.067590 fps, 1077795.461669 B/s).
<noinclude>{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x, STM32MP15x }}</noinclude> == Overview == {{highlight|'''Yavta'''}} stands for "Yet Another V4L2 Test Application". This is a test application based on V4L2 Linux<sup>®</sup> kernel interface that allows testing, debugging and controlling camera subsystem. {{Warning|Yavta is only available in [[STM32MP1_Distribution_Package | STM32MP1 Distribution Package weston image]]}} ==How to use Yavta==<pre> /usr/sbin # yavta --help Usage: yavta [options] device Supported options: -c, --capture[=nframes] Capture frames -C, --check-overrun Verify dequeued frames for buffer overrun -d, --delay Delay (in ms) before requeuing buffers -D, --display Display frames -f, --format format Set the video format -F, --file[=name] Read/write frames from/to disk For video capture devices, the first '#' character in the file name is expanded to the frame sequence number. The default file name is 'frame-#.bin'. -h, --help Show this help screen -i, --input input Select the video input -I, --fill-frames Fill frames with check pattern before queuing them -l, --list-controls List available controls -n, --nbufs n Set the number of video buffers -p, --pause Pause before starting the video stream -q, --quality n MJPEG quality (0-100) -r, --get-control ctrl Get control 'ctrl' -R, --realtime=[priority] Enable realtime RR scheduling -s, --size WxH Set the frame size -t, --time-per-frame num/denom Set the time per frame (eg. 1/25 = 25 fps) -u, --userptr Use the user pointers streaming method -w, --set-control 'ctrl value' Set control 'ctrl' to 'value' --enum-formats Enumerate formats --enum-inputs Enumerate inputs --no-query Don't query capabilities on open --offset User pointer buffer offset from page start --requeue-last Requeue the last buffers before streamoff --skip n Skip the first n frames --sleep-forever Sleep forever after configuring the device --stride value Line stride in bytes</pre> ==Examples== * Getting supported controls/formats/resolutions: yavta -l --enum-formats --enum-inputs /dev/video0<pre> Device /dev/video0 opened. Device `STM32 Camera Memory Interface' on `platform:dcmi' is a video capture device. --- Image Processing Controls (class 0x009f0001) --- control 0x009f0903 `Test Pattern' min 0 max 1 step 1 default 0 current 1. 1 control found. - Available formats: Format 0: RGB565 (50424752) Type: Video capture (1) Name: 16-bit RGB 5-6-5 Frame size: 640x480 () Frame size: 320x240 () Frame size: 160x120 () - Available inputs: Input 0: Camera. Video format: RGB565 (50424752) 160x120 (stride 320) buffer size 38400</pre> * Capturing 10 frames on the disk (default format/resolution): yavta -F /dev/video0 --capture=10<pre> /usr/sbin # yavta -F /dev/video0 --capture=10 Device /dev/video0 opened. Device `STM32 Camera Memory Interface' on `platform:dcmi' is a video capture device. Video format: RGB565 (50424752) 160x120 (stride 320) buffer size 38400 8 buffers requested. length: 38400 offset: 0 Buffer 0 mapped at address 0xc0710000. length: 38400 offset: 40960 Buffer 1 mapped at address 0xc0720000. length: 38400 offset: 81920 Buffer 2 mapped at address 0xc0730000. length: 38400 offset: 122880 Buffer 3 mapped at address 0xc0740000. length: 38400 offset: 163840 Buffer 4 mapped at address 0xc0750000. length: 38400 offset: 204800 Buffer 5 mapped at address 0xc0760000. length: 38400 offset: 245760 Buffer 6 mapped at address 0xc0770000. length: 38400 offset: 286720 Buffer 7 mapped at address 0xc0780000. 0 (0) [-] 0 38400 bytes 1378.374325 1378.374535 17.819 fps 1 (1) [-] 1 38400 bytes 1378.407623 1378.407822 30.032 fps 2 (2) [-] 2 38400 bytes 1378.440939 1378.441111 30.016 fps 3 (3) [-] 3 38400 bytes 1378.474288 1378.474450 29.986 fps 4 (4) [-] 4 38400 bytes 1378.507624 1378.507827 29.998 fps 5 (5) [-] 5 38400 bytes 1378.540989 1378.541196 29.972 fps 6 (6) [-] 6 38400 bytes 1378.574288 1378.574489 30.031 fps 7 (7) [-] 7 38400 bytes 1378.607624 1378.607827 29.998 fps 8 (0) [-] 8 38400 bytes 1378.640959 1378.641162 29.999 fps 9 (1) [-] 9 38400 bytes 1378.674288 1378.674488 30.004 fps Captured 10 frames in 0.356282 seconds (28.067590 fps, 1077795.461669 B/s).</pre> <noinclude> {{PublicationRequestId | 7662 | 2018-06-13 | AnneJ}} [[Category:V4L2]]</noinclude>
Line 1: | Line 1: | ||
− | {{ApplicableFor |
+ |
<noinclude>{{ApplicableFor |
|MPUs list=STM32MP13x, STM32MP15x |
|MPUs list=STM32MP13x, STM32MP15x |
||
− | |MPUs checklist=STM32MP13x, STM32MP15x |
+ | |MPUs checklist=STM32MP13x,STM32MP15x |
− | }} |
+ | }}</noinclude>
|
== Overview == |
== Overview == |
||
{{highlight|'''Yavta'''}} stands for "Yet Another V4L2 Test Application". This is a test application based on V4L2 Linux<sup>®</sup> kernel interface that allows testing, debugging and controlling camera subsystem. |
{{highlight|'''Yavta'''}} stands for "Yet Another V4L2 Test Application". This is a test application based on V4L2 Linux<sup>®</sup> kernel interface that allows testing, debugging and controlling camera subsystem. |
Retrieved from "https://wiki.st.com/stm32mpu/index.php?title=Yavta&oldid=79567"