Last edited 3 months ago

X-LINUX-TPM expansion package

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP25x lines

This version of X-LINUX-TPM expansion package is validated against the ecosystem release v6.0.0 More info.png

1. Article purpose

This article explains how to integrate the STPM4RasPI or STPM4RasPIV21 expansion boards with the STM32MP157F-DK2 Discovery kit More info green.png, STM32MP135F-DK Discovery kit More info green.png, or STM32MP257F-EV1 Evaluation board More info green.png. The X-LINUX-TPM OpenSTLinux expansion package provides the software add-ons for this integration. A signature verification use case is included to verify the TPM integration.
Multiple services are available using TPM (mostly on PC and mobile devices):

  • Generation, protection, management, and use of cryptographic keys
  • Cryptographic device identity
  • Secure logging, log reporting, and certification or authentication
  • Secure non-volatile storage
  • Other functions including hashing, random number generation, and secure clock

Several use cases are available:

  • Platform integrity: The boot process relies on TPM for software integrity and authentication during each boot stage
  • Disk encryption: Drive encryption and decryption using the TPM crypto core
  • Password protection and others

The use case described in this article uses the cryptographic key generation functionality on the TPM.

2. Prerequisites

2.1. Hardware prerequisites

  • STM32MP157F-DK2 Discovery kit More info green.png, STM32MP135F-DK Discovery kit More info green.png, or STM32MP257F-EV1 Evaluation board More info green.png

For more information on the STM32 discovery or evaluation boards and how to start them up, refer to the sections Getting started with STM32MP157x-DK2, Getting started with STM32MP135x-DK, Getting started with STM32MP257x-EV1 or Getting started with STM32MP257x-DK.

STM32MP157F-DK2
STM32MP135F-DK
STM32MP257F-EV1
STM32MP257F-DK


  • STPM4RasPI extension board[1]
STPM4RasPi.png
  • STPM4RasPIV21 extension board[2]
Tpm v2.png

STPM4RasPI and STPM4RasPIV21 are extension boards to connect STSAFE-TPM products to the STM32 microprocessor development kits such as STM32MP157F-DK2 or STM32MP135F-DK. The boards are designed for product evaluation, use case development, and integration activities. The boards are shipped with one trusted platform module soldered.

2.2. Software prerequisites

  • Get the OpenSTLinux ecosystem release v6.0.0 More info.png (steps described in the article above).

3. Hardware setup

Each discovery boards and evaluation boards offer a 40-pin connector, also called a Raspberry Pi® connector. To setup your hardware, plug the STPM4RasPI or STPM4RasPIV21 extension board on this connector (the small "1" marking indicates the correct orientation of the connector).

Warning DB.png Important
  • Warning: You risk damaging the STPM4RasPI or STPM4RasPIV21 extension board if you do not connect it to the Raspberry Pi connector as described above.

4. Software setup

X-LINUX-TPM is an STM32 MPU OpenSTLinux expansion package that aims to bring the support of STPM4RasPI[3] expansion board into the OpenSTLinux distribution.

This package is provided as a Yocto meta-layer and can be applied directly in the OpenSTLinux distribution.

TPM Expansion Package In STM32MPU Embedded Software.png
Info white.png Information
This version is compatible with the Yocto Project® build system Scarthgap. It is validated against the OpenSTLinux ecosystem release v6.0.0 More info.png on the following boards:
  • STM32MP157F-DK2 More info green.png
  • STM32MP135F-DK More info green.png
  • STM32MP257F-EV1 More info green.png
  • STM32MP257F-DK More info green.png

4.1. Main software modification

Through the Yocto-meta layer delivered by this package, changes are applied to the OpenSTLinux distribution mainly at two levels:

  • The Linux® kernel: at kernel configuration and device tree level.
  • User space: by providing the necessary libraries and tools to use the TPM extension board features.

4.1.1. Linux kernel configuration

To activate and use the right TPM SPI and I2C drivers, X-LINUX-TPM changes the Linux kernel configuration as follows:

CONFIG_TCG_TPM=y
CONFIG_TCG_TIS=y
CONFIG_TCG_TIS_SPI=y
CONFIG_TCG_TIS_I2C=y
CONFIG_CRC_CCITT=y

4.1.2. Linux kernel board device trees

On discovery boards mentioned in this article, both Raspberry PI connectors are linked with SPI5 provided by the STM32 device. This is the SPI instance that is used to access TPM features.
In the same way, some other TPM chips are controlled via the I2C interface. In this situation, the I2C5 instance is used on the Raspberry PI connector.

Note that some TPM devices can support both the SPI and I2C interfaces.

Therefore, the board device trees are patched into the X-LINUX-TPM to get the following SPI and I2C nodes:

  • arch/arm/boot/dts/st/stm32mp157f-dk2.dts Device Tree Source file:
&spi5{
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&spi5_pins_a>;
	pinctrl-1 = <&spi5_sleep_pins_a>;
	cs-gpios = <&gpiof 6 0>;
	status = "okay";

	st33htpm0: st33htpm@0{
		status="okay";
		compatible = "st,st33htpm-spi";
		#address-cells = <1>;
		#size-cells = <0>;
		reg = <0>; /* CS #0 */
		spi-max-frequency = <10000000>;
	};
}; 
&i2c5 {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&i2c5_pins_a>;
	pinctrl-1 = <&i2c5_sleep_pins_a>;
	i2c-scl-rising-time-ns = <185>;
	i2c-scl-falling-time-ns = <20>;
	clock-frequency = <400000>;
	/* spare dmas for other usage */
	/delete-property/dmas;
	/delete-property/dma-names;
	status = "okay";

	st33htpi: st33htpi@0{
		compatible = "infineon,slb9673", "tcg,tpm-tis-i2c";
		reg = <0x2e>;
		status="okay";
	};
};
  • arch/arm/boot/dts/st/stm32mp135f-dk.dts Device Tree Source file:
&spi5{
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&spi5_pins_a>;
	pinctrl-1 = <&spi5_sleep_pins_a>;
	cs-gpios = <&gpioh 11 0>;
	status = "okay";

	st33htpm0: st33htpm@0{
		status="okay";
		compatible = "st,st33htpm-spi";
		#address-cells = <1>;
		#size-cells = <0>;
		reg = <0>; /* CS #0 */
		spi-max-frequency = <10000000>;
	};
}; 
&i2c5 {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&i2c5_pins_a>;
	pinctrl-1 = <&i2c5_sleep_pins_a>;
	i2c-scl-rising-time-ns = <170>;
	i2c-scl-falling-time-ns = <5>;
	clock-frequency = <400000>;
	status = "okay";
	/* spare dmas for other usage */
	/delete-property/dmas;
	/delete-property/dma-names;

	st33htpi: st33htpi@0{
		compatible = "infineon,slb9673", "tcg,tpm-tis-i2c";
		reg = <0x2e>;
		status="okay";
	};
};
  • arch/arm64/boot/dts/st/stm32mp257f-ev1.dts Device Tree Source file:
&spi3 {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&spi3_pins_a>;
	pinctrl-1 = <&spi3_sleep_pins_a>;
	status = "okay";

	cs-gpios =  <&gpiob 1 0>;

	st33htpm0: st33htpm@0{
		status="okay";
		compatible = "st,st33htpm-spi";
		#address-cells = <1>;
		#size-cells = <0>;
		reg = <0>; /* CS #0 */
		spi-max-frequency = <10000000>;
	};
};
&i2c8 {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&i2c8_pins_a>;
	pinctrl-1 = <&i2c8_sleep_pins_a>;
	i2c-scl-rising-time-ns = <57>;
	i2c-scl-falling-time-ns = <7>;
	clock-frequency = <400000>;
	status = "okay";
	/* spare dmas for other usage */
	/delete-property/dmas;
	/delete-property/dma-names;

	st33htpi: st33htpi@0{
		compatible = "infineon,slb9673", "tcg,tpm-tis-i2c";
		reg = <0x2e>;
		status="okay";
	};
};

The cs-gpios property for SPI is schematics-dependent as it must target the SPI5_NSS pin. Other SPI5 pins are defined by pinctrl nodes.

The reg property for I2C represents the I2C address of the TPM device.

4.1.3. User space additional stacks

The X-LINUX-TPM package provides the TPM2 software stack (TSS) [4] into the OpenSTLinux distribution. It deals with TSS libraries as well as tpm2-tools. The latter are used to handle the TPM. The diagram below gives an overview of the software architecture, in the context of such an SPI-controlled device.

TSS2 tpm.png

4.2. How to build the OpenSTLinux distribution with X-LINUX-TPM

With the following procedure, the complete distribution is regenerated by enabling the X-LINUX-TPM expansion package.

4.2.1. Download the STM32MPU Distribution Package

For ecosystem release v6.0.0 More info.png :
Install the STM32MPU Distribution Package.

4.2.2. Install the X-LINUX-TPM environment

  • Add the Yocto Layer meta-security into your environment (it provides TPM2 recipes):
cd <Distribution Package installation directory>/layers
git clone https://git.yoctoproject.org/meta-security -b scarthgap
cd ..
  • Clone the meta-st-x-linux-tpm git repository:
cd <Distribution Package installation directory>/layers/meta-st
git clone -b yocto/scarthgap https://github.com/STMicroelectronics/meta-st-x-linux-tpm.git
cd ../..
  • Source the build environment (MACHINE value depends on the series you use):
DISTRO=openstlinux-weston MACHINE=<stm32mpX> source layers/meta-st/scripts/envsetup.sh
bitbake-layers add-layer ../layers/meta-st/meta-st-x-linux-tpm

4.2.3. Build the image

bitbake st-image-weston
Info white.png Information
Note that building the image might take a long time depending on the host computer performance.

4.2.4. Program the built image into the flash memory

Follow this link to see how to program the built image.

4.3. How to validate the proper behavior of X-LINUX-TPM

You can find below some ways of checking that the TPM2 features are working properly.

4.3.1. Driver load checking

When the TPM driver is loaded, /dev/tpm0 and /dev/tpmrm0 are present, as shown in the example below.

dmesg | grep tpm
[    1.525447] tpm_tis_spi spi0.0: 2.0 TPM (device-id 0x0, rev-id 78)
ls -l /dev | grep tpm
crw------- 1 tss  tss    10,   224 Oct 11 15:27 tpm0
crw------- 1 root root  253, 65536 Oct 11 15:27 tpmrm0

4.3.2. Simple TPM tool command checking

If the driver is loaded successfully, you can test it by running a simple 'tpm2' command in the Linux kernel console:

tpm2_getrandom --hex 20

If no error is raised, it means that the STM32 device is communicating properly with the STPM4RasPI or STPM4RasPIV21 extension board.

5. How to run a signature use case with X-LINUX-TPM

This is an example showing how to use the TPM to perform the signature of a file "msg.txt" hash (digest). A verification is done with the openssl "dgst -verify" command.

Message creation example:

echo dzeydezyetrefygzuedghdgie > msg.txt

Primary key creation:

tpm2_createprimary -C o -c pri.txt

Signature key creation:

tpm2_create -C pri.txt -g sha256 -G rsa -u kpub.bin -r kpriv.bin

Loading of the created signature key in TPM:

tpm2_load -u kpub.bin -r kpriv.bin -C pri.txt -c key.txt

Signature of the hash with the TPM signed key:

tpm2_sign -c key.txt -g sha256 -f plain -o hash.plain msg.txt

Read of the public part of the TPM signing key:

tpm2_readpublic -c key.txt -f der -o key_sig_pub.der

Verification with openssl dgst:

openssl dgst -verify key_sig_pub.der -keyform der -sha256 -signature hash.plain msg.txt

6. References