Difference between revisions of "X-LINUX-AI - object detection using TensorFlow Lite C++ API"

[quality revision] [quality revision]
m
m
Applicable for STM32MP13x lines, STM32MP15x lines

This article explains how to experiment TensorFlow Lite[1] applications for object detection based on the COCO SSD MobileNet v1 model using the TensorFlow Lite C++ API.

1 Description[edit]

The object detection[2] neural network model allows identification and localization of a known object within an image.

C/C++ TensorFlow Lite object detection application
C/C++ TensorFlow Lite object detection application

The application demonstrates a computer vision use case for object detection where frames are grabbed from a camera input (/dev/videox) and analyzed by a neural network model interpreted by the TensorFlow Lite[1] framework.
A Gstreamer pipeline is used to stream camera frames (using v4l2src), to display a preview (using waylandsink) and to execute a neural network inference (using appsink).
The result of the inference is displayed on the preview. The overlay is done using GtkWidget with cairo.
This combination is quite simple and efficient in terms of CPU overhead.

The model used with this application is the COCO SSD MobileNet v1 downloaded from downloaded from the object detection overview[2].

2 Installation[edit]

2.1 Install from the OpenSTLinux AI package repository[edit]

Warning white.png Warning
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.

After having configured the AI OpenSTLinux package you can install X-LINUX-AI components for this application:

 apt-get install tflite-cv-apps-object-detection-c++

Then restart the demo launcher:

- For OpenSTLinux distribution with a version lower than 4.0 use

 systemctl restart weston@root

- For other OpenSTLinux distribution use :

 systemctl restart weston-launch

2.2 Source code location[edit]

  • in the Openembedded OpenSTLinux Distribution:
<Distribution Package installation directory>/layers/meta-st/meta-st-stm32mpu-ai/recipes-samples/tflite-cv-apps/files/object-detection/src
  • on GitHub:
https://github.com/STMicroelectronics/meta-st-stm32mpu-ai/tree/dunfellv2.2.0/recipes-samples/tflite-cv-apps/files/object-detection/src

2.3 Re-generate the package from OpenSTLinux Distribution (optional)[edit]

Using the Openembedded OpenSTLinux distribution, you are able to rebuild the application.

Info white.png Information
If not already installed, the X-LINUX-AI OpenSTLinux Distribution need to be installed by following this link


  • Set up the build environment:
 cd <Distribution Package installation directory>
 source layers/meta-st/scripts/envsetup.sh
  • Rebuild the application:
 bitbake tflite-cv-apps-object-detection-c++ -c compile

The generated binary is available here:

<Distribution Package installation directory>/<build directory>/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/tflite-cv-apps-object-detection-c++/12.0.0-r0/tflite-cv-apps-object-detection-c++-12.0.0/object-detection/src/

3 How to use the application[edit]

3.1 Launching via the demo launcher[edit]

Launch cpp tfl object detection.png
Demo launcher

3.2 Executing with the command line[edit]

The objdetect_tfl_gst_gtk C/C++ application is located in the userfs partition:

/usr/local/demo-ai/computer-vision/tflite-object-detection/bin/objdetect_tfl_gst_gtk

It accepts the following input parameters:

Usage: ./objdetect_tfl_gst_gtk -m <model .tflite> -l <label .txt file>

                                                              
                                                                                                                                      
-m --model_file <.tflite file path>:  .tflite model to be executed
                                                                   
-l --label_file <label file path>:    name of file containing labels
                                                                 
-i --image <directory path>:          image directory with image to be classified
                                                    
-v --video_device <n>:                video device (default /dev/video0)
                                                             
--crop:                               if set, the nn input image is cropped (with the expected nn aspect ratio) before being resized,
                                       else the nn imputinput image is only resized to the nn input size (could cause picture deformation).

--frame_width  <val>:                 width of the camera frame (default is 640)
                                                     
--frame_height <val>:                 height of the camera frame (default is 480)
                                                    
--framerate <val>:                    framerate of the camera (default is 15fps)
                                                     
--input_mean <val>:                   model input mean (default is 127.5)
--input_std  <val>:                   model input standard deviation (default is 127.5)
--verbose:                            enable verbose mode
 
--input_std  <val>validation:                   model input standard deviation (default is 127.5)enable the validation mode
-t --threshold <val>:                 threshold of accuracy above which the boxes are displayed (default               
0.60)
--help:                               show this help

3.3 Testing with COCO SSD MobileNet V1[edit]

The model used for test is the detect.tflite downloaded from object detection overview[2]

Info white.png Information
The different objects the neural network is able to detect are listed in the labels.txt file located in the target:

/usr/local/demo-ai/computer-vision/models/coco_ssd_mobilenet/labels.txt


To ease launching of the application, two shell scripts are available:

  • launch object detection based on camera frame inputs
 /usr/local/demo-ai/computer-vision/tflite-object-detection/bin/launch_bin_objdetect_tfl_coco_ssd_mobilenet.sh
  • launch object detection based on the pictures located in /usr/local/demo-ai/computer-vision/models/mobilenet/testdata directory
 /usr/local/demo-ai/computer-vision/tflite-object-detection/bin/launch_bin_objdetect_tfl_coco_ssd_mobilenet_testdata.sh
Info white.png Information
Note that you need to populate the testdata directory with your own data sets.

The pictures are then randomly read from the testdata directory

4 References[edit]


<noinclude>{{ApplicableFor
|MPUs list=STM32MP13x, STM32MP15x
|MPUs checklist=STM32MP13x,STM32MP15x
}}</noinclude>
This article explains how to experiment {{Highlight|TensorFlow Lite<ref name=tensorflowlite_url>[https://www.tensorflow.org/lite TensorFlow Lite]</ref>}} applications for object detection based on the COCO SSD MobileNet v1 model using the TensorFlow Lite C++ API.

==Description==
The '''object detection'''<ref name=tflite_obj_detect_url>[https://www.tensorflow.org/lite/modelsexamples/object_detection/overview TFLite object detection overview]</ref> neural network model allows identification and localization of a known object within an image.
<div class="res-img">
[[File: cpp_tfl_object_detection_application_screenshot.png|thumb|upright=2|center|link=|center|C/C++ TensorFlow Lite object detection application]]
</div>

The application demonstrates a computer vision use case for object detection where frames are grabbed from a camera input (/dev/videox) and analyzed by a neural network model interpreted by the {{Highlight|TensorFlow Lite<ref name=tensorflowlite_url></ref>}} framework.<br>

A Gstreamer pipeline is used to stream camera frames (using v4l2src), to display a preview (using waylandsink) and to execute a neural network inference (using appsink).<br>

The result of the inference is displayed on the preview. The overlay is done using GtkWidget with cairo.<br>

This combination is quite simple and efficient in terms of CPU overhead.<br>


The model used with this application is the {{Highlight|COCO SSD MobileNet v1}} downloaded from downloaded from the '''object detection overview'''<ref name=tflite_obj_detect_url>[https://www.tensorflow.org/lite/modelsexamples/object_detection/overview TFLite object detection overview]</ref>.

==Installation==
===Install from the OpenSTLinux AI package repository===
{{Warning|{{SoftwareLicenseAgreement | distribution=X-LINUX-AI}}}}
After having [[X-LINUX-AI_OpenSTLinux_Expansion_Package#Configure the AI OpenSTLinux package repository|configured the AI OpenSTLinux package]] you can install X-LINUX-AI components for this application:
 {{Board$}} apt-get install tflite-cv-apps-object-detection-c++
Then restart the demo launcher:
- For OpenSTLinux distribution with a version lower than 4.0 use  {{Board$}} systemctl restart weston@root
- For other OpenSTLinux distribution use :
 {{Board$}} systemctl restart weston-launch
===Source code location===
* in the Openembedded OpenSTLinux Distribution:
:'''<Distribution Package installation directory>/layers/meta-st/meta-st-stm32mpu-ai/recipes-samples/tflite-cv-apps/files/object-detection/src'''
* on GitHub:
:https://github.com/STMicroelectronics/meta-st-stm32mpu-ai/tree/dunfellv2.2.0/recipes-samples/tflite-cv-apps/files/object-detection/src

===Re-generate the package from OpenSTLinux Distribution (optional)===
Using the Openembedded OpenSTLinux distribution, you are able to rebuild the application.

{{Info|If not already installed, the X-LINUX-AI OpenSTLinux Distribution need to be installed by following this [[X-LINUX-AI_OpenSTLinux_Expansion_Package#Re-generate_X-LINUX-AI_OpenSTLinux_distribution|link]]}}

* Set up the build environment:
 {{PC$}} cd <Distribution Package installation directory>

 {{PC$}} source layers/meta-st/scripts/envsetup.sh
* Rebuild the application:
 {{PC$}} bitbake tflite-cv-apps-object-detection-c++ -c compile
The generated binary is available here:<Distribution Package installation directory>/<build directory>/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/tflite-cv-apps-object-detection-c++/12.0.0-r0/tflite-cv-apps-object-detection-c++-12.0.0/object-detection/src/

==How to use the application==
===Launching via the demo launcher===<div class="res-img">
[[File: launch_cpp_tfl_object_detection.png|thumb|upright=2|center|link=]]
center|550px|Demo launcher]]</div>

===Executing with the command line===
The '''objdetect_tfl_gst_gtk''' C/C++ application is located in the userfs partition:
 /usr/local/demo-ai/computer-vision/tflite-object-detection/bin/objdetect_tfl_gst_gtk
It accepts the following input parameters:
<pre>

Usage: ./objdetect_tfl_gst_gtk -m <model .tflite> -l <label .txt file>

                                                              

-m --model_file <.tflite file path>:  .tflite model to be executed                                                                   
-l --label_file <label file path>:    name of file containing labels                                                                 
-i --image <directory path>:          image directory with image to be classified                                                    
-v --video_device <n>:                video device (default /dev/video0)                                                             
--crop:                               if set, the nn input image is cropped (with the expected nn aspect ratio) before being resized, else the nn imputinput image is only resized to the nn input size (could cause picture deformation).
--frame_width  <val>:                 width of the camera frame (default is 640)                                                     
--frame_height <val>:                 height of the camera frame (default is 480)                                                    
--framerate <val>:                    framerate of the camera (default is 15fps)                                                     
--input_mean <val>:                   model input mean (default is 127.5)                                                            

--input_std  <val>:                   model input standard deviation (default is 127.5)                                               --input_std  <val>:                   model input standard deviation (default is 127.5)
--verbose:                            enable verbose mode
--validation:                         enable the validation mode
-t --threshold <val>:                 threshold of accuracy above which the boxes are displayed (default 0.60)--help:                               show this help</pre>


===Testing with COCO SSD MobileNet V1===
The model used for test is the {{Highlight|detect.tflite}} downloaded from '''object detection overview'''<ref name=tflite_obj_detect_url>[https://www.tensorflow.org/lite/modelsexamples/object_detection/overview TFLite object detection overview]</ref>


{{Info|The different objects the neural network is able to detect are listed in the labels.txt file located in the target:
/usr/local/demo-ai/computer-vision/models/coco_ssd_mobilenet/labels.txt}}

To ease launching of the application, two shell scripts are available:
* launch object detection based on camera frame inputs
 {{Board$}} /usr/local/demo-ai/computer-vision/tflite-object-detection/bin/launch_bin_objdetect_tfl_coco_ssd_mobilenet.sh

*launch object detection based on the pictures located in '''/usr/local/demo-ai/computer-vision/models/mobilenet/testdata''' directory
 {{Board$}} /usr/local/demo-ai/computer-vision/tflite-object-detection/bin/launch_bin_objdetect_tfl_coco_ssd_mobilenet_testdata.sh

{{Info|Note that you need to populate the testdata directory with your own data sets.<br>

The pictures are then randomly read from the testdata directory}}

==References==<references />

<noinclude>

[[Category:Artificial intelligence sample apps|15]]
{{PublicationRequestId | 16541 | 24Jun'20}}</noinclude>
(6 intermediate revisions by 2 users not shown)
Line 1: Line 1:
  +
<noinclude>{{ApplicableFor
  +
|MPUs list=STM32MP13x, STM32MP15x
  +
|MPUs checklist=STM32MP13x,STM32MP15x
  +
}}</noinclude>
 
This article explains how to experiment {{Highlight|TensorFlow Lite<ref name=tensorflowlite_url>[https://www.tensorflow.org/lite TensorFlow Lite]</ref>}} applications for object detection based on the COCO SSD MobileNet v1 model using the TensorFlow Lite C++ API.
 
This article explains how to experiment {{Highlight|TensorFlow Lite<ref name=tensorflowlite_url>[https://www.tensorflow.org/lite TensorFlow Lite]</ref>}} applications for object detection based on the COCO SSD MobileNet v1 model using the TensorFlow Lite C++ API.
   
 
==Description==
 
==Description==
The '''object detection'''<ref name=tflite_obj_detect_url>[https://www.tensorflow.org/lite/models/object_detection/overview TFLite object detection overview]</ref> neural network model allows identification and localization of a known object within an image.
+
The '''object detection'''<ref name=tflite_obj_detect_url>[https://www.tensorflow.org/lite/examples/object_detection/overview TFLite object detection overview]</ref> neural network model allows identification and localization of a known object within an image.
   
[[File: cpp_tfl_object_detection_application_screenshot.png|thumb|upright=2|center|link=|C/C++ TensorFlow Lite object detection application]]
+
<div class="res-img">
  +
[[File: cpp_tfl_object_detection_application_screenshot.png|center|C/C++ TensorFlow Lite object detection application]]
  +
</div>
   
 
The application demonstrates a computer vision use case for object detection where frames are grabbed from a camera input (/dev/videox) and analyzed by a neural network model interpreted by the {{Highlight|TensorFlow Lite<ref name=tensorflowlite_url></ref>}} framework.<br>
 
The application demonstrates a computer vision use case for object detection where frames are grabbed from a camera input (/dev/videox) and analyzed by a neural network model interpreted by the {{Highlight|TensorFlow Lite<ref name=tensorflowlite_url></ref>}} framework.<br>
Line 11: Line 17:
 
This combination is quite simple and efficient in terms of CPU overhead.<br>
 
This combination is quite simple and efficient in terms of CPU overhead.<br>
   
The model used with this application is the {{Highlight|COCO SSD MobileNet v1}} downloaded from downloaded from the '''object detection overview'''<ref name=tflite_obj_detect_url>[https://www.tensorflow.org/lite/models/object_detection/overview TFLite object detection overview]</ref>.
+
The model used with this application is the {{Highlight|COCO SSD MobileNet v1}} downloaded from downloaded from the '''object detection overview'''<ref name=tflite_obj_detect_url>[https://www.tensorflow.org/lite/examples/object_detection/overview TFLite object detection overview]</ref>.
   
 
==Installation==
 
==Installation==
Line 18: Line 24:
 
After having [[X-LINUX-AI_OpenSTLinux_Expansion_Package#Configure the AI OpenSTLinux package repository|configured the AI OpenSTLinux package]] you can install X-LINUX-AI components for this application:
 
After having [[X-LINUX-AI_OpenSTLinux_Expansion_Package#Configure the AI OpenSTLinux package repository|configured the AI OpenSTLinux package]] you can install X-LINUX-AI components for this application:
 
  {{Board$}} apt-get install tflite-cv-apps-object-detection-c++
 
  {{Board$}} apt-get install tflite-cv-apps-object-detection-c++
  +
 
Then restart the demo launcher:
 
Then restart the demo launcher:
  +
  +
- For OpenSTLinux distribution with a version lower than 4.0 use 
 
  {{Board$}} systemctl restart weston@root
 
  {{Board$}} systemctl restart weston@root
  +
- For other OpenSTLinux distribution use :
  +
{{Board$}} systemctl restart weston-launch
   
 
===Source code location===
 
===Source code location===
Line 25: Line 36:
 
:'''<Distribution Package installation directory>/layers/meta-st/meta-st-stm32mpu-ai/recipes-samples/tflite-cv-apps/files/object-detection/src'''
 
:'''<Distribution Package installation directory>/layers/meta-st/meta-st-stm32mpu-ai/recipes-samples/tflite-cv-apps/files/object-detection/src'''
 
* on GitHub:
 
* on GitHub:
:https://github.com/STMicroelectronics/meta-st-stm32mpu-ai/tree/dunfell/recipes-samples/tflite-cv-apps/files/object-detection/src
+
:https://github.com/STMicroelectronics/meta-st-stm32mpu-ai/tree/v2.2.0/recipes-samples/tflite-cv-apps/files/object-detection/src
   
 
===Re-generate the package from OpenSTLinux Distribution (optional)===
 
===Re-generate the package from OpenSTLinux Distribution (optional)===
Line 39: Line 50:
 
  {{PC$}} bitbake tflite-cv-apps-object-detection-c++ -c compile
 
  {{PC$}} bitbake tflite-cv-apps-object-detection-c++ -c compile
 
The generated binary is available here:
 
The generated binary is available here:
  <Distribution Package installation directory>/<build directory>/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/tflite-cv-apps-object-detection-c++/1.0-r0/tflite-cv-apps-object-detection-c++-1.0/object-detection/src/
+
  <Distribution Package installation directory>/<build directory>/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/tflite-cv-apps-object-detection-c++/2.0.0-r0/tflite-cv-apps-object-detection-c++-2.0.0/object-detection/src/
   
 
==How to use the application==
 
==How to use the application==
 
===Launching via the demo launcher===
 
===Launching via the demo launcher===
[[File: launch_cpp_tfl_object_detection.png|thumb|upright=2|center|link=]]
+
<div class="res-img">
  +
[[File: launch_cpp_tfl_object_detection.png|center|550px|Demo launcher]]
  +
</div>
   
 
===Executing with the command line===
 
===Executing with the command line===
Line 51: Line 64:
   
 
<pre>
 
<pre>
Usage: ./objdetect_tfl_gst_gtk -m <model .tflite> -l <label .txt file>                                                              
+
Usage: ./objdetect_tfl_gst_gtk -m <model .tflite> -l <label .txt file>
                                                                                                                                     
+
 
-m --model_file <.tflite file path>:  .tflite model to be executed                                                                  
+
-m --model_file <.tflite file path>:  .tflite model to be executed
-l --label_file <label file path>:    name of file containing labels                                                                
+
-l --label_file <label file path>:    name of file containing labels
-i --image <directory path>:          image directory with image to be classified                                                    
+
-i --image <directory path>:          image directory with image to be classified
-v --video_device <n>:                video device (default /dev/video0)                                                            
+
-v --video_device <n>:                video device (default /dev/video0)
--crop:                              if set, the nn input image is cropped (with the expected nn aspect ratio) before being resized,  
+
--crop:                              if set, the nn input image is cropped (with the expected nn aspect ratio) before being resized,
                                       else the nn imput image is only resized to the nn input size (could cause picture deformation).  
+
                                       else the nn input image is only resized to the nn input size (could cause picture deformation).
--frame_width  <val>:                width of the camera frame (default is 640)                                                    
+
--frame_width  <val>:                width of the camera frame (default is 640)
--frame_height <val>:                height of the camera frame (default is 480)                                                    
+
--frame_height <val>:                height of the camera frame (default is 480)
--framerate <val>:                    framerate of the camera (default is 15fps)                                                    
+
--framerate <val>:                    framerate of the camera (default is 15fps)
--input_mean <val>:                  model input mean (default is 127.5)                                                            
+
--input_mean <val>:                  model input mean (default is 127.5)
--input_std  <val>:                  model input standard deviation (default is 127.5)                                              
+
--input_std  <val>:                  model input standard deviation (default is 127.5)
  +
--verbose:                            enable verbose mode
  +
--validation:                        enable the validation mode
  +
-t --threshold <val>:                threshold of accuracy above which the boxes are displayed (default 0.60)
 
--help:                              show this help
 
--help:                              show this help
 
</pre>
 
</pre>
   
 
===Testing with COCO SSD MobileNet V1===
 
===Testing with COCO SSD MobileNet V1===
The model used for test is the {{Highlight|detect.tflite}} downloaded from '''object detection overview'''<ref name=tflite_obj_detect_url>[https://www.tensorflow.org/lite/models/object_detection/overview TFLite object detection overview]</ref>
+
The model used for test is the {{Highlight|detect.tflite}} downloaded from '''object detection overview'''<ref name=tflite_obj_detect_url>[https://www.tensorflow.org/lite/examples/object_detection/overview TFLite object detection overview]</ref>
   
 
{{Info|The different objects the neural network is able to detect are listed in the labels.txt file located in the target:
 
{{Info|The different objects the neural network is able to detect are listed in the labels.txt file located in the target: