This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion
Weston is the reference implementation of a Wayland compositor.
The table below lists the actions that can be performed through Weston keyboard shortcuts, when the development board is connected to a keyboard.
It must be noted that:
- <modifier-key> in the table below corresponds to the key used for common bindings. It is defined by binding-modifier=<modifier-key> in the /etc/xdg/weston/weston.ini file. Possible values for <modifier-key> are:
- "super", i.e. Windows key between "ctrl" and "alt" (default Weston value)
- "ctrl" (default value in STMicroelectronics images)
- "alt"
- "none"
- The shortcuts are defined in desktop-shell/shell.c[1] file (shell_add_bindings() function)
- Some shortcuts require that both a keyboard and a mouse are connected to the development board
- Some shortcuts require that several workspaces are defined. The number of workspaces is defined by num-workspaces=<num-workspaces> in the /etc/xdg/weston/weston.ini file. The maximum number of workspaces is 6. If num-workspaces is not set, one single workspace is configured.
- The left mouse button allows the activation of a window.
Before proceeding, it is recommended to
- check the <modifier-key> value:
grep binding-modifier /etc/xdg/weston/weston.ini
binding-modifier=ctrl
- check the <num-workspaces> value:
grep num-workspaces /etc/xdg/weston/weston.ini
num-workspaces=6
Command | Action | Condition(s) |
---|---|---|
ctrl + alt + backspace | Kill Weston | Keyboard |
super + scroll | Zoom in / out the desktop | Keyboard + mouse |
super + alt + scroll | Change activated window opacity | Keyboard + mouse |
<modifier-key> + page up / page down | Zoom in / out the desktop | Keyboard |
<modifier-key> + shift + f | Put activated window fullscreen | Keyboard |
<modifier-key> + left mouse button | Move activated window | Keyboard + mouse |
<modifier-key> + middle mouse button | Rotate activated window | Keyboard + mouse |
<modifier-key> + right mouse button | Resize activated window | Keyboard + mouse |
<modifier-key> + shift + left mouse button | Resize activated window | Keyboard + mouse |
<modifier-key> + tab | Switch windows | Keyboard |
<modifier-key> + k | Kill activated window | Keyboard |
<modifier-key> + key up / key down | Switch to previous / next workspace | Keyboard + workspaces |
<modifier-key> + shift + key up / key down | Move activated window to previous / next workspace | Keyboard + workspaces |
<modifier-key> + Fn | Switch to workspace n | Keyboard + workspaces |
super + s | Capture a screenshot (see details below) | Keyboard |
super + r | Start / stop recording a screencast (see details below) | Keyboard |
Additional shortcuts can be found on internet.
1 Capturing a screenshot[edit source]
- Refer to the table above for the command to be used.
- The captured picture (PNG format) is automatically stored in /wayland-screenshot-2018-01-06_01-48-19.png.
- Copy the screenshot from the board to the host PC in the <file-path> directory (for example with the scp command).
scp root@<ip address>:/wayland-screenshot-*.png <file-path>/
Note: a screenshot capture is also named a snapshot or a screen capture.
2 Recording a screencast[edit source]
- Refer to the table above for the command to be used.
- The recorded screencast (WCAP format) is automatically stored in /capture.wcap. The WCAP format is a lossless video format specific to Weston (only the frame differences are recorded).
- To play the recorded screencast, convert it to a format that can be interpreted by any video player (e.g. VP8). Three steps are required:
- On the board, convert the WCAP file into a YUV file using wcap-decode:
wcap-decode capture.wcap --yuv4mpeg2 > capture.y4m
- Copy the YUV file from the board to the host PC in the <file-path> directory (for example with the scp command):
scp root@<ip address>:/capture.y4m <file-path>/
- On the host PC, transcode the YUV file to any other well-known format (e.g. VP8) using ffmpeg:
ffmpeg -i capture.y4m -c:v libvpx -b:v 1M capture.webm
- Optionally, choose a higher bitrate (-b:v 1M means a target bitrate of 1 MBit/s) if a better quality is required. Optionally, use the transpose parameter when a 90 degree clockwise rotation is needed:
ffmpeg -i capture.y4m -vf transpose=1 -c:v libvpx -b:v 1M capture.webm
Example:
- On the board: a 5-second screencast is recorded
wcap-decode capture.wcap --yuv4mpeg2 > capture.y4m
wcap file: size 720x1280, 192 frames
ls -l capture.*
-rw-r--r-- 1 8246868 Dec 13 14:58 capture.wcap
-rw-r--r-- 1 167821312 Dec 13 14:59 capture.y4m
- On the host PC
scp root@<ip address>:/capture.y4m .
ffmpeg -i capture.y4m -vf transpose=1 -c:v libvpx -b:v 1M capture.webm
ls -l capture.*
-rw-r--r-- 1 104470 Feb 8 11:01 capture.webm
-rw-r--r-- 1 167821312 Feb 8 10:56 capture.y4m
References list:
- ↑ https://cgit.freedesktop.org/wayland/weston/tree/desktop-shell/shell.c Weston Wayland Compositor official git