Difference between revisions of "WLAN device tree configuration"

[unchecked revision] [quality revision]
m
m
 

1 Article purpose[edit]

The purpose of this article is to explain how to configure the WLAN when the peripheral (or peripheral associated to the framework) is assigned to Linux® OS.

The configuration is performed using the device tree mechanism that provides a hardware description of the WLAN peripheral connected on SDIO bus.

The purpose of this article is to explain Cypress WLAN/BT companion chip[1]device tree node

2 DT bindings documentation[edit]

The WLAN[2] tree bindings are composed by :

  • SDIO link configuration[3]
  • WLAN device configuration[4]

3 DT configuration[edit]

This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.

3.1 DT configuration (STM32 level)[edit]

The companion chip uses the SDIO link so the DT is based on the SDMMC peripheral node which is located in stm32mp151.dtsi

  • This is a set of properties that may not vary for given STM32 device, such as: registers address, clock, reset.

The SDMMC DT configuration is explained at SDMMC device tree configuration

Warning.png This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.

3.2 DT configuration (board level)[edit]

Part of the device tree is used to describe the WLAN hardware used on a given board. The DT node ("sdmmc2") must be filled in:

  • mmc-pwrseq: phandle to the MMC power sequence node
&sdmmc2 {
       ...
       arm,primecell-periphid = <0x10153180>;       /* Mandatory version for SDIO */
       ...
       non-removable;
       st,neg-edge;
       bus-width = <4>;
       vmmc-supply = <&v3v3>;
       mmc-pwrseq = <&wifi_pwrseq>;                 /* phandle to the MMC power sequence node */
       ...
       brcmf: bcrmf@1 {                             /* node of WLAN companion chip */
          reg = <1>;
          compatible = "brcm,bcm4329-fmac";
       }
}

The arm,primecell-periphid property has to be forced to <0x10153180> for SDIO. If this field is not present, then the property may use the new version of the SDMMC peripheral <0x00253180> defined in SoC device tree file, which enables the Setting this version disables the support for Linked List in the SDMMC Internal DMA. But Linked List are not supported mandates all the blocks in the list (except the last one) are the same size, which cannot be satisfied with SDIO.

4 References[edit]


== Article purpose ==
The purpose of this article is to explain how to configure the [[WLAN and Bluetooth hardware component|WLAN]] when the peripheral ''(or peripheral associated to the framework)'' is assigned to Linux<sup>&reg;</sup> OS'''. 

The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the WLAN peripheral connected on SDIO bus.

The purpose of this article is to explain Cypress WLAN/BT companion chip<ref>[http://wireless.murata.com/datasheet?/RFM/data/lbee5kl1dx.pdf], CYW4343W</ref>         [[Device tree|device tree]] node

== DT bindings documentation ==

The ''WLAN''<ref name="WLAN and Bluetooth hardware component"> [[WLAN and Bluetooth hardware component]]</ref> ''' tree bindings are composed by :

* SDIO link configuration<ref>[[SDMMC device tree configuration]]</ref>


* WLAN device configuration<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/net/wireless/brcm,bcm43xx-fmac.txt}}</ref>


== DT configuration ==
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split. 

=== DT configuration (STM32 level) ===
The companion chip uses the SDIO link so the DT is based on the SDMMC peripheral node which is located in ''stm32mp151.dtsi''
* This is a set of properties that may not vary for given STM32 device, such as: registers address, clock, reset.
The SDMMC DT configuration is explained at [[SDMMC device tree configuration]]
{{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}}

=== DT configuration (board level) ===
Part of the [[Device tree|device tree]] is used to describe the WLAN hardware used on a given board. The DT node ('''"sdmmc2"''') must be filled in:
* mmc-pwrseq: phandle to the MMC power sequence node

 &sdmmc2 {
        ...
        arm,primecell-periphid = <0x10153180>;       {{highlight|/* Mandatory version for SDIO */}}
        ...
        non-removable;
        st,neg-edge;
        bus-width = <4>;
        vmmc-supply = <&v3v3>;
        mmc-pwrseq = <&wifi_pwrseq>;                 {{highlight|/* phandle to the MMC power sequence node */}}
        ...
        brcmf: bcrmf@1 {                             {{highlight|/* node of WLAN companion chip */}}
           reg = <1>;
           compatible = "brcm,bcm4329-fmac";
        }
 }

The arm,primecell-periphid property has to be forced to <0x10153180> for SDIO. IfSetting this field is not present, then the property may use the new version of the SDMMC peripheral <0x00253180> defined in SoC device tree file, which enables the support for Linked List in the SDMMC Internal DMA. But Linked List are not supported with SDIO.
version disables the support for Linked List in the SDMMC Internal DMA. Linked List mandates all the blocks in the list (except the last one) are the same size, which cannot be satisfied with SDIO. 
==References==<references />

<noinclude>

[[Category:Device tree configuration]]
[[Category:WLAN]]
{{PublicationRequestId | 10169 | 2019-01-03 | AlainF}}
{{ArticleBasedOnModel | Peripheral or framework device tree configuration model}}</noinclude>
Line 43: Line 43:
 
  }
 
  }
   
The arm,primecell-periphid property has to be forced to <0x10153180> for SDIO. If this field is not present, then the property may use the new version of the SDMMC peripheral <0x00253180> defined in SoC device tree file, which enables the support for Linked List in the SDMMC Internal DMA. But Linked List are not supported with SDIO.
+
The arm,primecell-periphid property has to be forced to <0x10153180> for SDIO. Setting this version disables the support for Linked List in the SDMMC Internal DMA. Linked List mandates all the blocks in the list (except the last one) are the same size, which cannot be satisfied with SDIO.  
   
 
==References==
 
==References==