Difference between revisions of "U-Boot - How to debug"
[quality revision] | [quality revision] |
m
|
m (→Load U-Boot symbol)
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
Contents
1 Debug with console[edit]
See U-Boot Documentation or doc/develop/logging.rst for U-Boot logging details.
CONFIG_LOG is enable in OpenSTLinux.
By default, traces are available on the U-Boot console which use stdout-path
defined in the chosen
node of the Linux kernel device tree as described in the Linux kernel binding[1].
See page How to configure U-Boot for your board for configuration details.
The ST boards use the default logging configuration:
-
CONFIG_LOG_DEFAULT_LEVEL = CONFIG_LOG_MAX_LEVEL = LOGL_INFO = 6
the 'debug' macros used by U-Boot (log_debug(), debug(), pr_debug()...) are removed in the U-Boot binary. - CONFIG_LOGF_FILE, CONFIG_LOGF_LINE, CONFIG_LOGF_FUNC are not activated
no debug information in log messages by default.
To enable all the debug traces in U-Boot you need to increase the max logging level with a major impact on U-Boot size; e.g. set CONFIG_LOG_MAX_LEVEL to LOGL_DEBUG by adding in your defconfig file the line:
CONFIG_LOG_MAX_LEVEL=7
When the traces are present in U-Boot, you can change the default trace level with CONFIG_LOG_DEFAULT_LEVEL or you can use the log
command (CONFIG_CMD_LOG) to dynamically configure and filter the output:
log level 7 log format all
1.1 Activate debug trace on one file[edit]
To turn on this debug logging just in one file, you can define LOG_DEBUG and DEBUG for this file
- add define before any include in the <file>.c file
#define LOG_DEBUG #define DEBUG
- with a Makefile
CFLAGS_<file>.o+= -DLOG_DEBUG -DDEBUG
1.2 Debug before console[edit]
If U-Boot fails before the console configuration (in the first stage of U-Boot execution), trace is not available.
In this case, you need to:
- debug with GDB (see the next chapter)
or,
- activate the debug UART feature:
- add in defconfig of U-Boot configuration
- CONFIG_DEBUG_UART
- CONFIG_DEBUG_UART_STM32
- adapt the function board_debug_uart_init(): that configures the required resources (pad, clock) before initialization by the U-Boot driver.
This function needs to be adapted for your board.
- add in defconfig of U-Boot configuration
2 Debug with GDB[edit]
With OpenSTLinux, you can directly use GDB script Setup.gdb:
Or for manual GDB connection, you need to:
- get the elf files for U-Boot =
u-boot
available in the build directory - connect GDB to the target
-
reset with attach the target with the gdb "monitor reset halt" command:
execution is stopped in ROM code or at the beginning of FSBL execution. - load the symbols of the binary to be debugged with commands available in next chapter:
#Load U-Boot symbol - start execution with the "continue" command
2.1 Load U-Boot symbol[edit]
With U-Boot relocation, symbols are more difficult to load. See https://www.denx.de/wiki/DULG/DebuggingUBoot , see doc/README.arm-relocation for details.
If you connect GDB on running target, you can load the debug symbols:
- Before relocation with "symbol-file" command:
symbol-file u-boot
- After relocation with "add-symbol-file" command to relocate the symbol with the code offset = gd->relocaddr:
symbol-file u-boot --> only for "gd_t" definition set $offset = ((gd_t *)$r9)->relocaddr --> get relocation offset symbol-file --> clear previous symbol add-symbol-file u-boot $offset
The following GDB example script automatically loads the U-Boot symbol before and after relocation for a programmed board, after "monitor reset halt" command:
thbreak *0xC0100000
commands
> symbol-file u-boot
> thbreak relocate_code
> commands
> print "RELOCATE U-Boot..."
> set $offset = ((gd_t *)$r9)->relocaddr
> print $offset
> symbol-file
> add-symbol-file u-boot $offset
> thbreak boot_jump_linux
> continue
> end
> continue
> end
This script uses a temporary hardware breakpoint "thbreak" to load the symbol when U-Boot code is loaded in DDR by FSBL = TF-A at the U-Boot entry point, CONFIG_SYS_TEXT_BASE =
It allows the symbol to be loaded only when code is executed to avoid DDR access before DDR initialization.
3 References[edit]
- ↑ Documentation/devicetree/bindings/chosen.txt the Linux kernel binding for chosen node
<noinclude>{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x,STM32MP15x }}</noinclude> == Debug with console == See {{DocSource | domain=U-Boot |path=develop/logging.html | text=U-Boot Documentation}} or {{CodeSource | U-Boot |doc/develop/logging.rst}} for U-Boot logging details. '''CONFIG_LOG''' is enable in OpenSTLinux. By default, traces are available on the U-Boot console which use <code>stdout-path</code> defined in the <code>chosen</code> node of the Linux kernel device tree as described in the Linux kernel binding<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/chosen.txt | Documentation/devicetree/bindings/chosen.txt}} the Linux kernel binding for chosen node</ref>. See page [[How_to_configure_U-Boot_for_your_board#Console|How to configure U-Boot for your board]] for configuration details. The ST boards use the default logging configuration: * {{highlight|CONFIG_LOG_DEFAULT_LEVEL}} = {{highlight|CONFIG_LOG_MAX_LEVEL}} = {{highlightParam|LOGL_INFO}} = {{highlightParam|6}}<br/>the 'debug' macros used by U-Boot (log_debug(), debug(), pr_debug()...) are removed in the U-Boot binary. * CONFIG_LOGF_FILE, CONFIG_LOGF_LINE, CONFIG_LOGF_FUNC are not activated<br/>no debug information in log messages by default. To enable all the debug traces in U-Boot you need to increase the max logging level with a major impact on U-Boot size; e.g. set {{highlight|CONFIG_LOG_MAX_LEVEL}} to {{highlightParam|LOGL_DEBUG}} by adding in your defconfig file the line: {{highlight|CONFIG_LOG_MAX_LEVEL}}={{HighlightParam|7}} When the traces are present in U-Boot, you can change the default trace level with {{highlight|CONFIG_LOG_DEFAULT_LEVEL}} or you can use the <code>log</code> command (CONFIG_CMD_LOG) to dynamically configure and filter the output: {{U-Boot$}} log level 7 {{U-Boot$}} log format all === Activate debug trace on one file === To turn on this debug logging just in one file, you can define LOG_DEBUG and DEBUG for this file * add define before any include in the <file>.c file #define LOG_DEBUG #define DEBUG * with a Makefile CFLAGS_<file>.o+= -DLOG_DEBUG -DDEBUG === Debug before console === If U-Boot fails before the console configuration (in the first stage of U-Boot execution), trace is not available. In this case, you need to: * debug with GDB (see the next chapter) or, * activate the debug UART feature: ** add in defconfig of [[U-Boot_overview#U-Boot_configuration|U-Boot configuration]] *** {{Highlight|CONFIG_DEBUG_UART}} *** {{Highlight|CONFIG_DEBUG_UART_STM32}} ** adapt the function {{Highlight|board_debug_uart_init()}}: that configures the required resources (pad, clock) before initialization by the U-Boot driver.<br/>This function needs to be adapted for your board. == Debug with GDB == With OpenSTLinux, you can directly use GDB script Setup.gdb: * [[GDB#U-Boot_execution_phase]] * [[GDB#U-Boot_boot_case]] Or for manual GDB connection, you need to: # get the [[U-Boot_overview#Output_files|elf files]] for U-Boot = <code>u-boot</code> available in the build directory # connect [[GDB]] to the target # '''reset with attach''' the target with the gdb {{Highlight|"monitor reset halt"}} command:<br/>execution is stopped in ROM code or at the beginning of FSBL execution. # load the symbols of the binary to be debugged with commands available in next chapter:<br/>[[#Load U-Boot symbol]] # start execution with the {{Highlight|"continue"}} command === Load U-Boot symbol === With [[U-Boot_overview#U-Boot_execution_sequence|U-Boot relocation]], symbols are more difficult to load. See https://www.denx.de/wiki/DULG/DebuggingUBoot , see {{CodeSource | U-Boot | doc/README.arm-relocation}} for details. If you connect GDB on running target, you can load the debug symbols: * Before relocation with {{Highlight|"symbol-file"}} command: {{GDB$}} {{Highlight|symbol-file u-boot}} * After relocation with {{Highlight|"add-symbol-file"}} command to relocate the symbol with the code offset = gd->relocaddr: {{GDB$}} symbol-file u-boot {{Highlight|--> only for "gd_t" definition}} {{GDB$}} set $offset = ((gd_t *)$r9)->relocaddr {{Highlight|--> get relocation offset}} {{GDB$}} symbol-file {{Highlight|--> clear previous symbol }} {{GDB$}} {{Highlight|add-symbol-file u-boot $offset}} The following GDB example script automatically loads the U-Boot symbol before and after relocation for a programmed board, after {{Highlight|"monitor reset halt"}} command: {{GDB$}} thbreak *{{HighlightParam|0xC0100000}} {{GDB$}} commands > symbol-file u-boot > thbreak relocate_code > commands > print "RELOCATE U-Boot..." > set $offset = ((gd_t *)$r9)->relocaddr > print $offset > symbol-file > add-symbol-file u-boot $offset > thbreak boot_jump_linux > continue > end > continue > end This script uses a temporary hardware breakpoint {{Highlight|"thbreak"}} to load the symbol when U-Boot code is loaded in DDR by FSBL = TF-A at the U-Boot entry point, CONFIG_SYS_TEXT_BASE = * {{HighlightParam|0xC0000000}} for {{MicroprocessorDevice | device=13}} * {{HighlightParam|0xC0100000}} for {{MicroprocessorDevice | device=15}} It allows the symbol to be loaded only when code is executed to avoid DDR access before DDR initialization. == References ==<references/> <noinclude> [[Category:U-Boot|U-Boot - 8]] [[Category:Tracing tools]] [[Category:Debugging tools]] {{PublicationRequestId | 12894 | 2019-08-01}}</noinclude>
Line 65: | Line 65: | ||
=== Load U-Boot symbol === |
=== Load U-Boot symbol === |
||
− | With [[U-Boot_overview#U-Boot_execution_sequence|U-Boot relocation]], symbols are more difficult to load |
+ | With [[U-Boot_overview#U-Boot_execution_sequence|U-Boot relocation]], symbols are more difficult to load, see {{CodeSource | U-Boot | doc/README.arm-relocation}} for details. |
− | |||
− | |||
If you connect GDB on running target, you can load the debug symbols: |
If you connect GDB on running target, you can load the debug symbols: |