Template:ArticleApprovedVersion
1 Debug with console[edit source]
Trace and error are available on the console defined in the chosen node of the device tree by the stdout-path field:
chosen { stdout-path = "serial3:115200n8"; };
By default, the macros used by U-Boot (debug(), pr_debug()...) do not print any trace; to activate the debug traces on a specific file, you need to enable the DEBUG compilation flag and change the LOGLEVEL for the file:
- define DEBUG before any include in the <file>.c file
#define DEBUG #undef CONFIG_LOGLEVEL #define CONFIG_LOGLEVEL 8
- with a Makefile
CFLAGS_<file>.o+= -DDEBUG -DCONFIG_LOGLEVEL=8
If U-Boot fails before the console configuration (in the first stage of U-Boot execution), trace is not available.
In this case, you need to:
- debug with GDB (see the next chapter)
or,
- activate the debug UART feature:
- activate CONFIG_DEBUG_UART with configure
- board_debug_uart_init(): this is a weak function that configures the required resources (pad, clock) before initialization by the U-Boot driver.
This function needs to be adapted for your case.
2 Debug with GDB on a Flashed device[edit source]
You need to:
- connect GDB to the target
- load the symbols of the binary to be debugged (see #SPL symbol load and #U-Boot symbol load).
The required files are available in the build directory. - reset with attach the target with the gdb "monitor reset halt" command
- start execution with the "continue" command
2.1 SPL symbol load[edit source]
To debug SPL, the GDB script just consists of loading the SPL symbols:
(gdb) symbol-file spl/u-boot-spl
2.2 U-Boot symbol load[edit source]
With U-Boot relocation, symbols are more difficult to load.
See https://www.denx.de/wiki/DULG/DebuggingUBoot
Here is an example of a GDB script to debug U-Boot:
(gdb) thbreak *0xC0100000
(gdb) commands
> symbol-file u-boot
> thbreak relocate_code
> commands
> print "RELOCATE U-Boot..."
> set $offset = ((gd_t *)$r9)->relocaddr
> print $offset
> symbol-file
> add-symbol-file u-boot $offset
> thbreak boot_jump_linux
> continue
> end
> continue
> end
The U-Boot code is relocated at the end of the DDR, at gd->relocaddr.
The script uses a temporary hardware breakpoint (thbreak) to automatically load the U-Boot symbol with
- 'u-boot' = the elf file for U-Boot
- CONFIG_SYS_TEXT_BASE = 0xC0100000 (loading symbol only when code is executed)
3 Load code and debug with GDB[edit source]
To load and debug on the target, you need to:
- reset and attach to the target as soon as possible: with the GDB "monitor reset halt" command, see GDB for details
- load the code and device-tree by using GDB (with the load command, see the following examples)
- execute the binary (the PC is automatically updated, execute the code with the GDB "continue" command)
Depending on the device tree location defined with one of the CONFIG_OF_* configuration flags, the scripts to load the SPL code are:
- CONFIG_OF_SEPARATE = dtb appended at the end of the code, not present in the elf file
(gdb) file spl/u-boot-spl (gdb) load (gdb) set $dtb = __bss_end (gdb) restore spl/dt.dtb binary $dtb
- CONFIG_OF_EMBED = dtb embedded in the elf file
(gdb) file spl/u-boot-spl (gdb) load