Difference between revisions of "Trace-cmd and kernelshark trace viewer"

[quality revision] [quality revision]
m
 
imported>Frq07399
m


Template:ArticleMainWriter

Template:ArticleDraftVersionArticleApprovedVersion


1 Article purpose[edit]

This article provides the basic information needed to start using the Linux tool: trace-cmd[1] and host trace viewer kernelshark[2].

2 Introduction[edit]

The following table provides a brief description of the tool, as well as its availability depending on the software packages:

Yes: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.

No: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.

Tool STM32MPU Embedded Software distribution STM32MPU Embedded Software distribution for Android™
Name Category Purpose Starter Package Developer Package Distribution Package Starter Package Developer Package Distribution Package
trace-cmd Tracing tools trace-cmd[1] command interacts with the Ftrace tracer that is built inside the Linux kernel. It interfaces with the Ftrace specific files found in the debugfs file system under the tracing directory.

kernelshark[2] is a front-end reader of trace-cmd output. "trace-cmd record" and "trace-cmd extract" create a trace.dat (trace-cmd.dat) file. kernelshark can read this file, and produce a graph and list view of the corresponding data.

No No Yes
Under construction.png Coming soon

Note: in case you want to trace at boot time, it is recommended to use ftrace.

3 Installing the trace and debug tool on your target board[edit]

3.1 Using the STM32MPU Embedded Software distribution[edit]

Since Yocto Thud version, trace-cmd recipe is no more present in openembedded-core meta package and so is not installed by default in all STM32MPU Software Packages.

Following recipes are proposed to integrate trace-cmd in STM32MPU Embedded Software distribution. It has to be added in layers/meta-st/meta-st-stm32mp/recipes-kernel.

  • Create trace-cmd directory:
PC $> mkdir layers/meta-st/meta-st-stm32mp/recipes-kernel/trace-cmd
PC $> cd layers/meta-st/meta-st-stm32mp/recipes-kernel/trace-cmd
  • Create trace-cmd.inc file with the following content:
SRCREV = "57371aaa2f469d0ba15fd85276deca7bfdd7ce36"
PV = "2.6.2"

inherit pkgconfig

FILESEXTRAPATHS =. "${FILE_DIRNAME}/trace-cmd:"

SRC_URI = "git://git.kernel.org/pub/scm/linux/kernel/git/rostedt/trace-cmd.git;branch=trace-cmd-stable-v2.6"

S = "${WORKDIR}/git"
  • Create trace-cmd_git.bb file with the following content:
SUMMARY = "User interface to Ftrace"
HOMEPAGE = "http://git.kernel.org/"
LICENSE = "GPLv2 & LGPLv2.1"

require trace-cmd.inc

LIC_FILES_CHKSUM = "file://COPYING;md5=751419260aa954499f7abaabaa882bbe \
                    file://trace-cmd.c;beginline=6;endline=8;md5=2c22c965a649ddd7973d7913c5634a5e \
                    file://COPYING.LIB;md5=edb195fe538e4552c1f6ca0fd7bf4f0a \
                    file://trace-input.c;beginline=5;endline=8;md5=3ec82f43bbe0cfb5951ff414ef4d44d0 \
"

EXTRA_OEMAKE = "\
    'prefix=${prefix}' \
    'bindir=${bindir}' \
    'man_dir=${mandir}' \
    'html_install=${datadir}/kernelshark/html' \
    'img_install=${datadir}/kernelshark/html/images' \
    \
    'bindir_relative=${@oe.path.relative(prefix, bindir)}' \
    'libdir=${libdir}' \
    \
    NO_PYTHON=1 \
"

do_compile_prepend() {
    # Make sure the recompile is OK
    rm -f ${B}/.*.d
}

do_install() {
        oe_runmake DESTDIR="${D}" install
}
  • Add trace-cmd package install to the st-image-weston , by adding following lines at the end of fine layersimage:
PC $> echo 'IMAGE_INSTALL_append += "trace-cmd"' >> layer/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.
bb
CORE_IMAGE_EXTRA_INSTALL += " \
    trace-cmd \
	"
bbappend

  • Rebuilt the st-image-weston target:
PC $> cd <build_directory>
PC $> bitbake st-image-weston

When testing the new image on the target board, trace-cmd can be found in the following path:

Board $> which trace-cmd
/usr/bin/trace-cmd


However, an additional configuration of the Linux kernel must be performed to obtain the trace.

This is the configuration used for ftrace. Please refer to Ftrace install to complete the configuration of the Linux kernel.

This is the reason why you can not use this tool in Starter and Developer Packages context.

3.2 Using the STM32MPU Embedded Software distribution for Android™[edit]

Under construction.png Coming soon

4 Getting started[edit]

trace-cmd inherits all available configurations from Ftrace.

It is possible to get filtered trace with both function and graph function mode.

It is also possible to trace specific prints done in the source file.

You first need to mount the tracefs:

Board $> mount -t tracefs nodev /sys/kernel/tracing

To find out which tracers are available, simply cat the available_tracers file in the tracing directory:

 
Board $> cat /sys/kernel/tracing/available_tracers
 function_graph function nop

Note that you must be placed on the target board within a directory path where you have access rights for writing the generated trace file.

4.1 Making a trace using function tracer mode[edit]

The example below shows how to filter on a set of functions that contains uart:

- To get a trace on UART, you can connect to the target board with the new console (i.e. through ssh), and then type a simple command, like "ls"
- Then press Ctrl-C to stop the trace
Board $> trace-cmd record -p function -l *uart*
  plugin 'function'
Hit Ctrl^C to stop recording
^CCPU0 data recorded at offset=0x15d000
    4096 bytes in size
CPU1 data recorded at offset=0x15e000
    4096 bytes in size

See below for reading the trace.

4.2 Making a trace using graph function tracer mode[edit]

The example below shows how to filter on a set of graph functions that contains uart:

- To get trace on UART, you can connect to the target board with the new console (i.e. through ssh), and then type a simple command, like "ls"
- Then press Ctrl-C to stop the trace
Board $> trace-cmd record -p function_graph -l *uart*
  plugin 'function_graph'
Hit Ctrl^C to stop recording
^CCPU0 data recorded at offset=0x15d000
    4096 bytes in size
CPU1 data recorded at offset=0x15e000
    4096 bytes in size

See below for reading the trace.

4.3 Reading the trace[edit]

Command to read the trace:

Board $> trace-cmd report

By default, it reads the previously created file trace.dat at the position where the command is entered.

If you want to specify an other file name:

Board $> trace-cmd report -i mytrace.dat
or
Board $> trace-cmd report mytrace.dat

5 To go further[edit]

5.1 Visualizing trace using kernelshark[edit]

5.1.1 Host installation (Linux environment)[edit]

PC $> sudo apt-get install kernelshark

5.1.2 Opening and reading trace-cmd trace[edit]

kernelshark can read trace-cmd report and produce a graph and list view of the data. Please refer to kernelshark home page[2] for detail.

  • Get the trace from the board. It is possible to get the trace directly from the SDCard under use, or remotely from the target board:
PC $> scp root@<board_ip_address>/<path_to>/trace.dat <path_on_host>

  • Open trace with kernelshark

It can be done by opening kernelshark and then opening trace.dat file from the menu, or using the following command:

PC $> kernelshark <path_on_host>/trace.dat

Here is the example of a trace filtered with UART function_graph mode:
Kernelshark functiongraph.png

6 References[edit]


  • Useful external links
Document link Document Type Description
Using KernelShark User Guide https://lwn.net
Trace-cmd presentation User Guide https://lwn.net
KernelShark quick tutorial Presentation https://elinux.org
<noinclude>

{{ArticleBasedOnModel | [[Trace and debug tools article model]]}}
{{ArticleMainWriter | Jean-PhilippeR}}

{{ ArticleDraftVersionArticleApprovedVersion | Jean-PhilippeR | Jean-ChristopheT, GeraldB, AlexandreT | 15Nov'18 | BrunoB - 14Nov'18 | 22Jan | No previous approved version  | BrunoB - 14Nov'18 - 9570 | 01Feb'19 }} 

[[Category:Linux tracing tools]]</noinclude>


== Article purpose ==
This article provides the basic information needed to start using the Linux tool: '''trace-cmd'''<ref name=lwndotnet_tracecmd/> and host trace viewer '''kernelshark'''<ref name=homelinuxdotcom_kernelshark/>.

== Introduction ==
{{:Trace_and_debug_tools_assignment_table_template}}<onlyinclude>

 | [[Trace-cmd and kernelshark trace viewer|trace-cmd]]
 | [[:Category:Tracing tools|Tracing tools]]
 | style="text-align:left;" |'''trace-cmd'''<ref name=lwndotnet_tracecmd>https://lwn.net/Articles/410200/</ref> command interacts with the [[Ftrace]] tracer that is built inside the Linux kernel. It interfaces with the [[Ftrace]] specific files found in the debugfs file system under the tracing directory.<br>

'''kernelshark'''<ref name=homelinuxdotcom_kernelshark>http://rostedt.homelinux.com/kernelshark</ref> is a front-end reader of trace-cmd output. "trace-cmd record" and "trace-cmd extract" create a trace.dat (trace-cmd.dat) file. kernelshark can read this file, and produce a graph and list view of the corresponding data.
 | {{N}} || {{N}} || {{Y}}
 | colspan="3" | {{UnderConstruction}}
 |-</onlyinclude>

|}

''Note: in case you want to trace at boot time, it is recommended to use [[Ftrace|ftrace]]''.

== Installing the trace and debug tool on your target board ==

=== Using the STM32MPU Embedded Software distribution ===
Since Yocto Thud version, '''trace-cmd''' recipe is no more present in openembedded-core meta package and so is not installed by default in all STM32MPU Software Packages.

Following recipes are proposed to integrate trace-cmd in STM32MPU Embedded Software distribution. ''It has to be added in layers/meta-st/meta-st-stm32mp/recipes-kernel''.

* Create ''trace-cmd'' directory:

 {{PC$}} mkdir layers/meta-st/meta-st-stm32mp/recipes-kernel/trace-cmd
 {{PC$}} cd layers/meta-st/meta-st-stm32mp/recipes-kernel/trace-cmd

* Create ''trace-cmd.inc'' file with the following content:

 SRCREV = "57371aaa2f469d0ba15fd85276deca7bfdd7ce36"
 PV = "2.6.2"

 inherit pkgconfig

 FILESEXTRAPATHS =. "${FILE_DIRNAME}/trace-cmd:"

 SRC_URI = "git://git.kernel.org/pub/scm/linux/kernel/git/rostedt/trace-cmd.git;branch=trace-cmd-stable-v2.6"

 S = "${WORKDIR}/git"

* Create ''trace-cmd_git.bb'' file with the following content:

 SUMMARY = "User interface to Ftrace"
 HOMEPAGE = "http://git.kernel.org/"
 LICENSE = "GPLv2 & LGPLv2.1"

 require trace-cmd.inc

 LIC_FILES_CHKSUM = "file://COPYING;md5=751419260aa954499f7abaabaa882bbe \
                     file://trace-cmd.c;beginline=6;endline=8;md5=2c22c965a649ddd7973d7913c5634a5e \
                     file://COPYING.LIB;md5=edb195fe538e4552c1f6ca0fd7bf4f0a \
                     file://trace-input.c;beginline=5;endline=8;md5=3ec82f43bbe0cfb5951ff414ef4d44d0 \
 "

 EXTRA_OEMAKE = "\
     'prefix=${prefix}' \
     'bindir=${bindir}' \
     'man_dir=${mandir}' \
     'html_install=${datadir}/kernelshark/html' \
     'img_install=${datadir}/kernelshark/html/images' \
     \
     'bindir_relative=${@oe.path.relative(prefix, bindir)}' \
     'libdir=${libdir}' \
     \
     NO_PYTHON=1 \
 "

 do_compile_prepend() {
     # Make sure the recompile is OK
     rm -f ${B}/.*.d
 }

 do_install() {
         oe_runmake DESTDIR="${D}" install
 }

* Add '''trace-cmd''' package install to the st-image-weston, by adding following lines at the end of fine ''layers image:
 {{PC$}} echo 'IMAGE_INSTALL_append += "trace-cmd"' >> layer/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb''
 CORE_IMAGE_EXTRA_INSTALL += " \
     trace-cmd \
 	"
* Rebuilt the st-image-weston targetbbappend

* Rebuilt the ''st-image-weston'' target:

 {{PC$}} cd {{orange|<build_directory>}}
 {{PC$}} bitbake st-image-weston

When testing the new image on the target board, trace-cmd can be found in the following path:

 {{Board$}} which trace-cmd
 /usr/bin/trace-cmd

{{highlight|However, an additional configuration of the Linux kernel must be performed to obtain the trace.}}

This is the configuration used for '''ftrace'''. Please refer to [[Ftrace#Installing the trace and debug tool on your target board|Ftrace install]] to complete the configuration of the Linux kernel.

{{highlight|This is the reason why you can not use this tool in Starter and Developer Packages context.}}

=== Using the STM32MPU Embedded Software distribution for Android&trade; ===
{{UnderConstruction}}

== Getting started ==
trace-cmd inherits all available configurations from [[Ftrace]].

It is possible to get filtered trace with both function and graph function mode.

It is also possible to trace specific prints done in the source file.

You first need to mount the tracefs:
 {{Board$}} mount -t tracefs nodev /sys/kernel/tracing

To find out which tracers are available, simply cat the available_tracers file in the tracing directory:
  {{Board$}} cat /sys/kernel/tracing/available_tracers
  function_graph function nop

{{highlight|Note that you must be placed on the target board within a directory path where you have access rights for writing the generated trace file.}}

=== Making a trace using function tracer mode ===

The example below shows how to filter on a set of functions that contains uart:
:- To get a trace on UART, you can connect to the target board with the new console (i.e. through ssh), and then type a simple command, like "''ls''"
:- Then press Ctrl-C to stop the trace
 {{Board$}} trace-cmd record -p {{green|function}} -l {{orange|*uart*}}
   plugin '{{green|function}}'
 Hit Ctrl^C to stop recording
 {{highlight|^C}}CPU0 data recorded at offset=0x15d000
     4096 bytes in size
 CPU1 data recorded at offset=0x15e000
     4096 bytes in size

See below for [[#Reading the trace|reading the trace]].

=== Making a trace using graph function tracer mode ===
The example below shows how to filter on a set of graph functions that contains uart:
:- To get trace on UART, you can connect to the target board with the new console (i.e. through ssh), and then type a simple command, like "''ls''"
:- Then press Ctrl-C to stop the trace
 {{Board$}} trace-cmd record -p {{green|function_graph}} -l {{orange|*uart*}}
   plugin '{{green|function_graph}}'
 Hit Ctrl^C to stop recording
 {{highlight|^C}}CPU0 data recorded at offset=0x15d000
     4096 bytes in size
 CPU1 data recorded at offset=0x15e000
     4096 bytes in size

See below for [[#Reading the trace|reading the trace]].

=== Reading the trace ===
Command to read the trace:
 {{Board$}} trace-cmd report
By default, it reads the previously created file ''trace.dat'' at the position where the command is entered.

If you want to specify an other file name:
 {{Board$}} trace-cmd report -i {{orange|mytrace.dat}}
 or
 {{Board$}} trace-cmd report {{orange|mytrace.dat}}

== To go further ==
=== Visualizing trace using kernelshark ===
==== Host installation (Linux environment) ====
 {{PC$}} sudo apt-get install kernelshark

==== Opening and reading trace-cmd trace ====
kernelshark can read trace-cmd report and produce a graph and list view of the data. Please refer to kernelshark home page<ref name=homelinuxdotcom_kernelshark/> for detail.
* Get the trace from the board. It is possible to get the trace directly from the SDCard under use, or remotely from the target board:
 {{PC$}} scp root@{{orange|<''board_ip_address''>/<''path_to''>}}/trace.dat {{orange|<''path_on_host''>}}

* Open trace with kernelshark
It can be done by opening kernelshark and then opening trace.dat file from the menu, or using the following command:
 {{PC$}} kernelshark {{orange|<''path_on_host''>}}/trace.dat
Here is the example of a trace filtered with UART function_graph mode:<br />

[[File:Kernelshark functiongraph.png|1000px|link=]]

== References ==<references />


* Useful external links
{|
! scope=col | Document link
! scope=col | Document Type
! scope=col | Description
|-
| [https://lwn.net/Articles/425583/ Using KernelShark]
| User Guide
| https://lwn.net
|-
| [https://lwn.net/Articles/341902/ Trace-cmd presentation]
| User Guide
| https://lwn.net
|-
| [https://elinux.org/images/6/64/Elc2011_rostedt.pdf KernelShark quick tutorial]
| Presentation
| https://elinux.org
|}
Line 3: Line 3:
 
{{ArticleMainWriter | Jean-PhilippeR}}
 
{{ArticleMainWriter | Jean-PhilippeR}}
   
{{ ArticleDraftVersion| Jean-PhilippeR | Jean-ChristopheT, GeraldB, AlexandreT | 15Nov'18 | BrunoB - 14Nov'18 | 22Jan'19 }}  
+
{{ ArticleApprovedVersion | Jean-PhilippeR | Jean-ChristopheT | No previous approved version  | BrunoB - 14Nov'18 - 9570 | 01Feb'19 }}  
   
 
[[Category:Linux tracing tools]]
 
[[Category:Linux tracing tools]]
Line 31: Line 31:
 
Since Yocto Thud version, '''trace-cmd''' recipe is no more present in openembedded-core meta package and so is not installed by default in all STM32MPU Software Packages.
 
Since Yocto Thud version, '''trace-cmd''' recipe is no more present in openembedded-core meta package and so is not installed by default in all STM32MPU Software Packages.
   
Following recipes are proposed to integrate trace-cmd in STM32MPU Embedded Software distribution. ''It has to be added in layers/meta-st/meta-st-stm32mp/recipes-kernel''
+
Following recipes are proposed to integrate trace-cmd in STM32MPU Embedded Software distribution. ''It has to be added in layers/meta-st/meta-st-stm32mp/recipes-kernel''.
* Create trace-cmd directory
+
* Create ''trace-cmd'' directory:
 
  {{PC$}} mkdir layers/meta-st/meta-st-stm32mp/recipes-kernel/trace-cmd
 
  {{PC$}} mkdir layers/meta-st/meta-st-stm32mp/recipes-kernel/trace-cmd
 
  {{PC$}} cd layers/meta-st/meta-st-stm32mp/recipes-kernel/trace-cmd
 
  {{PC$}} cd layers/meta-st/meta-st-stm32mp/recipes-kernel/trace-cmd
   
* Create ''trace-cmd.inc'' file with the following content
+
* Create ''trace-cmd.inc'' file with the following content:
 
  SRCREV = "57371aaa2f469d0ba15fd85276deca7bfdd7ce36"
 
  SRCREV = "57371aaa2f469d0ba15fd85276deca7bfdd7ce36"
 
  PV = "2.6.2"
 
  PV = "2.6.2"
Line 48: Line 48:
 
  S = "${WORKDIR}/git"
 
  S = "${WORKDIR}/git"
   
* Create ''trace-cmd_git.bb'' file with the following content
+
* Create ''trace-cmd_git.bb'' file with the following content:
 
  SUMMARY = "User interface to Ftrace"
 
  SUMMARY = "User interface to Ftrace"
 
  HOMEPAGE = "http://git.kernel.org/"
 
  HOMEPAGE = "http://git.kernel.org/"
Line 83: Line 83:
 
  }
 
  }
   
* Add '''trace-cmd''' package to the st-image-weston, by adding following lines at the end of fine ''layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb''
+
* Add ''trace-cmd'' package install to the st-image-weston image:
CORE_IMAGE_EXTRA_INSTALL += " \
+
{{PC$}} echo 'IMAGE_INSTALL_append += "trace-cmd"' >> layer/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bbappend
    trace-cmd \
+
 
"
+
* Rebuilt the ''st-image-weston'' target:
* Rebuilt the st-image-weston target
 
 
  {{PC$}} cd {{orange|<build_directory>}}
 
  {{PC$}} cd {{orange|<build_directory>}}
 
  {{PC$}} bitbake st-image-weston
 
  {{PC$}} bitbake st-image-weston
   
When testing the new image on the target board, trace-cmd can be found in the following path
+
When testing the new image on the target board, trace-cmd can be found in the following path:
 
  {{Board$}} which trace-cmd
 
  {{Board$}} which trace-cmd
 
  /usr/bin/trace-cmd
 
  /usr/bin/trace-cmd