- Last edited 9 months ago ago
EcosystemRelease
Contents
1 Usage[edit]
The EcosystemRelease template is used to indicate for which ecosystem release revision(s) of the flow associated with this wiki (e.g. v1.y.z ,or v2.y.z, or...), an article part (chapter, paragraph, table...) is valid. Per default (i.e. if this template is not used), any part of an article is valid for all ecosystem release revisions for which the entire article is valid.
It outputs a "standardized" string that might be used to name an article part.
Usage: {{EcosystemRelease | revision=<revision> | range =<range> | revision2=<revision2>}}
Where:
- <revision> is the mandatory ecosystem release revision for which the article part is valid.
- The possible values for this parameter are available in the EcosystemRelease/Revision template.
- The optional <range> and <revision2> parameters allow to define a range of revisions.
- <range> is the optional range of the ecosystem release revisions for which the article part is valid. The possible values are:
- and before: the article part is valid only for the revision(s) less than or equal to <revision>
- and after: the article part is valid only for the revision(s) greater than or equal to <revision>
- to: the article part is only valid from <revision> to <revision2>
- <revision2> is the mandatory ecosystem release upper revision for which the article part is valid, when <range> is set to "to"; in this case, <revision> becomes the lower revision for which the article part is valid.
- The possible values for this parameter are available in the EcosystemRelease/Revision template.
- This parameter is ignored if <range> is either not set, or set to another value than "to".
If the mouse is left over a revision (or the icon), a popup window shows, for that revision:
- the versions of the Linux kernel, U-Boot, TF-A and OP-TEE
- the version of the STM32Cube MPU Package
- the version of OpenEmbedded
- the version of Android
This information comes from the EcosystemRelease/Components template.
2 Basic examples[edit]
You type | You get |
---|---|
A specific revision (revision 5.0.0) that is the latest one
{{EcosystemRelease | revision=5.0.0}} |
|
The latest revision
{{EcosystemRelease | revision=latest}} |
|
Specific revisions that are former ones
{{EcosystemRelease | revision=4.1.0}}<br /> {{EcosystemRelease | revision=4.0.0}}<br /> {{EcosystemRelease | revision=3.1.0}}<br /> {{EcosystemRelease | revision=3.0.0}}<br /> {{EcosystemRelease | revision=2.1.0}}<br /> {{EcosystemRelease | revision=2.0.0}}<br /> {{EcosystemRelease | revision=1.2.0}}<br /> {{EcosystemRelease | revision=1.1.0}}<br /> {{EcosystemRelease | revision=1.0.0}} |
ecosystem release v4.1.0 |
Revisions that are lower than or equal to a revision
{{EcosystemRelease | revision=x.1.0 | range=and before}} |
|
Revisions that are greater than or equal to a revision
{{EcosystemRelease | revision=x.1.0 | range=and after}} |
|
Range of revisions
{{EcosystemRelease | revision=x.0.0 | range=to | revision2=x.1.0}} |
|
Revisions that are lower than or equal to the latest one
{{EcosystemRelease | revision=latest | range=and before}} |
|
Revisions that are greater than or equal to the latest one
{{EcosystemRelease | revision=latest | range=and after}} |
|
Range of revisions
{{EcosystemRelease | revision=x.0.0 | range=to | revision2=latest}} |