Approved version. Approved on: 14:36, 16 October 2020
You are viewing an old version of this page. Return to the latest version.
Difference between revisions of "Template:EcosystemRelease"
[unchecked revision] | [quality revision] |
m
|
m
|
Contents
1 Usage[edit]
The EcosystemRelease template is used to indicate for which ecosystem release revision(s) of the flow associated with this wiki (e.g. v1.y.z ,or v2.y.z, or...), an article part (chapter, paragraph, table...) is valid. Per default (i.e. if this template is not used), any part of an article is valid for all ecosystem release revisions for which the entire article is valid.
It outputs a "standardized" string that might be used to name an article part.
Usage: {{EcosystemRelease | revision=<revision> | range =<range> | revision2=<revision2>}}
Where:
-
<revision> is the mandatory ecosystem release revision for which the article part is valid.
- The possible values for this parameter are available in the EcosystemRelease/Revision template.
- The optional <range> and <revision2> parameters allow to define a range of revisions.
-
<range> is the optional range of the ecosystem release revisions for which the article part is valid. The possible values are:
- and before: the article part is valid only for the revision(s) less than or equal to <revision>
- and after: the article part is valid only for the revision(s) greater than or equal to <revision>
- to: the article part is only valid from <revision> to <revision2>
-
<revision2> is the mandatory ecosystem release upper revision for which the article part is valid, when <range> is set to "to"; in this case, <revision> becomes the lower revision for which the article part is valid.
- This parameter is ignored if <range> is either not set, or set to another value than "to".
If the mouse is left over a revision (or the icon), a popup window shows, for that revision:
- the versions of the Linux kernel, U-Boot, TF-A and OP-TEE
- the version of the STM32Cube MPU Package
- the version of OpenEmbedded
- the version of Android
This information comes from the EcosystemRelease/Components template.
2 Basic examples[edit]
You type | You get |
---|---|
A specific revision (revision 2.0.0) {{EcosystemRelease | revision=2.0.0}} |
ecosystem release v2.0.0 |
Revisions that are lower than or equal to a revision {{EcosystemRelease | revision=x.1.0 | range=and before}} |
|
Revisions that are greater than or equal to a revision {{EcosystemRelease | revision=x.1.0 | range=and after}} |
|
Range of revisions {{EcosystemRelease | revision=x.0.0 | range=to | revision2=x.1.0}} |
3 More examples[edit]
4 Code[edit]
<noinclude> ==Usage== The [[Template:EcosystemRelease|EcosystemRelease]] template is used '''to indicate for which ecosystem release revision(s)''' of the flow associated with this wiki (e.g. v1.y.z ,or v2.y.z, or...), '''an article part (chapter, paragraph, table...) is valid'''. Per default (i.e. if this template is not used), any part of an article is valid for all ecosystem release revisions for which the entire article is valid. It outputs a "standardized" string that might be used to name an article part. Usage: <nowiki>{{</nowiki>EcosystemRelease | revision={{HighlightParam|<revision>}} | range ={{HighlightParam|<range>}} | revision2={{HighlightParam|<revision2>}}}} Where: * {{HighlightParam|<revision>}} is the '''mandatory''' ecosystem release revision for which the article part is valid. ** The possible values for this parameter are available in the [[Template:EcosystemRelease/Revision|EcosystemRelease/Revision]] template. ** The optional {{HighlightParam|<range>}} and {{HighlightParam|<revision2>}} parameters allow to define a range of revisions. * {{HighlightParam|<range>}} is the '''optional''' range of the ecosystem release revisions for which the article part is valid. The possible values are: ** '''and before''': the article part is valid only for the revision(s) less than or equal to {{HighlightParam|<revision>}} ** '''and after''': the article part is valid only for the revision(s) greater than or equal to {{HighlightParam|<revision>}} ** '''to''': the article part is only valid from {{HighlightParam|<revision>}} to {{HighlightParam|<revision2>}} * {{HighlightParam|<revision2>}} is the '''mandatory''' ecosystem release upper revision for which the article part is valid, '''when {{HighlightParam|<range>}} is set to "to'''"; in this case, {{HighlightParam|<revision>}} becomes the lower revision for which the article part is valid. ** This parameter is ignored if {{HighlightParam|<range>}} is either not set, or set to another value than "'''to'''". If the mouse is left over a revision (or the <sup>[[File:More_info.png|15px|link=]]</sup> icon), '''a popup window''' shows, for that revision: * the versions of the Linux kernel, U-Boot, TF-A and OP-TEE * the version of the STM32Cube MPU Package * the version of OpenEmbedded * the version of Android This information comes from the [[Template:EcosystemRelease/Components|EcosystemRelease/Components]] template. ==Basic examples== {| class="st-table" ! style="width: 50%;" | You type !! You get |- | A specific revision (revision 2.0.0)<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=2.0.0}}</pre> | {{EcosystemRelease | revision=2.0.0}} |- | Revisions that are lower than or equal to a revision<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.1.0 | range=and before}}</pre> | {{EcosystemRelease | revision=x.1.0 | range=and before}} |- | Revisions that are greater than or equal to a revision<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.1.0 | range=and after}}</pre> | {{EcosystemRelease | revision=x.1.0 | range=and after}} |- | Range of revisions<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.0.0 | range=to | revision2=x.1.0}}</pre> | {{EcosystemRelease | revision=x.0.0 | range=to | revision2=x.1.0}} |} ==More examples== {| class="st-table" ! style="width: 50%;" | You type !! You get |- | Revision x.1.0<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.1.0}}</pre> | {{EcosystemRelease | revision=x.1.0}} |- | Revision x.0.0<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.0.0}}</pre> | {{EcosystemRelease | revision=x.0.0}} |- | Former revision that is part of a flow that is not the one associated with this wiki.<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=0.y.0}} <br> {{EcosystemRelease | revision=0.y.0 | range=and before}}<br> {{EcosystemRelease | revision=0.y.0 | range=and after}}</pre> | {{EcosystemRelease | revision=0.y.0}} |<br> {{EcosystemRelease | revision=0.y.0 | range=and before}}<br> {{EcosystemRelease | revision=0.y.0 | range=and after}} |- | Unspecified revision<pre style="white-space: pre-wrap;"> {{EcosystemRelease}}</pre> | {{EcosystemRelease}} |- | Unknown revision<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=10.20.30}}</pre> | {{EcosystemRelease | revision=10.20.30}} |- | Unspecified revision2<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.1.0 | range=to}}</pre> | {{EcosystemRelease | revision=x.1.0 | range=to}} |- | Unknown revision2<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.1.0 | range=to | revision2=10.20.30}}</pre> | {{EcosystemRelease | revision=x.1.0 | range=to | revision2=10.20.30}} |- | Former revision2 that is part of a flow that is not the one associated with this wiki.<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.0.0 | range=to | revision2=0.y.0}} <br> {{EcosystemRelease | revision=0.y.0 | range=to | revision2=0.y.0}}</pre> | {{EcosystemRelease | revision=x.0.0 | range=to | revision2=0.y.0}} |<br> {{EcosystemRelease | revision=0.y.0 | range=to | revision2=0.y.0}} |- | Ignored revision2<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.0.0 | range=and after | revision2=x.1.0}}</pre> | {{EcosystemRelease | revision=x.0.0 | range=and after | revision2=x.1.0}} |- | Unknown range<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.1.0 | range=error}}</pre> | {{EcosystemRelease | revision=x.1.0 | range=error}} |- | Check that there's no space before and after the text<pre style="white-space: pre-wrap;"> BEFORE{{EcosystemRelease | revision=x.0.0}}AFTER<br> BEFORE{{EcosystemRelease | revision=x.1.0 | range=and before}}AFTER<br> BEFORE{{EcosystemRelease | revision=x.1.0 | range=and after}}AFTER<br> BEFORE{{EcosystemRelease | revision=x.0.0 | range=to | revision2=x.1.0}}AFTER</pre> | BEFORE{{EcosystemRelease | revision=x.0.0}}AFTER<br> BEFORE{{EcosystemRelease | revision=x.1.0 | range=and before}}AFTER<br> BEFORE{{EcosystemRelease | revision=x.1.0 | range=and after}}AFTER<br> BEFORE{{EcosystemRelease | revision=x.0.0 | range=to | revision2=x.1.0}}AFTER |} ==Code== {{UpdateNeededForNewRelease| * Update the first "basic example" with the latest revision, and add in "more examples" the legacy revisions * Update, if needed, the below sentence "not valid in the flow (v1.y.z) associated"}}</noinclude>ecosystem release {{#switch:{{ {{{range|}}} | and before = ≤ | and after = ≥ }} {{#switch:{{EcosystemRelease/Revision | revision={{{revision|}}}}} | unknown = <span title="This revision value is not valid">{{Highlight|unknown revision {{{revision|}}}}} <sup>[[File:Warning.png|15px|link=]]</sup></span> | former = {{#set:Ecosystem release=unknown revision {{{revision}}}}} | former = v{{{revision|}}}{{#set:Ecosystem release=revision of a previous flow {{{revision}}}}} | #default = {{#switch: {{{range|}}} | and before = ≤ | and after = ≥ }} <span title="{{EcosystemRelease/Components | revision={{{revision|}}}}}">v{{{revision}}} <sup>[[File:More_info.png|15px|link=]]</sup></span> {{#switch: {{{range}}}{{#set:Ecosystem release={{{revision}}}}}}} {{#switch: {{{range}}}| and before | and after = | to = to {{#switch:{{EcosystemRelease/Revision | revision={{{revision2|}}}}} | unknown = <span title="This revision value is not valid">{{Highlight|unknown revision {{{revision2|}}}}} <sup>[[File:Warning.png|15px|link=]]</sup></span> | former = v{{{revision2|}}} | #default = <span title="{{EcosystemRelease/Components | revision={{{revision2|}}}}}">v{{{revision2}}} <sup>[[File:More_info.png|15px|link=]]</sup></span> }}}}| #default = {{#if: {{{range|}}} | <span title="This range value is not valid">{{Highlight|unknown range {{{range|}}}}} <sup>[[File:Warning.png|15px|link=]]</sup></span> |}} }}{{#set:Ecosystem release={{{revision}}}}} }}}}
Line 79: | Line 79: | ||
| Former revision that is part of a flow that is not the one associated with this wiki. |
| Former revision that is part of a flow that is not the one associated with this wiki. |
||
<pre style="white-space: pre-wrap;"> |
<pre style="white-space: pre-wrap;"> |
||
− | {{EcosystemRelease | revision=0.y.0}} |
+ | {{EcosystemRelease | revision=0.y.0}}<br>
|
+ | {{EcosystemRelease | revision=0.y.0 | range=and before}}<br> |
||
+ |
{{EcosystemRelease | revision=0.y.0 | range=and after}} |
||
</pre> |
</pre> |
||
| |
| |
||
− | {{EcosystemRelease | revision=0.y.0}} |
+ | {{EcosystemRelease | revision=0.y.0}}<br>
|
+ | {{EcosystemRelease | revision=0.y.0 | range=and before}}<br> |
||
+ |
{{EcosystemRelease | revision=0.y.0 | range=and after}} |
||
|- |
|- |
||
| Unspecified revision |
| Unspecified revision |
||
Line 115: | Line 119: | ||
| Former revision2 that is part of a flow that is not the one associated with this wiki. |
| Former revision2 that is part of a flow that is not the one associated with this wiki. |
||
<pre style="white-space: pre-wrap;"> |
<pre style="white-space: pre-wrap;"> |
||
− | {{EcosystemRelease | revision=x.0.0 | range=to | revision2=0.y.0}} |
+ | {{EcosystemRelease | revision=x.0.0 | range=to | revision2=0.y.0}}<br>
|
+ |
{{EcosystemRelease | revision=0.y.0 | range=to | revision2=0.y.0}} |
||
</pre> |
</pre> |
||
| |
| |
||
− | {{EcosystemRelease | revision=x.0.0 | range=to | revision2=0.y.0}} |
+ | {{EcosystemRelease | revision=x.0.0 | range=to | revision2=0.y.0}}<br>
|
+ |
{{EcosystemRelease | revision=0.y.0 | range=to | revision2=0.y.0}} |
||
|- |
|- |
||
| Ignored revision2 |
| Ignored revision2 |
||
Line 152: | Line 158: | ||
* Update the first "basic example" with the latest revision, and add in "more examples" the legacy revisions |
* Update the first "basic example" with the latest revision, and add in "more examples" the legacy revisions |
||
* Update, if needed, the below sentence "not valid in the flow (v1.y.z) associated"}} |
* Update, if needed, the below sentence "not valid in the flow (v1.y.z) associated"}} |
||
− | </noinclude>ecosystem release {{#switch:{{EcosystemRelease/Revision | revision={{{revision|}}}}} |
+ | </noinclude>ecosystem release {{#switch: {{{range|}}}
|
− | | unknown = <span title="This revision value is not valid">{{Highlight|unknown revision {{{revision|}}}}} <sup>[[File:Warning.png|15px|link=]]</sup></span> |
+ | | and before = ≤ |
− | | former = v{{{revision|}}}{{#set:Ecosystem release=revision of a previous flow {{{revision}}}}} |
+ | | and after = ≥ |
− | | #default = |
+ |
}} {{#switch:{{EcosystemRelease/Revision | revision={{{revision|}}}}} |
− | + | | unknown = <span title="This revision value is not valid">{{Highlight|unknown revision {{{revision|}}}}} <sup>[[File:Warning.png|15px|link=]]</sup></span>{{#set:Ecosystem release=unknown revision {{{revision}}}}}
|
|
− | + | | former = v{{{revision|}}}{{#set:Ecosystem release=revision of a previous flow {{{revision}}}}} |
|
− | + | | #default = <span title="{{EcosystemRelease/Components | revision={{{revision|}}}}}">v{{{revision}}} <sup>[[File:More_info.png|15px|link=]]</sup></span>{{#set:Ecosystem release={{{revision}}}}}}} {{#switch: {{{range}}} |
|
− | + | | and before | and after = |
|
− | + | | to = to {{#switch:{{EcosystemRelease/Revision | revision={{{revision2|}}}}} |
|
− | + |
| unknown = <span title="This revision value is not valid">{{Highlight|unknown revision {{{revision2|}}}}} <sup>[[File:Warning.png|15px|link=]]</sup></span> |
|
− | + |
| former = v{{{revision2|}}} |
|
− | + |
| #default = <span title="{{EcosystemRelease/Components | revision={{{revision2|}}}}}">v{{{revision2}}} <sup>[[File:More_info.png|15px|link=]]</sup></span> |
|
− | + |
}} |
|
− | + | | #default = {{#if: {{{range|}}} | <span title="This range value is not valid">{{Highlight|unknown range {{{range|}}}}} <sup>[[File:Warning.png|15px|link=]]</sup></span> |}} |
|
− | |||
− | |||
}} |
}} |