Approved version. Approved on: 18:29, 19 January 2021
You are viewing an old version of this page. Return to the latest version.
Difference between revisions of "Template:EcosystemRelease"
[quality revision] | [quality revision] |
m (Undo revision 76165 by Nathalie Sangouard (talk))
(Tag: Undo)
|
m
|
Contents
1 Usage[edit]
The EcosystemRelease template is used to indicate for which ecosystem release revision(s) of the flow associated with this wiki (e.g. v1.y.z ,or v2.y.z, or...), an article part (chapter, paragraph, table...) is valid. Per default (i.e. if this template is not used), any part of an article is valid for all ecosystem release revisions for which the entire article is valid.
It outputs a "standardized" string that might be used to name an article part.
Usage: {{EcosystemRelease | revision=<revision> | range =<range> | revision2=<revision2>}}
Where:
-
<revision> is the mandatory ecosystem release revision for which the article part is valid.
- The possible values for this parameter are available in the EcosystemRelease/Revision template.
- The optional <range> and <revision2> parameters allow to define a range of revisions.
-
<range> is the optional range of the ecosystem release revisions for which the article part is valid. The possible values are:
- and before: the article part is valid only for the revision(s) less than or equal to <revision>
- and after: the article part is valid only for the revision(s) greater than or equal to <revision>
- to: the article part is only valid from <revision> to <revision2>
-
<revision2> is the mandatory ecosystem release upper revision for which the article part is valid, when <range> is set to "to"; in this case, <revision> becomes the lower revision for which the article part is valid.
- This parameter is ignored if <range> is either not set, or set to another value than "to".
If the mouse is left over a revision (or the icon), a popup window shows, for that revision:
- the versions of the Linux kernel, U-Boot, TF-A and OP-TEE
- the version of the STM32Cube MPU Package
- the version of OpenEmbedded
- the version of Android
This information comes from the EcosystemRelease/Components template.
2 Basic examples[edit]
You type | You get |
---|---|
A specific revision (revision 2.1.0): the next a former one {{EcosystemRelease | revision=2.1.0}} |
ecosystem release v2.1.0 |
Another specific revision (revision 2.0.0): the latest a former one {{EcosystemRelease | revision=2.0.0}} |
ecosystem release v2.0.0 |
Another specific revision (revision 3.0.0): the latest one
{{EcosystemRelease | revision=3.0.0}}
|
ecosystem release v3.0.0 |
Revisions that are lower than or equal to a revision {{EcosystemRelease | revision=x.1.0 | range=and before}} |
|
Revisions that are greater than or equal to a revision {{EcosystemRelease | revision=x.1.0 | range=and after}} |
|
Range of revisions {{EcosystemRelease | revision=x.0.0 | range=to | revision2=x.1.0}} |
3 More examples[edit]
4 Code[edit]
<noinclude> ==Usage== The [[Template:EcosystemRelease|EcosystemRelease]] template is used '''to indicate for which ecosystem release revision(s)''' of the flow associated with this wiki (e.g. v1.y.z ,or v2.y.z, or...), '''an article part (chapter, paragraph, table...) is valid'''. Per default (i.e. if this template is not used), any part of an article is valid for all ecosystem release revisions for which the entire article is valid. It outputs a "standardized" string that might be used to name an article part. Usage: <nowiki>{{</nowiki>EcosystemRelease | revision={{HighlightParam|<revision>}} | range ={{HighlightParam|<range>}} | revision2={{HighlightParam|<revision2>}}}} Where: * {{HighlightParam|<revision>}} is the '''mandatory''' ecosystem release revision for which the article part is valid. ** The possible values for this parameter are available in the [[Template:EcosystemRelease/Revision|EcosystemRelease/Revision]] template. ** The optional {{HighlightParam|<range>}} and {{HighlightParam|<revision2>}} parameters allow to define a range of revisions. * {{HighlightParam|<range>}} is the '''optional''' range of the ecosystem release revisions for which the article part is valid. The possible values are: ** '''and before''': the article part is valid only for the revision(s) less than or equal to {{HighlightParam|<revision>}} ** '''and after''': the article part is valid only for the revision(s) greater than or equal to {{HighlightParam|<revision>}} ** '''to''': the article part is only valid from {{HighlightParam|<revision>}} to {{HighlightParam|<revision2>}} * {{HighlightParam|<revision2>}} is the '''mandatory''' ecosystem release upper revision for which the article part is valid, '''when {{HighlightParam|<range>}} is set to "to'''"; in this case, {{HighlightParam|<revision>}} becomes the lower revision for which the article part is valid. ** This parameter is ignored if {{HighlightParam|<range>}} is either not set, or set to another value than "'''to'''". If the mouse is left over a revision (or the <sup>[[File:More_info.png|15px|link=]]</sup> icon), '''a popup window''' shows, for that revision: * the versions of the Linux kernel, U-Boot, TF-A and OP-TEE * the version of the STM32Cube MPU Package * the version of OpenEmbedded * the version of Android This information comes from the [[Template:EcosystemRelease/Components|EcosystemRelease/Components]] template. ==Basic examples== {| class="st-table" ! style="width: 50%;" | You type !! You get |- | A specific revision (revision 2.1.0): the nexta former one<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=2.1.0}}</pre> | {{EcosystemRelease | revision=2.1.0}} |- | Another specific revision (revision 2.0.0): the latesta former one<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=2.0.0}}</pre> | {{EcosystemRelease | revision=2.0.0}} |- | Another specific revision (revision 3.0.0): the latest one<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=3.0.0}}</pre> | {{EcosystemRelease | revision=3.0.0}} |- | Revisions that are lower than or equal to a revision<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.1.0 | range=and before}}</pre> | {{EcosystemRelease | revision=x.1.0 | range=and before}} |- | Revisions that are greater than or equal to a revision<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.1.0 | range=and after}}</pre> | {{EcosystemRelease | revision=x.1.0 | range=and after}} |- | Range of revisions<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.0.0 | range=to | revision2=x.1.0}}</pre> | {{EcosystemRelease | revision=x.0.0 | range=to | revision2=x.1.0}} |} ==More examples== {| class="st-table" ! style="width: 50%;" | You type !! You get |- | Revision x.1.0<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.1.0}}</pre> | {{EcosystemRelease | revision=x.1.0}} |- | Revision x.0.0<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.0.0}}</pre> | {{EcosystemRelease | revision=x.0.0}} |- | Former revision that is part of a flow that is not the one associated with this wiki.<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=0.y.0}}<br> {{EcosystemRelease | revision=0.y.0 | range=and before}}<br> {{EcosystemRelease | revision=0.y.0 | range=and after}}</pre> | {{EcosystemRelease | revision=0.y.0}}<br> {{EcosystemRelease | revision=0.y.0 | range=and before}}<br> {{EcosystemRelease | revision=0.y.0 | range=and after}} |- | Unspecified revision<pre style="white-space: pre-wrap;"> {{EcosystemRelease}}</pre> | {{EcosystemRelease}} |- | Unknown revision<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=10.20.30}}</pre> | {{EcosystemRelease | revision=10.20.30}} |- | Unspecified revision2<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.1.0 | range=to}}</pre> | {{EcosystemRelease | revision=x.1.0 | range=to}} |- | Unknown revision2<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.1.0 | range=to | revision2=10.20.30}}</pre> | {{EcosystemRelease | revision=x.1.0 | range=to | revision2=10.20.30}} |- | Former revision2 that is part of a flow that is not the one associated with this wiki.<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.0.0 | range=to | revision2=0.y.0}}<br> {{EcosystemRelease | revision=0.y.0 | range=to | revision2=0.y.0}}</pre> | {{EcosystemRelease | revision=x.0.0 | range=to | revision2=0.y.0}}<br> {{EcosystemRelease | revision=0.y.0 | range=to | revision2=0.y.0}} |- | Ignored revision2<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.0.0 | range=and after | revision2=x.1.0}}</pre> | {{EcosystemRelease | revision=x.0.0 | range=and after | revision2=x.1.0}} |- | Unknown range<pre style="white-space: pre-wrap;"> {{EcosystemRelease | revision=x.1.0 | range=error}}</pre> | {{EcosystemRelease | revision=x.1.0 | range=error}} |- | Check that there's no space before and after the text<pre style="white-space: pre-wrap;"> BEFORE{{EcosystemRelease | revision=x.0.0}}AFTER<br> BEFORE{{EcosystemRelease | revision=x.1.0 | range=and before}}AFTER<br> BEFORE{{EcosystemRelease | revision=x.1.0 | range=and after}}AFTER<br> BEFORE{{EcosystemRelease | revision=x.0.0 | range=to | revision2=x.1.0}}AFTER</pre> | BEFORE{{EcosystemRelease | revision=x.0.0}}AFTER<br> BEFORE{{EcosystemRelease | revision=x.1.0 | range=and before}}AFTER<br> BEFORE{{EcosystemRelease | revision=x.1.0 | range=and after}}AFTER<br> BEFORE{{EcosystemRelease | revision=x.0.0 | range=to | revision2=x.1.0}}AFTER |} ==Code== {{UpdateNeededForNewRelease| * Update the first "basic example" with the latest revision, and add in "more examples" the legacy revisions * Update, if needed, the below sentence "not valid in the flow (v1.y.z) associated"}}</noinclude>ecosystem release {{#switch: {{{range|}}} | and before = ≤ | and after = ≥ }} {{#switch:{{EcosystemRelease/Revision | revision={{{revision|}}}}} | unknown = <span title="This revision value is not valid">{{Highlight|unknown revision {{{revision|}}}}} <sup>[[File:Warning.png|15px|link=]]</sup></span>{{#set:Ecosystem release=unknown revision {{{revision}}}}} | former = v{{{revision|}}}{{#set:Ecosystem release=revision of a previous flow {{{revision}}}}} | #default = <span title="{{EcosystemRelease/Components | revision={{{revision|}}}}}">v{{{revision}}} <sup>[[File:More_info.png|15px|link=]]</sup></span>{{#set:Ecosystem release={{{revision}}}}}}} {{#switch: {{{range}}} | and before | and after = | to = to {{#switch:{{EcosystemRelease/Revision | revision={{{revision2|}}}}} | unknown = <span title="This revision value is not valid">{{Highlight|unknown revision {{{revision2|}}}}} <sup>[[File:Warning.png|15px|link=]]</sup></span> | former = v{{{revision2|}}} | #default = <span title="{{EcosystemRelease/Components | revision={{{revision2|}}}}}">v{{{revision2}}} <sup>[[File:More_info.png|15px|link=]]</sup></span> }} | #default = {{#if: {{{range|}}} | <span title="This range value is not valid">{{Highlight|unknown range {{{range|}}}}} <sup>[[File:Warning.png|15px|link=]]</sup></span> |}} }}
Line 30: | Line 30: | ||
! style="width: 50%;" | You type !! You get |
! style="width: 50%;" | You type !! You get |
||
|- |
|- |
||
− | | A specific revision (revision 2.1.0): |
+ | | A specific revision (revision 2.1.0): a former one |
<pre style="white-space: pre-wrap;"> |
<pre style="white-space: pre-wrap;"> |
||
{{EcosystemRelease | revision=2.1.0}} |
{{EcosystemRelease | revision=2.1.0}} |
||
Line 37: | Line 37: | ||
{{EcosystemRelease | revision=2.1.0}} |
{{EcosystemRelease | revision=2.1.0}} |
||
|- |
|- |
||
− | | Another specific revision (revision 2.0.0): |
+ | | Another specific revision (revision 2.0.0): a former one |
<pre style="white-space: pre-wrap;"> |
<pre style="white-space: pre-wrap;"> |
||
{{EcosystemRelease | revision=2.0.0}} |
{{EcosystemRelease | revision=2.0.0}} |
||
Line 43: | Line 43: | ||
| |
| |
||
{{EcosystemRelease | revision=2.0.0}} |
{{EcosystemRelease | revision=2.0.0}} |
||
+ | |- |
||
+ | | Another specific revision (revision 3.0.0): the latest one |
||
+ | <pre style="white-space: pre-wrap;"> |
||
+ | {{EcosystemRelease | revision=3.0.0}} |
||
+ | </pre> |
||
+ | | |
||
+ | {{EcosystemRelease | revision=3.0.0}} |
||
|- |
|- |
||
| Revisions that are lower than or equal to a revision |
| Revisions that are lower than or equal to a revision |