Difference between revisions of "TIM Linux driver"
[quality revision] | [quality revision] |
m
|
m
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
Contents
1 Article purpose[edit]
This article introduces the TIM Linux® driver for the TIM internal peripheral[1]:
- Which TIM features are supported by the driver
- How to configure, use and debug the driver
- What is the driver structure, and where the source code can be found.
2 Short description[edit]
The TIM[1] Linux driver (kernel space) is based on the PWM, IIO and IIO counter frameworks. It provides several functionalities:
MFD driver:
- handles registers, clock and DMA[2] resources
- detects the TIM counter resolution, e.g. 16 or 32 bits.
PWM driver:
- detects the number of TIM channels.
- handles PWM output channels.
- handles PWM capture channels (input). Note that the PWM capture relies on DMA, which is handled by the MFD core.
IIO driver:
- handles hardware trigger sources (synchronously with PWM) for other internal peripherals such as ADC[3], DAC[4], DFSDM[5].
counter driver:
- handles the quadrature encoder interface[6].
3 Configuration[edit]
3.1 Kernel configuration[edit]
Activate the TIM[1] Linux driver in the kernel configuration using the Linux Menuconfig tool: Menuconfig or how to configure kernel.
Enable the following configurations (and their dependencies):
- CONFIG_MFD_STM32_TIMERS
- CONFIG_PWM_STM32
- CONFIG_IIO_STM32_TIMER_TRIGGER
- CONFIG_STM32_TIMER_CNT
Device Drivers --->
-> Multifunction device drivers --->
<*> Support for STM32 Timers
-> Pulse-width modulation (PWM) support --->
<*> STMicroelectronics STM32 PWM
-> Industrial I/O support --->
-> Triggers - standalone --->
<*> STM32 timer trigger
-> Counter support --->
<*> STM32 Timer encoder counter driver
3.2 Device tree[edit]
Refer to the TIM device tree configuration article when configuring the TIM Linux kernel driver.
4 How to use[edit]
How to use PWM with sysfs interface
How to set up a TIM or LPTIM trigger using the sysfs interface
How to use the quadrature encoder with the sysfs interface
5 How to trace and debug[edit]
The TIM[1] Linux driver can access the timer registers through REGMAP.
It comes with debugfs[7] entries, which allow dumping registers:
$ cd /sys/kernel/debug/regmap $ ls 40004000.timer 44000000.timer $ cd 44000000.timer $ cat registers 000: 00000081 004: 00000000 008: 00000000 00c: 00000000 ...
It also comes with tracepoints[8]:
$ cd /sys/kernel/debug/tracing $ cat available_events | grep regmap ... regmap:regmap_reg_read regmap:regmap_reg_write
6 Source code location[edit]
The TIM Linux driver source code is composed of:
- stm32-timers.c MFD driver to handle common resources: registers, clock, dmas.
- pwm-stm32.c PWM driver to handle PWM channel(s).
- stm32-timer-trigger.c IIO driver to handle trigger source for other internal peripherals and .
- stm32-timer-cnt.c counter driver to handle the quadrature encoder interface.
- include/linux/mfd/stm32-timers.h and include/linux/iio/timer/stm32-timer-trigger.h header files
7 References[edit]
- ↑ 1.01.11.21.3 TIM internal peripheral
- ↑ DMA_internal_peripheral
- ↑ ADC internal peripheral
- ↑ DAC internal peripheral
- ↑ DFSDM internal peripheral
- ↑ Incremental encoder Incremental encoder overview
- ↑ Debugfs
- ↑ Ftrace
{{EcosystemFlow/Warning| flow=Current}}<noinclude>{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x,STM32MP15x }}</noinclude> == Article purpose == This article introduces the TIM Linux<sup>®</sup> driver for the TIM internal peripheral<ref name="TIM internal peripheral">[[TIM internal peripheral]]</ref>: * Which TIM features are supported by the driver * How to configure, use and debug the driver * What is the driver structure, and where the source code can be found. {{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 16:48, 13 November 2020 (CET)<br />Article to be updated to be compliant with ecosystem v2.0.0 (BZ 80500)}} == Short description == The ''TIM''<ref name="TIM internal peripheral"/> Linux driver (kernel space) is based on the [[PWM overview|PWM]] and , [[IIO overview|IIO]] and <span style="color: {{STLightBlue}};">counter</span> frameworks. It provides several functionalities: '''MFD driver''': * handles registers, clock and DMA<ref name="DMA internal peripheral">[[DMA_internal_peripheral]]</ref> resources * detects the TIM counter resolution, e.g. 16 or 32 bits. '''PWM driver''': * detects the number of TIM channels. * handles '''PWM output''' channels. * handles '''PWM capture''' channels (input). Note that the PWM capture relies on DMA, which is handled by the MFD core. '''IIO driver''': * handles hardware '''trigger sources''' (synchronously with PWM) for other internal peripherals such as ADC<ref name="adc_internal">[[ADC internal peripheral]]</ref>, DAC<ref name="dac_internal">[[DAC internal peripheral]]</ref>, DFSDM<ref name="dfsdm_internal">[[DFSDM internal peripheral]]</ref>.'''counter driver''':* handles the '''quadrature encoder''' interface<ref>[https://en.wikipedia.org/wiki/Rotary_encoder#Incremental_encoder Incremental encoder] Incremental encoder overview</ref>. == Configuration == === Kernel configuration === Activate the TIM<ref name="TIM internal peripheral"/> Linux driver in the kernel configuration using the Linux Menuconfig tool: [[Menuconfig or how to configure kernel]]. Enable the following configurations (and their dependencies): * CONFIG_MFD_STM32_TIMERS * CONFIG_PWM_STM32 * CONFIG_IIO_STM32_TIMER_TRIGGER * CONFIG_STM32_TIMER_CNT Device Drivers ---> -> Multifunction device drivers ---><*> Support for STM32 Timers -> Pulse-width modulation (PWM) support ---><*> STMicroelectronics STM32 PWM -> Industrial I/O support ---> -> Triggers - standalone ---><*> STM32 timer trigger -> Counter support ---><*> STM32 Timer encoder counter driver === Device tree === Refer to the [[TIM device tree configuration]] article when configuring the TIM Linux kernel driver. == How to use == [[PWM_overview#How_to_use_PWM_with_sysfs_interface|How to use PWM with sysfs interface]] [[How to use the IIO user space interface#How to set up a TIM or LPTIM trigger using the sysfs interface|How to set up a TIM or LPTIM trigger using the sysfs interface]] [[How to use the IIO user space interface#How to use the quadrature encoder with the sysfs interface|How to use the quadrature encoder with the sysfs interface]] == How to trace and debug == The ''TIM''<ref name="TIM internal peripheral"/> Linux driver can access the timer registers through REGMAP. It comes with debugfs<ref name="debugfs">[[Debugfs]]</ref> entries, which allow dumping registers: $ cd /sys/kernel/debug/regmap $ ls 40004000.timer 44000000.timer $ cd 44000000.timer $ cat registers 000: 00000081 004: 00000000 008: 00000000 00c: 00000000 ... It also comes with tracepoints<ref name="ftrace">[[Ftrace]]</ref>: $ cd /sys/kernel/debug/tracing $ cat available_events | grep regmap ... regmap:regmap_reg_read regmap:regmap_reg_write == Source code location == The TIM Linux driver source code is composed of: * {{CodeSource | Linux kernel | drivers/mfd/stm32-timers.c | stm32-timers.c MFD driver}} to handle common resources: registers, clock, dmas. * {{CodeSource | Linux kernel | drivers/pwm/pwm-stm32.c | pwm-stm32.c PWM driver}} to handle PWM channel(s). * {{CodeSource | Linux kernel | drivers/iio/trigger/stm32-timer-trigger.c | stm32-timer-trigger.c IIO driver}} to handle trigger source for other internal peripherals and . * {{CodeSource | Linux kernel | drivers/counter/stm32-timer-cnt.c | stm32-timer-cnt.c counter driver}} to handle the quadrature encoder interface. * {{CodeSource | Linux kernel | include/linux/mfd/stm32-timers.h}} and {{CodeSource | Linux kernel | include/linux/iio/timer/stm32-timer-trigger.h}} header files ==References==<references /> <noinclude> [[Category:Timers]] [[Category:IIO]] {{PublicationRequestId | 9233 | 2018-10-15 | AnneJ}} {{ArticleBasedOnModel | Linux driver OpenSTLinux drivers article model}}</noinclude>
(4 intermediate revisions by the same user not shown) | |||
Line 1: | Line 1: | ||
− | {{ |
+ |
<noinclude>{{ApplicableFor
|
+ | |MPUs list=STM32MP13x, STM32MP15x |
||
+ | |MPUs checklist=STM32MP13x,STM32MP15x
|
||
+ | }}</noinclude>
|
||
== Article purpose == |
== Article purpose == |
||
This article introduces the TIM Linux<sup>®</sup> driver for the TIM internal peripheral<ref name="TIM internal peripheral">[[TIM internal peripheral]]</ref>: |
This article introduces the TIM Linux<sup>®</sup> driver for the TIM internal peripheral<ref name="TIM internal peripheral">[[TIM internal peripheral]]</ref>: |
||
Line 5: | Line 8: | ||
* How to configure, use and debug the driver |
* How to configure, use and debug the driver |
||
* What is the driver structure, and where the source code can be found. |
* What is the driver structure, and where the source code can be found. |
||
− | |||
− | |||
== Short description == |
== Short description == |
||
− | The ''TIM''<ref name="TIM internal peripheral"/> Linux driver (kernel space) is based on the [[PWM overview|PWM]] |
+ | The ''TIM''<ref name="TIM internal peripheral"/> Linux driver (kernel space) is based on the [[PWM overview|PWM]], [[IIO overview|IIO]] and <span style="color: {{STLightBlue}};">counter</span> frameworks. It provides several functionalities: |
'''MFD driver''': |
'''MFD driver''': |
||
Line 20: | Line 21: | ||
'''IIO driver''': |
'''IIO driver''': |
||
* handles hardware '''trigger sources''' (synchronously with PWM) for other internal peripherals such as ADC<ref name="adc_internal">[[ADC internal peripheral]]</ref>, DAC<ref name="dac_internal">[[DAC internal peripheral]]</ref>, DFSDM<ref name="dfsdm_internal">[[DFSDM internal peripheral]]</ref>. |
* handles hardware '''trigger sources''' (synchronously with PWM) for other internal peripherals such as ADC<ref name="adc_internal">[[ADC internal peripheral]]</ref>, DAC<ref name="dac_internal">[[DAC internal peripheral]]</ref>, DFSDM<ref name="dfsdm_internal">[[DFSDM internal peripheral]]</ref>. |
||
+ | '''counter driver''': |
||
* handles the '''quadrature encoder''' interface<ref>[https://en.wikipedia.org/wiki/Rotary_encoder#Incremental_encoder Incremental encoder] Incremental encoder overview</ref>. |
* handles the '''quadrature encoder''' interface<ref>[https://en.wikipedia.org/wiki/Rotary_encoder#Incremental_encoder Incremental encoder] Incremental encoder overview</ref>. |
||
Line 30: | Line 32: | ||
* CONFIG_PWM_STM32 |
* CONFIG_PWM_STM32 |
||
* CONFIG_IIO_STM32_TIMER_TRIGGER |
* CONFIG_IIO_STM32_TIMER_TRIGGER |
||
+ | * CONFIG_STM32_TIMER_CNT |
||
Device Drivers ---> |
Device Drivers ---> |
||
Line 39: | Line 42: | ||
-> Triggers - standalone ---> |
-> Triggers - standalone ---> |
||
<*> STM32 timer trigger |
<*> STM32 timer trigger |
||
+ | -> Counter support ---> |
||
+ | <*> STM32 Timer encoder counter driver |
||
=== Device tree === |
=== Device tree === |
||
Line 77: | Line 82: | ||
* {{CodeSource | Linux kernel | drivers/mfd/stm32-timers.c | stm32-timers.c MFD driver}} to handle common resources: registers, clock, dmas. |
* {{CodeSource | Linux kernel | drivers/mfd/stm32-timers.c | stm32-timers.c MFD driver}} to handle common resources: registers, clock, dmas. |
||
* {{CodeSource | Linux kernel | drivers/pwm/pwm-stm32.c | pwm-stm32.c PWM driver}} to handle PWM channel(s). |
* {{CodeSource | Linux kernel | drivers/pwm/pwm-stm32.c | pwm-stm32.c PWM driver}} to handle PWM channel(s). |
||
− | * {{CodeSource | Linux kernel | drivers/iio/trigger/stm32-timer-trigger.c | stm32-timer-trigger.c IIO driver}} to handle trigger source for other internal peripherals |
+ | * {{CodeSource | Linux kernel | drivers/iio/trigger/stm32-timer-trigger.c | stm32-timer-trigger.c IIO driver}} to handle trigger source for other internal peripherals.
|
+ |
* {{CodeSource | Linux kernel | drivers/counter/stm32-timer-cnt.c | stm32-timer-cnt.c counter driver}} to handle the quadrature encoder interface. |
||
* {{CodeSource | Linux kernel | include/linux/mfd/stm32-timers.h}} and {{CodeSource | Linux kernel | include/linux/iio/timer/stm32-timer-trigger.h}} header files |
* {{CodeSource | Linux kernel | include/linux/mfd/stm32-timers.h}} and {{CodeSource | Linux kernel | include/linux/iio/timer/stm32-timer-trigger.h}} header files |
||
Line 87: | Line 93: | ||
[[Category:IIO]] |
[[Category:IIO]] |
||
{{PublicationRequestId | 9233 | 2018-10-15 | AnneJ}} |
{{PublicationRequestId | 9233 | 2018-10-15 | AnneJ}} |
||
− | {{ArticleBasedOnModel | |
+ | {{ArticleBasedOnModel |OpenSTLinux drivers article model}} |
</noinclude> |
</noinclude> |