Difference between revisions of "TF-A overview"

[quality revision] [quality revision]
m
 

Template:ArticleMainWriter Template:ArticleApprovedVersion

1 Trusted Firmware-A[edit]

Zoom out to STM32MPU Embedded Software

Trusted Firmware-A is a reference implementation of secure-world software provided by Arm®. It was first designed for Armv8-A platforms, and has been adapted to be used on Armv7-A platforms by STMicroelectronics. Arm is transferring the Trusted Firmware project to be managed as an open-source project by Linaro.[1]

It is used as the first-stage boot loader (FSBL) on STM32 MPU platforms when using the trusted boot chain.

The code is open source, under a BSD-3-Clause licence, and can be found on github [2], including an up-to-date documentation about Trusted Firmware-A implementation [3].

Trusted Firmware-A also implements a secure monitor with various Arm interface standards:

  • The power state coordination interface (PSCI) [4]
  • Trusted board boot requirements (TBBR) [5]
  • SMC calling convention [6]
  • System control and management interface [7]

Trusted Firmware-A is usually shortened to TF-A.

2 Architecture[edit]

The global architecture of TF-A is explained in the Trusted Firmware-A design [8] document.

TF-A is divided into several binaries, each with a dedicated main role. For 32-bit Arm processors (AArch32), it is divided into four steps (in order of execution):

  • Boot loader stage 1 (BL1) application processor trusted ROM
  • Boot loader stage 2 (BL2) trusted boot firmware
  • Boot loader stage 3-2 (BL32) runtime software
  • Boot loader stage 3-3 (BL33) non-trusted firmware

BL1, BL2 and BL32 are parts of TF-A.

BL1 is now optional, and can be removed by enabling the compilation flag: BL2_AT_EL3. It is then removed for the STM32MP1, as all BL1 tasks are done by ROM code, or BL2.

BL33 is outside of TF-A. This is the first non-secure code loaded by TF-A. During the boot sequence, this is the secondary stage boot loader (SSBL). For STM32 MPU platforms, the SSBL is U-Boot by default.

TF-A can manage its configuration with a device tree, as this is the case on STM32MP1. It is a reduced version of the Linux kernel one, with only the devices used during boot. It can be configured with STM32CubeMX.

In STMicroelectronics' implementation, the 2 binaries, BL2 and BL32, and the device tree are put together in a single binary, to be loaded at once to the SYSRAM by the ROM code.

Boot ATF.png

TF-A loading steps:

  1. ROM code loads TF-A binary and calls BL2
  2. BL2 prepares BL32
  3. BL2 loads BL33
  4. BL2 calls BL32
  5. BL32 calls BL33

3 Boot loader stages[edit]

3.1 BL1[edit]

BL1 is the first stage executed, and is designed to act as ROM code; it is loaded and executed in internal RAM. It is not used for the STM32MP1. As the STM32MP1 has its own proprietary ROM code, this part can be removed and BL2 is then the first TF-A binary to be executed.

3.2 BL2[edit]

BL2 (trusted boot firmware) is in charge of loading the next-stage images (secure and non secure). To achieve this role, BL2 has to initialize all the required peripherals.

It has to initialize the security components.
For the STM32MP15, these security peripherals are:

BL2 is also in charge of initializing the DDR and clock tree.

The boot peripheral has to be initialized.
On the STM32MP15, it can be one of the following:

USB (OTG internal peripheral) or UART(USART internal peripheral) are used when Flashing, see STM32CubeProgrammer for more details.

BL2 also integrates image verification and authentication. Authentication is achieved by calling BootROM verification services.

At the end of its execution, after having loaded BL32 and the next boot stage (BL33), BL2 jumps to BL32.

3.3 BL32[edit]

BL32 provides runtime secure services. In TF-A, the BL32 default implementation is SP_min solution. It is described in the TF-A functionality list [3] as: "A minimal AArch32 Secure Payload (SP_MIN) to demonstrate PSCI [4] library integration with AArch32 EL3 Runtime Software."

This minimal implementation can be replaced with a trusted OS or trusted environment execution (TEE), such as OP-TEE. Both solutions (SP_min or OP-TEE) are supported by STMicroelectronics for STM32MP1.

BL32 acts as a secure monitor and thus provides secure services to non-secure OSs. These services are called by non-secure software with secure monitor calls [6].

This code is in charge of standard service calls, like PSCI [4].

It also provides STMicroelectronics dedicated services, to access secure peripherals. On the STM32MP1, these services are used to access RCC internal peripheral, PWR internal peripheral, RTC internal peripheral or BSEC internal peripheral.

4 References[edit]


<noinclude>

{{ArticleMainWriter | YannG}}
{{ ArticleApprovedVersion| YannG | NathalieS, GeraldB, LionelD, NicolasLB | YannG - 22Jan'18 | PhilipS - 24Oct'18 - 9178 | 5Nov'18}}
[[Category:Trusted Firmware-A (TF-A)| 01]]</noinclude>

== Trusted Firmware-A ==
[[File: STM32MPU Embedded Software architecture overview.png|link=STM32MPU Embedded Software architecture overview|thumb|Zoom out to STM32MPU Embedded Software]]
Trusted Firmware-A is a reference implementation of secure-world software provided by Arm<sup>&reg;</sup>. It was first designed for Armv8-A platforms, and has been adapted to be used on Armv7-A platforms by STMicroelectronics. Arm is transferring the Trusted Firmware project to be managed as an open-source project by Linaro.<ref>https://www.trustedfirmware.org/</ref>


It is used as the first-stage boot loader (FSBL) on STM32 MPU platforms when using the [[Boot_chains_overview#STM32MP boot chains|trusted boot chain]].

The code is open source, under a BSD-3-Clause licence, and can be found on github<ref>https://github.com/ARM-software/arm-trusted-firmware</ref>, including an up-to-date documentation about Trusted Firmware-A implementation <ref name=readme>{{CodeSource | TF-A | readme.rst}}</ref>.

Trusted Firmware-A also implements a secure monitor with various Arm interface standards:
* The power state coordination interface (PSCI) <ref name=psci>http://infocenter.arm.com/help/topic/com.arm.doc.den0022d/Power_State_Coordination_Interface_PDD_v1_1_DEN0022D.pdf</ref>

* Trusted board boot requirements (TBBR) <ref>Arm DEN0006C-1</ref>

* SMC calling convention <ref name=smc>http://infocenter.arm.com/help/topic/com.arm.doc.den0028b/ARM_DEN0028B_SMC_Calling_Convention.pdf </ref>

* System control and management interface <ref>http://infocenter.arm.com/help/topic/com.arm.doc.den0056a/DEN0056A_System_Control_and_Management_Interface.pdf </ref>


Trusted Firmware-A is usually shortened to TF-A.

== Architecture ==

The global architecture of TF-A is explained in the Trusted Firmware-A design <ref>{{CodeSource | TF-A | docs/firmware-design.rst}}</ref> document.

TF-A is divided into several binaries, each with a dedicated main role. For 32-bit Arm processors (AArch32), it is divided into four steps (in order of execution):
* Boot loader stage 1 (BL1) application processor trusted ROM
* Boot loader stage 2 (BL2) trusted boot firmware
* Boot loader stage 3-2 (BL32) runtime software
* Boot loader stage 3-3 (BL33) non-trusted firmware

BL1, BL2 and BL32 are parts of TF-A.

BL1 is now optional, and can be removed by enabling the compilation flag: BL2_AT_EL3. It is then removed for the STM32MP1, as all BL1 tasks are done by [[:Category:ROM code|ROM code]], or BL2.

BL33 is outside of TF-A. This is the first non-secure code loaded by TF-A. During the boot sequence, this is the secondary stage boot loader (SSBL). For STM32 MPU platforms, the SSBL is [[U-Boot overview|U-Boot]] by default.

TF-A can manage its configuration with a [[STM32MP15_device_tree#Device tree structure for Linux, U-Boot and TF-A|device tree]], as this is the case on STM32MP1. It is a reduced version of the Linux kernel one, with only the devices used during boot. It can be configured with [[STM32CubeMX]].

In STMicroelectronics' implementation, the 2 binaries, BL2 and BL32, and the device tree are put together in a single binary, to be loaded at once to the SYSRAM by the ROM code.

[[File:Boot_ATF.png|center|link=]]

[[File:Boot_ATF_legend.png|center|link=]]

TF-A loading steps:
# ROM code loads TF-A binary and calls BL2
# BL2 prepares BL32
# BL2 loads BL33
# BL2 calls BL32
# BL32 calls BL33

== Boot loader stages ==

=== BL1 ===
BL1 is the first stage executed, and is designed to act as ROM code; it is loaded and executed in internal RAM.
It is not used for the STM32MP1. As the  STM32MP1 has its own proprietary [[:Category:ROM code|ROM code]], this part can be removed and BL2 is then the first TF-A binary to be executed.

=== BL2 ===
BL2 (trusted boot firmware) is in charge of loading the next-stage images (secure and non secure).
To achieve this role, BL2 has to initialize all the required peripherals.

It has to initialize the security components.<br>

For the STM32MP15, these security peripherals are:
* boot and security, and OTP control ([[BSEC internal peripheral]])
* extended TrustZone protection controller ([[ETZPC internal peripheral]])
* TrustZone address space controller for DDR ([[TZC internal peripheral]])

BL2 is also in charge of initializing the DDR and clock tree.

The boot peripheral has to be initialized.<br>

On the STM32MP15, it can be one of the following:
* SD-card via the [[SDMMC internal peripheral]]
* eMMC via the [[SDMMC internal peripheral]]
* NAND via the [[FMC internal peripheral]]
* NOR via the [[QUADSPI internal peripheral]]

USB ([[OTG internal peripheral]]) or UART([[USART internal peripheral]]) are used when Flashing, see [[STM32CubeProgrammer]] for more details.

BL2 also integrates image verification and authentication. Authentication is achieved by calling [[STM32MP15 ROM code overview|BootROM]] verification services.

At the end of its execution, after having loaded BL32 and the next boot stage (BL33), BL2 jumps to BL32.

=== BL32 ===
BL32 provides runtime secure services. In TF-A, the BL32 default implementation is SP_min solution.
It is described in the TF-A functionality list <ref name=readme/> as:
"A minimal AArch32 Secure Payload (SP_MIN) to demonstrate PSCI <ref name=psci/> library integration with AArch32 EL3 Runtime Software."

This minimal implementation can be replaced with a trusted OS or trusted environment execution (TEE), such as [[OP-TEE overview|OP-TEE]]. 
Both solutions (SP_min or OP-TEE) are supported by STMicroelectronics for STM32MP1.

BL32 acts as a secure monitor and thus provides secure services to non-secure OSs. These services are called by non-secure software with secure monitor calls <ref name=smc/>.

This code is in charge of standard service calls, like PSCI <ref name=psci/>.<br/>


It also provides STMicroelectronics dedicated services, to access secure peripherals. On the  STM32MP1, these services are used to access [[RCC internal peripheral]], [[PWR internal peripheral]], [[RTC internal peripheral]] or [[BSEC internal peripheral]].

==References==<references />

<noinclude>

[[Category:Trusted Firmware-A (TF-A)| 01]]
{{PublicationRequestId | 9178 | 2018-10-24 | PhilipS}}</noinclude>
Line 1: Line 1:
<noinclude>
 
{{ArticleMainWriter | YannG}}
 
{{ ArticleApprovedVersion| YannG | NathalieS, GeraldB, LionelD, NicolasLB | YannG - 22Jan'18 | PhilipS - 24Oct'18 - 9178 | 5Nov'18}}
 
[[Category:Trusted Firmware-A (TF-A)| 01]]
 
</noinclude>
 
 
 
== Trusted Firmware-A ==
 
== Trusted Firmware-A ==
 
[[File: STM32MPU Embedded Software architecture overview.png|link=STM32MPU Embedded Software architecture overview|thumb|Zoom out to STM32MPU Embedded Software]]
 
[[File: STM32MPU Embedded Software architecture overview.png|link=STM32MPU Embedded Software architecture overview|thumb|Zoom out to STM32MPU Embedded Software]]
Line 100: Line 94:
 
==References==
 
==References==
 
<references />
 
<references />
  +
  +
<noinclude>
  +
[[Category:Trusted Firmware-A (TF-A)| 01]]
  +
{{PublicationRequestId | 9178 | 2018-10-24 | PhilipS}}
  +
</noinclude>