Difference between revisions of "TF-A overview"
[quality revision] | [quality revision] |
m
|
Yann Gautier (talk | contribs)
m
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
Contents
1 Trusted Firmware-A[edit]
Trusted Firmware-A is a reference implementation of secure-world software provided by Arm®. It was first designed for Armv8-A platforms, and has been adapted to be used on Armv7-A platforms by STMicroelectronics. Arm is transferring Trusted Firmware-A is part of the Trusted Firmware project to be managed as that is an open -source governance community project hosted by Linaro.[1]
It is used as the first-stage boot loader (FSBL) on STM32 MPU platforms when using the trusted boot chain.
The code is open source, under a BSD-3-Clause licencelicense, and can be found on github Linaro project page [2], including an up-to-date documentation about Trusted Firmware-A implementation [3].
Trusted Firmware-A also implements a secure monitor set of features with various Arm interface standards:
- The power state coordination interface (PSCI) [4]
- Trusted board boot requirements (TBBR) [5]
- SMC calling convention [65]
- System control and management interface [76]
Trusted Firmware-A is usually shortened to TF-A.
2 Architecture[edit]
The global architecture of TF-A is explained in the Trusted Firmware-A design [83] document.
TF-A is divided into several binaries, each with a dedicated main role.
For 32-bit Arm processors (AArch32), it the trusted boot is divided into four steps stages (in order of execution):
- Boot loader stage 1 (BL1) application processor trusted ROM
- Boot loader stage 2 (BL2) trusted boot firmware
- Boot loader stage 3-2 (BL32) trusted runtime softwarefirmware
- Boot loader stage 3-3 (BL33) non-trusted firmware
BL1, BL2 and BL32 are parts of TF-A.
Because STM32 MPU platforms uses a dedicated ROM code, the BL1 is now optional, and can be removed by enabling the compilation flag: BL2boot stage is then removed. ROM code expects the BL2 to run at EL3 execution level. This mode is selected when the BL2_AT_EL3 . It is then removed for the STM32MP1, as all BL1 tasks are done by ROM code, or BL2build flag is enabled.
BL33 is outside of TF-A. This is the first non-secure code loaded by TF-A. During the boot sequence, this is the secondary stage boot loader (SSBL). For STM32 MPU platforms, the SSBL is U-Boot by default.
TF-A can manage its configuration with a device tree, as this is the case on STM32MP1. It is . In the BL2 stage, it is a reduced version of the Linux kernel one, with only the required devices used during boot. It can be configured with STM32CubeMX.
In STMicroelectronics' implementation, the 2 binaries, BL2 and BL32, and the device tree are put together in a single binary, to be loaded at once to the SYSRAM by the ROM code.
TF-A loading steps:
- ROM code loads TF-A binary and calls BL2
- BL2 prepares loads BL32
- BL2 loads BL33
- BL2 calls BL32
- BL32 calls BL33
3 Boot loader stages[edit]
3.1 BL1[edit]
BL1 is the first stage executed, and is designed to act as ROM code; it is loaded and executed in internal RAM. It is not used for the STM32MP1STM32 MPU. As the STM32MP1 STM32 MPU has its own proprietary ROM code, this part can be removed and BL2 is then the first TF-A binary to be executed.
3.2 BL2[edit]
BL2 (trusted boot firmware) is in charge of loading the next-stage images (secure and non secure). To achieve this role, BL2 has to initialize all the required peripherals.
It has to initialize the security components.
For the STM32MP15, these security peripherals are:
- boot and security, and OTP control (BSEC internal peripheral)
- extended TrustZone protection controller (ETZPC internal peripheral)
- TrustZone address space controller for DDR (TZC internal peripheral)
BL2 is also in charge of initializing the DDR and clock tree.
The boot peripheral has to be initialized.
On the STM32MP15, it can be one of the following:
- SD-card via the SDMMC internal peripheral
- eMMC via the SDMMC internal peripheral
- NAND via the FMC internal peripheral
- NOR via the QUADSPI internal peripheral
USB (OTG internal peripheral) or UART(USART internal peripheral) are used when Flashing, see STM32CubeProgrammer for more details.
BL2 also integrates image verification and authentication. Authentication is achieved by calling BootROM verification services.- System components: clocks, DDR, ...
- Security components: cryptographic peripheral, memory firewall, ...
- Storage
BL2 offers different features to load and authenticate images.
At the end of its execution, after having loaded BL32 and the next boot stage (BL33), BL2 jumps to BL32.
3.3 BL32[edit]
BL32 provides runtime secure services. In
On Armv7 architecture, the BL32 must embed a Secure Monitor as it will be executed in the same privilege level (PL1-SVC Secure). TF-A , the BL32 default implementation is provides a minimal monitor implementation: SP-MIN solution. It is described in the TF-A functionality list [3] as: "A minimal AArch32 Secure Payload (SP-MIN) to demonstrate PSCI [4] library integration with AArch32 EL3 Runtime Software."
This minimal implementation can be replaced with a trusted OS or trusted environment execution (TEE), such as OP-TEE. Both solutions ( that also embeds a secure monitor on Armv7.
![]() |
STM32MP15 supports the SP-MIN |
but it is no more recommended. OP-TEE |
is the BL32 official solution. |
BL32 acts as a secure monitor and thus provides secure services to non-secure OSs. These services are called by non-secure software with secure monitor calls [65].
This code is in charge of standard service calls, like PSCI [4]or SCMI [6].
It also provides STMicroelectronics dedicated proprietary services , to access secure peripherals. On the STM32MP1, these services are used to access RCC internal peripheral, PWR internal peripheral, RTC internal peripheral or BSEC internal peripheralsome specific and limited secure peripherals (with secure access control).
4 References[edit]
- ↑ https://www.trustedfirmware.org/
- ↑ https://githubgit.comtrustedfirmware.org/ARMTF-softwareA/arm-trusted-firmware-a.git
- ↑ 3.0 3.1 readme.rst
- 3.2 Trusted Firmware-A documentation
- ↑ 4.04.14.2 http://infocenter.arm.com/help/topic/com.arm.doc.den0022d/Power_State_Coordination_Interface_PDD_v1_1_DEN0022D.pdf
- ↑ Arm DEN0006C-1
- ↑ 6.0 6.1 http://infocenter.arm.com/help/topic/com.arm.doc.den0028b/ARM_DEN0028B_SMC_Calling_Convention.pdf
- ↑ http://infocenter.arm.com/help/topic/com.arm.doc.den0056a/DEN0056A_System_Control_and_Management_Interface.pdf
- ↑ docs/firmware-design.rst
- ARM Power State Coordination Interface
- ↑ 5.0 5.1 SMC Calling Convention (SMCCC)
- ↑ 6.0 6.1 Arm System Control and Management Interface
== <noinclude>{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x,STM32MP15x }}</noinclude> == Trusted Firmware-A == [[File: STM32MPU Embedded Software architecture overview.png|link=STM32MPU Embedded Software architecture overview|thumb|Zoom out to STM32MPU Embedded Software]] Trusted Firmware-A is a reference implementation of secure-world software provided by Arm<sup>®</sup>. It was first designed for Armv8-A platforms, and has been adapted to be used on Armv7-A platforms by STMicroelectronics. Arm is transferring Trusted Firmware-A is part of the Trusted Firmware project to be managed as an open-source project that is an open governance community project hosted by Linaro.<ref>https://www.trustedfirmware.org/</ref> It is used as the first-stage boot loader (FSBL) on STM32 MPU platforms when using the [[Boot_chain_overview#STM32MP boot sequence|trusted boot chain]]. The code is open source, under a BSD-3-Clause licencelicense, and can be found on github<ref>https://github.com/ARM-software/arm-trusted-firmwareLinaro project page<ref>https://git.trustedfirmware.org/TF-A/trusted-firmware-a.git</ref>, including an up-to-date documentation about Trusted Firmware-A implementation <ref name=readmeTrustedFirmware>{{CodeSource | TF-A | readme.rst {{DocSource | domain=TF-A | path=index.html | text=Trusted Firmware-A documentation}}</ref>. Trusted Firmware-A also implements a secure monitor set of features with various Arm interface standards: * The power state coordination interface (PSCI) <ref name=psci>http://infocenter.arm.com/help/topic/com.arm.doc.den0022d/Power_State_Coordination_Interface_PDD_v1_1_DEN0022D.pdf</ref> * Trusted board boot requirements (TBBR) <ref>Arm DEN0006C-1[https://developer.arm.com/documentation/den0022/ ARM Power State Coordination Interface]</ref> * SMC calling convention <ref name=smc>http://infocenter.arm.com/help/topic/com.arm.doc.den0028b/ARM_DEN0028B_SMC_Calling_Convention.pdf [https://developer.arm.com/documentation/den0028/ SMC Calling Convention (SMCCC)]</ref> * System control and management interface <ref name=scmi>http://infocenter.arm.com/help/topic/com.arm.doc.den0056a/DEN0056A_System_Control_and_Management_Interface.pdf [https://developer.arm.com/documentation/den0056/ Arm System Control and Management Interface]</ref> Trusted Firmware-A is usually shortened to TF-A. == Architecture == The global architecture of TF-A is explained in the Trusted Firmware-A design <ref name=TrustedFirmware/>{{CodeSource | TF-A | docs/firmware-design.rst}}</ref> document. TF-A is divided into several binaries, each with a dedicated main role.<br> For 32-bit Arm processors (AArch32), it the trusted boot is divided into four stepsstages (in order of execution): * Boot loader stage 1 (BL1) application processor trusted ROM * Boot loader stage 2 (BL2) trusted boot firmware * Boot loader stage 3-2 (BL32) trusted runtime softwarefirmware * Boot loader stage 3-3 (BL33) non-trusted firmware BL1, BL2 and BL32 are parts of TF-A. BL1 is now optional, and can be removed by enabling the compilation flag: BL2_AT_EL3. It is then removed for the STM32MP1, as all BL1 tasks are done by Because STM32 MPU platforms uses a dedicated [[:Category:ROM code|ROM code]], the BL1 boot stage is then removed. [[:Category:ROM code|ROM code]], or expects the BL2. to run at EL3 execution level. This mode is selected when the BL2_AT_EL3 build flag is enabled. BL33 is outside of TF-A. This is the first non-secure code loaded by TF-A. During the boot sequence, this is the secondary stage boot loader (SSBL). For STM32 MPU platforms, the SSBL is [[U-Boot overview|U-Boot]] by default. TF-A can manage its configuration with a [[STM32MP15_STM32_MPU_device_tree#Device tree structure for Linux, U-Boot and TF-A|device tree]], as this is the case on STM32MP1. It . In the BL2 stage, it is a reduced version of the Linux kernel one, with only the required devices used during boot. It can be configured with [[STM32CubeMX]]. In STMicroelectronics' implementation, the 2 binaries, BL2 and BL32, and the device tree are put together in a single binary, to be loaded at once to the SYSRAM by the ROM code. [[File:Boot_ATF.png|center|link=]] [[File:Boot_ATF_legend.png|center|link=]] upright=2]] TF-A loading steps: # ROM code loads TF-A binary and calls BL2 # BL2 preparesloads BL32 # BL2 loads BL33 # BL2 calls BL32 # BL32 calls BL33 == Boot loader stages == === BL1 === BL1 is the first stage executed, and is designed to act as ROM code; it is loaded and executed in internal RAM. It is not used for the STM32MP1STM32 MPU. As the STM32MP1STM32 MPU has its own proprietary [[:Category:ROM code|ROM code]], this part can be removed and BL2 is then the first TF-A binary to be executed. === BL2 === BL2 (trusted boot firmware) is in charge of loading the next-stage images (secure and non secure). To achieve this role, BL2 has to initialize all the required peripherals. It has to initialize the security components.<br> For the STM32MP15, these security peripherals are: * boot and security, and OTP control ([[BSEC internal peripheral]]) * extended TrustZone protection controller ([[ETZPC internal peripheral]]) * TrustZone address space controller for DDR ([[TZC internal peripheral]]) BL2 is also in charge of initializing the DDR and clock tree. The boot peripheral has to be initialized.<br> On the STM32MP15, it can be one of the following: * SD-card via the [[SDMMC internal peripheral]] * eMMC via the [[SDMMC internal peripheral]] * NAND via the [[FMC internal peripheral]] * NOR via the [[QUADSPI internal peripheral]] USB ([[OTG internal peripheral]]) or UART([[USART internal peripheral]]) are used when Flashing, see [[STM32CubeProgrammer]] for more details. BL2 also integrates image verification and authentication. Authentication is achieved by calling [[STM32MP15 ROM code overview|BootROM]] verification services* System components: clocks, DDR, ... * Security components: cryptographic peripheral, memory firewall, ... * Storage [[TF-A_BL2_overview|BL2 offers different features]] to load and authenticate images. At the end of its execution, after having loaded BL32 and the next boot stage (BL33), BL2 jumps to BL32. === BL32 === BL32 provides runtime secure services.In TF-A, the BL32 default implementation is SP-MIN solution On Armv7 architecture, the BL32 must embed a Secure Monitor as it will be executed in the same privilege level (PL1-SVC Secure). TF-A provides a minimal monitor implementation: SP-MIN. It is described in the TF-A functionality list <ref name=readmeTrustedFirmware/> as: "A minimal AArch32 Secure Payload (SP-MIN) to demonstrate PSCI <ref name=psci/> library integration with AArch32 EL3 Runtime Software." This minimal implementation can be replaced with a trusted OS or trusted environment execution (TEE), such as [[OP-TEE overview|OP-TEE]]. Both solutions (SP-MIN or OP-TEE) are supported by STMicroelectronics for STM32MP1. that also embeds a secure monitor on Armv7. {{Info|STM32MP15 supports the SP-MIN but it is no more recommended. [[OP-TEE overview|OP-TEE]] is the BL32 official solution.}} BL32 acts as a secure monitor and thus provides secure services to non-secure OSs. These services are called by non-secure software with secure monitor calls <ref name=smc/>. This code is in charge of standard service calls, like PSCI <ref name=psci/> or SCMI <ref name=scmi/>.<br/> It also provides STMicroelectronics dedicatedproprietary services, to access secure peripherals. On the STM32MP1, these services are used to access [[RCC internal peripheral]], [[PWR internal peripheral]], [[RTC internal peripheral]] or [[BSEC internal peripheral]]some specific and limited secure peripherals (with secure access control). ==References==<references /> <noinclude> [[Category:Trusted Firmware-A (TF-ABL2)| 01]] [[Category:Trusted Firmware-A (SP-MIN)| 01]] {{PublicationRequestId | 19292 (Previous 9178 | 2018-10-24) | 2120-03-10 | PhilipS}}</noinclude>
(27 intermediate revisions by 5 users not shown) | |||
Line 1: | Line 1: | ||
+ | <noinclude>{{ApplicableFor |
||
+ | |MPUs list=STM32MP13x, STM32MP15x |
||
+ | |MPUs checklist=STM32MP13x,STM32MP15x |
||
+ | }}</noinclude> |
||
== Trusted Firmware-A == |
== Trusted Firmware-A == |
||
[[File: STM32MPU Embedded Software architecture overview.png|link=STM32MPU Embedded Software architecture overview|thumb|Zoom out to STM32MPU Embedded Software]] |
[[File: STM32MPU Embedded Software architecture overview.png|link=STM32MPU Embedded Software architecture overview|thumb|Zoom out to STM32MPU Embedded Software]] |
||
− | Trusted Firmware-A is a reference implementation of secure-world software provided by Arm<sup>®</sup>. It was first designed for Armv8-A platforms, and has been adapted to be used on Armv7-A platforms by STMicroelectronics. |
+ | Trusted Firmware-A is a reference implementation of secure-world software provided by Arm<sup>®</sup>. It was first designed for Armv8-A platforms, and has been adapted to be used on Armv7-A platforms by STMicroelectronics. Trusted Firmware-A is part of the Trusted Firmware project that is an open governance community project hosted by Linaro.<ref>https://www.trustedfirmware.org/</ref> |
It is used as the first-stage boot loader (FSBL) on STM32 MPU platforms when using the [[Boot_chain_overview#STM32MP boot sequence|trusted boot chain]]. |
It is used as the first-stage boot loader (FSBL) on STM32 MPU platforms when using the [[Boot_chain_overview#STM32MP boot sequence|trusted boot chain]]. |
||
− | The code is open source, under a BSD-3-Clause |
+ | The code is open source, under a BSD-3-Clause license, and can be found on Linaro project page
|
− | <ref>https:// |
+ | <ref>https://git.trustedfirmware.org/TF-A/trusted-firmware-a.git</ref>, including an up-to-date documentation about Trusted Firmware-A implementation <ref name=TrustedFirmware> {{DocSource | domain=TF-A | path=index.html | text=Trusted Firmware-A documentation}}</ref>. |
− | Trusted Firmware-A also implements a |
+ | Trusted Firmware-A also implements a set of features with various Arm interface standards: |
− | * The power state coordination interface (PSCI) <ref name=psci> |
+ | * The power state coordination interface (PSCI) <ref name=psci>[https://developer.arm.com/documentation/den0022/ ARM Power State Coordination Interface]</ref> |
− | + | * SMC calling convention <ref name=smc>[https://developer.arm.com/documentation/den0028/ SMC Calling Convention (SMCCC)]</ref> |
|
− | * SMC calling convention <ref name=smc> |
+ | * System control and management interface <ref name=scmi>[https://developer.arm.com/documentation/den0056/ Arm System Control and Management Interface]</ref> |
− | * System control and management interface <ref> |
||
Trusted Firmware-A is usually shortened to TF-A. |
Trusted Firmware-A is usually shortened to TF-A. |
||
Line 18: | Line 21: | ||
== Architecture == |
== Architecture == |
||
− | The global architecture of TF-A is explained in the Trusted Firmware-A design <ref |
+ | The global architecture of TF-A is explained in the Trusted Firmware-A design <ref name=TrustedFirmware/> document. |
− | TF-A is divided into several binaries, each with a dedicated main role. For 32-bit Arm processors (AArch32), |
+ | TF-A is divided into several binaries, each with a dedicated main role.<br>
|
+ | For 32-bit Arm processors (AArch32), the trusted boot is divided into four stages (in order of execution): |
||
* Boot loader stage 1 (BL1) application processor trusted ROM |
* Boot loader stage 1 (BL1) application processor trusted ROM |
||
* Boot loader stage 2 (BL2) trusted boot firmware |
* Boot loader stage 2 (BL2) trusted boot firmware |
||
− | * Boot loader stage 3-2 (BL32) runtime |
+ | * Boot loader stage 3-2 (BL32) trusted runtime firmware
|
* Boot loader stage 3-3 (BL33) non-trusted firmware |
* Boot loader stage 3-3 (BL33) non-trusted firmware |
||
BL1, BL2 and BL32 are parts of TF-A. |
BL1, BL2 and BL32 are parts of TF-A. |
||
− | + |
Because STM32 MPU platforms uses a dedicated [[:Category:ROM code|ROM code]], the BL1 boot stage is then removed. [[:Category:ROM code|ROM code]] expects the BL2 to run at EL3 execution level. This mode is selected when the BL2_AT_EL3 build flag is enabled. |
|
BL33 is outside of TF-A. This is the first non-secure code loaded by TF-A. During the boot sequence, this is the secondary stage boot loader (SSBL). For STM32 MPU platforms, the SSBL is [[U-Boot overview|U-Boot]] by default. |
BL33 is outside of TF-A. This is the first non-secure code loaded by TF-A. During the boot sequence, this is the secondary stage boot loader (SSBL). For STM32 MPU platforms, the SSBL is [[U-Boot overview|U-Boot]] by default. |
||
− | TF-A can manage its configuration with a [[ |
+ | TF-A can manage its configuration with a [[STM32_MPU_device_tree#Device tree structure for Linux, U-Boot and TF-A|device tree]]. In the BL2 stage, it is a reduced version of the Linux kernel one, with only the required devices used during boot. It can be configured with [[STM32CubeMX]]. |
− | + | [[File:Boot_ATF.png|center|upright=2]] |
|
− | |||
− | [[File:Boot_ATF.png|center| |
||
− | |||
− | |||
TF-A loading steps: |
TF-A loading steps: |
||
− | # ROM code loads |
+ | # ROM code loads and calls BL2 |
− | # BL2 |
+ | # BL2 loads BL32 |
# BL2 loads BL33 |
# BL2 loads BL33 |
||
# BL2 calls BL32 |
# BL2 calls BL32 |
||
Line 51: | Line 51: | ||
=== BL1 === |
=== BL1 === |
||
BL1 is the first stage executed, and is designed to act as ROM code; it is loaded and executed in internal RAM. |
BL1 is the first stage executed, and is designed to act as ROM code; it is loaded and executed in internal RAM. |
||
− | It is not used for the |
+ | It is not used for the STM32 MPU. As the STM32 MPU has its own proprietary [[:Category:ROM code|ROM code]], this part can be removed and BL2 is then the first TF-A binary to be executed. |
=== BL2 === |
=== BL2 === |
||
− | BL2 |
+ | BL2 is in charge of loading the next-stage images (secure and non secure). |
To achieve this role, BL2 has to initialize all the required peripherals. |
To achieve this role, BL2 has to initialize all the required peripherals. |
||
+ | * System components: clocks, DDR, ... |
||
+ | * Security components: cryptographic peripheral, memory firewall, ... |
||
+ | * Storage |
||
− | + | [[TF-A_BL2_overview|BL2 offers different features]] to load and authenticate images. |
|
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
At the end of its execution, after having loaded BL32 and the next boot stage (BL33), BL2 jumps to BL32. |
At the end of its execution, after having loaded BL32 and the next boot stage (BL33), BL2 jumps to BL32. |
||
=== BL32 === |
=== BL32 === |
||
− | BL32 provides runtime secure services. |
+ | BL32 provides runtime secure services. |
− | It is described in the TF-A functionality list <ref name= |
+ | |
+ | On Armv7 architecture, the BL32 must embed a Secure Monitor as it will be executed in the same privilege level (PL1-SVC Secure). |
||
+ | TF-A provides a minimal monitor implementation: SP-MIN. |
||
+ | It is described in the TF-A functionality list <ref name=TrustedFirmware/> as: |
||
"A minimal AArch32 Secure Payload (SP-MIN) to demonstrate PSCI <ref name=psci/> library integration with AArch32 EL3 Runtime Software." |
"A minimal AArch32 Secure Payload (SP-MIN) to demonstrate PSCI <ref name=psci/> library integration with AArch32 EL3 Runtime Software." |
||
− | This minimal implementation can be replaced with a trusted OS or trusted environment execution (TEE), such as [[OP-TEE overview|OP-TEE]]. |
+ | This minimal implementation can be replaced with a trusted OS or trusted environment execution (TEE), such as [[OP-TEE overview|OP-TEE]] that also embeds a secure monitor on Armv7. |
− | + |
{{Info|STM32MP15 supports the SP-MIN but it is no more recommended. [[OP-TEE overview|OP-TEE]] is the BL32 official solution.}}
|
|
BL32 acts as a secure monitor and thus provides secure services to non-secure OSs. These services are called by non-secure software with secure monitor calls <ref name=smc/>. |
BL32 acts as a secure monitor and thus provides secure services to non-secure OSs. These services are called by non-secure software with secure monitor calls <ref name=smc/>. |
||
− | This code is in charge of standard service calls, like PSCI <ref name=psci/>.<br/> |
+ | This code is in charge of standard service calls, like PSCI <ref name=psci/> or SCMI <ref name=scmi/>.<br/> |
− | It also provides STMicroelectronics |
+ | It also provides STMicroelectronics proprietary services to access some specific and limited secure peripherals (with secure access control). |
==References== |
==References== |
||
Line 96: | Line 85: | ||
<noinclude> |
<noinclude> |
||
− | [[Category:Trusted Firmware-A ( |
+ | [[Category:Trusted Firmware-A (BL2)| 01]] |
[[Category:Trusted Firmware-A (SP-MIN)| 01]] |
[[Category:Trusted Firmware-A (SP-MIN)| 01]] |
||
− | {{PublicationRequestId | 9178 | |
+ | {{PublicationRequestId | 19292 (Previous 9178) | 2120-03-10 | PhilipS}} |
</noinclude> |
</noinclude> |