Difference between revisions of "TF-A BL2 overview"

[unchecked revision] [quality revision]
m
m
 

1 Article purpose[edit]

This section details the TF-A BL2 stage (Trusted Firmware-A Boot Loader stage 2) used as FSBL (First Stage Boot Loader). TF-A BL2 is the FSBL for ST boot chain. It is loaded by the ROM code in internal SYSRAM.
The main goal of this stage is to configure the DDR to load (and authenticate) other components from a FIP binary.

2 Device tree[edit]

TF-A BL2 is based on device tree configuration. It uses the same device tree as the kernel but keeping only the mandatory nodes for the boot stage (to reduce binary size) thanks to a dedicated device tree file (such as fdts/stm32mp15-bl2.dtsi ). The device tree is part of the final STM32 file in order to be authenticated by the ROM code and loaded at the same time in the SYSRAM.
It must be configured or updated depending on your platform.

3 STM32 binary file[edit]

To be properly loaded into SYSRAM by the ROM code, the TF-A BL2 firmware needs to be encapsulated in a binary that starts with a STM32 header.
The STM32 header information is mandatory for the ROM code to be able to load, authenticate and start the firmware.
As the ROM code can only load a single binary, the STM32 file must embed in a single image, the header, the device tree and the BL2 binary firmware.

TF-A BL2 is part of the trusted boot and can be signed to be authenticated by ROM code. See Secure boot process for more details.

4 Binary mapping[edit]

Below the TF-A BL2 mapping including the STM32 header layout:

Atf.stm32.png

The different sizes can be customized depending on build options and device tree customization. All sizes can be changed in the platform definition file. STM32MP1 platform uses plat/st/stm32mp1/stm32mp1_def.h :

  • STM32MP_BL2_DTB_BASE: device tree base address in SYSRAM with its associated SIZE
  • STM32MP_BL2_BASE: start address from which the code is loaded and executed
  • STM32MP_BL2_SIZE, which cannot exceed SYSRAM size.

5 Boot device[edit]

5.1 External memory[edit]

TF-A BL2 needs to access storage devices to load the other software components. By default, it uses the boot device selected by boot pins or OTP.
The selected device needs to be properly set up:

  • Device tree configuration (all devices)
  • BL2 boot device configuration for Flash memories .

Each device support needs a specific framework in the BL2 firmware.
By default, STMicroelectronics chose to select one single device support per binary. A BL2 with full storage support cannot fit in the SYSRAM size.
Storage build flags allow the BL2 firmware to be configured to support the requested boot storage.

5.2 Serial mode (USB/UART)[edit]

The Programmer mode (USB or UART boot device) requires the complete FIP binary to start the load image process as previously explained. This is achieved by loading the complete FIP binary into DDR before starting the normal boot sequence. The FIP load address configurable with DWL_BUFFER_BASE parameter. The default value is in plat/st/stm32mp1/platform.mk

6 DDR[edit]

TF-A BL2 needs to set up the DDR to load the next binaries. DDR settings come from the device tree and must be adapted by the customer depending on DDR type, DDR configuration and boards. This can be done using STM32CubeMX.

6.1 DDR encryption[edit]

On STM32MP13x lines Warning.png, a region of the DDR can be encrypted, thanks to DDRMCE. Its configuration is done in TF-A Firmware configuration device tree, with the DDRMCE configuration.

7 Clock management[edit]

An initial clock tree must be set up to allow accessing the DDR and the external storage devices.
It also improves the performance by increasing the default CPU speed and the storage transfer speed.

8 FIP[edit]

The Firmware Image Package (FIP)[1] is a TF-A archive binary that encapsulates bootloader images into a single archive. It can also contain other data such as certificates that are required to complete the boot process.

See the page How to configure TF-A FIP for more information.

9 FCONF[edit]

The Firmware Configuration Framework (FCONF)[2] is a way to offer more flexibility in the firmware.

It is used to provide most of the platform-specific data that were previously hard coded inside the firmware. This framework uses device tree (one or multiple) that are passed to the firmware during load processing. BL2 uses it for several purposes:

  • list images to be loaded, with their load addresses and max sizes
  • DDR firewall configuration
  • describe the chain of trust parameters

TF-A BL2 configuration is done with a dedicated device tree file named FW_CONFIG. More details about the FW_CONFIG file are given by the page How to configure TF-A FW CONFIG.

10 Authentication[edit]

TF-A BL2 manages authentication thanks to Trusted Board Boot activation.


== Article purpose ==
This section details the TF-A BL2 stage (Trusted Firmware-A Boot Loader stage 2) used as FSBL (First Stage Boot Loader).
TF-A BL2 is the FSBL for ST boot chain. It is loaded by the [[STM32_MPU_ROM_code_overview|ROM code]] in internal [[SYSRAM_internal_memory|SYSRAM]].<br>

The main goal of this stage is to configure the DDR to load (and authenticate) other components from a [[How to configure TF-A FIP|FIP binary]].<br>


== Device tree ==
TF-A BL2 is based on device tree configuration. It uses the same device tree as the kernel but keeping only the mandatory nodes for the boot stage (to reduce binary size) thanks to a dedicated device tree file (such as {{CodeSource | TF-A | fdts/stm32mp15-bl2.dtsi}}).
The device tree is part of the final STM32 file in order to be authenticated by the [[STM32_MPU_ROM_code_overview|ROM code]] and loaded at the same time in the [[SYSRAM_internal_memory|SYSRAM]].<br>

It must be configured or updated depending on your platform.<br>


== STM32 binary file ==
To be properly loaded into [[SYSRAM_internal_memory|SYSRAM]] by the [[STM32_MPU_ROM_code_overview|ROM code]], the TF-A BL2 firmware needs to be encapsulated in a binary that starts with a [[STM32_header_for_binary_files|STM32 header]].<br>

The [[STM32_header_for_binary_files|STM32 header]] information is mandatory for the [[STM32_MPU_ROM_code_overview|ROM code]] to be able to load, authenticate and start the firmware.<br>

As the ROM code can only load a single binary, the STM32 file must embed in a single image, the header, the device tree and the BL2 binary firmware. <br>


TF-A BL2 is part of the trusted boot and can be signed to be authenticated by [[STM32_MPU_ROM_code_overview|ROM code]]. See [[Security_overview#Secure_boot|Secure boot]] process for more details.

== Binary mapping ==
Below the TF-A BL2 mapping including the STM32 header layout:
[[File:Atf.stm32.png|600px|center|link=]]

The different sizes can be customized depending on build options and device tree customization. All sizes can be changed in the platform definition file. STM32MP1 platform uses {{ CodeSource | TF-A | plat/st/stm32mp1/stm32mp1_def.h }}:
* STM32MP_BL2_DTB_BASE: device tree base address in SYSRAM with its associated SIZE
* STM32MP_BL2_BASE: start address from which the code is loaded and executed
* STM32MP_BL2_SIZE, which cannot exceed [[SYSRAM_internal_memory|SYSRAM]] size.

== Boot device ==
=== External memory ===
TF-A BL2 needs to access storage devices to load the other software components. By default, it uses the boot device selected by [[STM32_MPU_ROM_code_overview#Boot_device_selection_via_the_boot_pins_and_OTP|boot pins or OTP]].<br>

The selected device needs to be properly set up:
* Device tree configuration (all devices)
* BL2 boot device configuration for [[How to configure flash memory for TF-A BL2| Flash memories ]].

Each device support needs a specific framework in the BL2 firmware.<br>

By default, STMicroelectronics chose to select one single device support per binary. A BL2 with full storage support cannot fit in the [[SYSRAM_internal_memory|SYSRAM]] size.<br>

Storage [[How_to_configure_TF-A_BL2#TF-A_Build_flags|build flags]] allow the BL2 firmware to be configured to support the requested boot storage.

=== Serial mode (USB/UART) ===
The Programmer mode (USB or UART boot device) requires the complete [[How to configure TF-A FIP|FIP binary]] to start the load image process as previously explained.
This is achieved by loading the complete [[How to configure TF-A FIP|FIP binary]] into DDR before starting the normal boot sequence.
The FIP load address configurable with DWL_BUFFER_BASE parameter. The default value is in {{CodeSource | TF-A | plat/st/stm32mp1/platform.mk}}

== DDR ==
TF-A BL2 needs to set up the DDR to load the next binaries.
DDR settings come from the device tree and must be adapted by the customer depending on DDR type, DDR configuration and boards.
This can be done using [[DDRCTRL_and_DDRPHYC_device_tree_configuration#How_to_configure_the_DT_using_STM32CubeMX|STM32CubeMX]].

=== DDR encryption ===
On {{MicroprocessorDevice | device=13}}, a region of the DDR can be encrypted, thanks to [[DDRMCE_internal_peripheral|DDRMCE]]. Its configuration is done in TF-A [[TF-A_overview#Firmware_Configuration|Firmware configuration]] device tree, with the [[How_to_configure_TF-A_FW_CONFIG#DDR_Encryption_area|DDRMCE configuration]].

== Clock management ==
An initial [[Clock_device_tree_configuration_-_Bootloader_specific|clock tree]] must be set up to allow accessing the DDR and the external storage devices.<br>

It also improves the performance by increasing the default CPU speed and the storage transfer speed.

== FIP ==
The Firmware Image Package (FIP)<ref name=fip>{{DocSource | domain=TF-A | path=design/firmware-design.html#firmware-image-package-fip | text=Firmware Image Package}}</ref> is a TF-A archive binary that encapsulates bootloader images into a single archive.</br> 

It can also contain other data such as certificates that are required to complete the boot process.

See the page [[How to configure TF-A FIP]] for more information.

== FCONF ==
The Firmware Configuration Framework (FCONF)<ref name=fconf>{{DocSource | domain=TF-A | path=components/fconf/index.html | text=Firmware Configuration Framework}}</ref> is a way to offer more flexibility in the firmware.

It is used to provide most of the platform-specific data that were previously hard coded inside the firmware.
This framework uses device tree (one or multiple) that are passed to the firmware during load processing.
BL2 uses it for several purposes:
* list images to be loaded, with their load addresses and max sizes
* DDR firewall configuration
* describe the chain of trust parameters

TF-A BL2 configuration is done with a dedicated device tree file named FW_CONFIG.
More details about the FW_CONFIG file are given by the page [[How to configure TF-A FW CONFIG]].

== Authentication ==
TF-A BL2 manages authentication thanks to [[TF-A_BL2_Trusted_Board_Boot|Trusted Board Boot]] activation.
<noinclude>

{{PublicationRequestId | 19288| 2021-03-10 | reviewed by AnneJ in the article STM32 MPU TF-A (BL2) which has been split in 2 articles How_to_configure_TF-A_BL2 and this one}}
[[Category:Trusted Firmware-A (BL2)| 02]]</noinclude>
Line 50: Line 50:
   
 
== Clock management ==
 
== Clock management ==
An initial [[Clock_device_tree_configuration_-_Bootloader_specific|clock tree]] must be set up to allow accessing the DDR and the external storage devices.<br>
+
An initial [[Clock_device_tree_configuration|clock tree]] must be set up to allow accessing the DDR and the external storage devices.<br>
 
It also improves the performance by increasing the default CPU speed and the storage transfer speed.
 
It also improves the performance by increasing the default CPU speed and the storage transfer speed.