Difference between revisions of "Subpart - STM32MP1 - Starter Package"

[unchecked revision] [quality revision]
m
m
Applicable for STM32MP15x lines, STM32MP13x lines

1 Article purpose[edit]

This article gathers the information that applies to any STM32MP1 board.

Warning white.png Warning
To start efficiently the board, it's recommended to go through the Starter Package article relative to your board: Category:Starter Package

That's the reason why the steps 2, 3 and 6 referenced in this article depend on the considered board:


2 Checking the boot sequence[edit]

Assuming you have performed the optional step 6 above, the information (coming successively from the TF-A, OP-TEE OS, U-Boot and the Linux operating system that is booting on the board), should be displayed on the host PC Terminal.

Info white.png Information
The information displayed below might differ from that on your own application, and should just be considered as an example.
First information scrolled on the remote Terminal during boot
Last information scrolled on the remote Terminal during boot

In parallel, a U-Boot splash screen picture is displayed on the DSI display (if one is connected to the board).DSI U-Boot splash screen.png

A user space graphical boot splash screen (PSplash) picture is then briefly displayed on the HDMI monitor if one is connected to the board, or otherwise on the DSI display (if one is connected to the board).DSI user splash screen.png

When the boot process is complete, the launcher application is shown on the HDMI monitor if one is connected to the board, or otherwise on the DSI display (if one is connected to the board).

More detail about this launcher application in GTK demo launcher page.

3 Mouse, keyboard and Ethernet hot-plugs[edit]

Let's assume that the optional step 2 and step 3 were not achieved when setting up the system above.

When connecting a USB mouse, the following information is displayed by the Terminal program:

[  926.786326] usb 2-1.1: new low-speed USB device number 3 using ehci-platform
[  926.961413] input: Logitech Optical USB Mouse as /devices/platform/soc/5800d000.usbh-ehci/usb2/2-1/2-1.1/2-1.1:1.0/0003:046D:C016.0001/input/input2
[  926.975098] hid-generic 0003:046D:C016.0001: input: USB HID v1.10 Mouse [Logitech Optical USB Mouse] on usb-5800d000.usbh-ehci-1.1/input0


When connecting a USB keyboard, the following information is displayed by the Terminal program:

[ 1009.026567] usb 2-1.3: new low-speed USB device number 4 using ehci-platform
[ 1009.193990] input: Dell Dell USB Keyboard as /devices/platform/soc/5800d000.usbh-ehci/usb2/2-1/2-1.3/2-1.3:1.0/0003:413C:2003.0002/input/input3
[ 1009.280101] hid-generic 0003:413C:2003.0002: input: USB HID v1.10 Keyboard [Dell Dell USB Keyboard] on usb-5800d000.usbh-ehci-1.3/input0


When connecting an Ethernet cable, the following information is displayed by the Terminal program:

[ 1215.356377] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 1215.363377] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 1215.391068] Link is Up - 1000/Half

or on STM32MP13x lines Warning.png for the second Ethernet interface

[  117.370989] stm32-dwmac 5800e000.eth2 eth1: Link is Up - 100Mbps/Full - flow control rx/tx
[  117.377950] IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready

4 Remote and local Terminal programs[edit]

As already explained in the step 6 above, a remote Terminal program can be installed and configured on your host PC in order to communicate with the board through a serial link or an Ethernet link: see How to get Terminal.

The remote Terminal on your host PC can be used to enter command lines, as shown below with the ifconfig command to query the network interface parameters:

Example of command (ifconfig) executed on the remote Terminal program


A local Terminal program can be launched directly on the board. Click on the small icon at the top left corner of the display (see the red arrow on the figure below):

Icon to launch a local Terminal program
Wayland Terminal program


Then the on-board Wayland Terminal can be used to directly enter command lines as shown below, still with the ip addr command to query the network interface parameters:

Example of command (ip addr) executed on the Wayland Terminal program


Consequently, unless an explicit restriction is mentioned, command lines can be run from both Terminals.

Note: in this article, any command executed on the board (through the remote Terminal or the Wayland Terminal) starts with , while any command executed on the host PC starts with .

5 Executing basic commands[edit]

Info white.png Information
The outputs of the commands executed below are examples; the outputs obtained might differ.

5.1 Having a look at the OpenSTLinux directory structure[edit]

The directory structure and directory contents in the OpenSTLinux distribution is standard. Some details are available in the OpenSTLinux directory structure article.

5.2 Identifying the software running on board[edit]

Info white.png Information
Obviously, what you obtain might differ from what is displayed on the Output example column.

5.2.1 For ecosystem release v4.0.0 More info.png[edit]

Software How to get its version Output example
TF-A TF-A Version number

NOTICE: BL2: v2.6-stm32mp1-r1.0(debug):v2.6-dirty

U-Boot See the version displayed in the console

2021.10-stm32mp-r1 [...]

Linux kernel
 cat /proc/version

Linux version 5.15.24 (xxxx@yyyy) (arm-ostl-linux-gnueabi-gcc (GCC) 11.2.0 ) [...]

GCC
 cat /proc/version

Linux version 5.15.24 (xxxx@yyyy) (arm-ostl-linux-gnueabi-gcc (GCC) 11.2.0) [...]

Yocto Project
 grep DISTRO_CODENAME /etc/build

DISTRO_CODENAME = kirkstone

Weston
 weston --version

weston 10.0.0

GStreamer
 gst-play-1.0 --version

GStreamer 1.20.1

GPU (only on STM32MP15x lines More info.png)
 cat /sys/kernel/debug/gc/version

6.4.7.365873 built [...]

5.3 Configuration tips[edit]

5.4 Getting board IP address[edit]

Prerequisite: your board is connected to your local network through the Ethernet connector (see step 3).

 ip addr show eth0                                                                           
3: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000
    link/ether xx:xx:xx:xx:xx:xx brd ff:ff:ff:ff:ff:ff
    inet xx.xx.xx.xx/xx brd xx.xx.xx.xx scope global dynamic eth0
       valid_lft 159045sec preferred_lft 159045sec
    inet6 xxxx::xx:xx:xx:xx/xx scope link 
       valid_lft forever preferred_lft forever
  • Get the IP address of your board with the ifconfig Linux command line (a deprecated but well-known command):
 ifconfig eth0
eth0      Link encap:Ethernet  HWaddr xx:xx:xx:xx:xx:xx
          inet addr:xx.xx.xx.xx  Bcast:xx.xx.xx.xx  Mask:255.255.252.0
          inet6 addr: xxxx::xx:xx:xx:xx/xx Scope:Link
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:2619 errors:0 dropped:0 overruns:0 frame:0
          TX packets:1311 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:353250 (344.9 KiB)  TX bytes:118305 (115.5 KiB)
          Interrupt:247

5.5 Copying a file from your host PC to your board (and reciprocally)[edit]

5.6 Miscellaneous commands[edit]

Info white.png Information
The outputs of the commands executed below are examples; the outputs that you obtain might differ.

5.6.1 Printing distribution specific information[edit]

 cat /etc/os-release 
ID=openstlinux-weston
NAME="ST OpenSTLinux - Weston - (A Yocto Project Based Distro)"
VERSION="4.0.1-openstlinux-22-06-15 (kirkstone)"
VERSION_ID=4.0.1-openstlinux-22-06-15 
PRETTY_NAME="ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 4.0.1-openstlinux-22-06-15 (kirkstone)"
DISTRO_CODENAME="kirkstone"

Where:

ID A lower-case string identifying the operating system
NAME A string identifying the operating system
VERSION A string identifying the operating system version, including a release code name
VERSION_ID A lower case string identifying the operating system version
PRETTY_NAME A full pretty name of the release

5.6.2 Printing system information[edit]

 uname -a
Linux stm32mp1 5.15.24 #1 SMP PREEMPT Wed Feb 16 11:56:41 UTC 2022 armv7l armv7l armv7l GNU/Linux

Where:

Linux Kernel name
stm32mp1 Network node hostname
5.15.24 Kernel release
#1 SMP PREEMPT Wed Feb 16 11:56:41 UTC 2022 Kernel version
armv7l Machine hardware name
GNU/Linux Operating system

5.6.3 Printing Linux kernel and GCC versions[edit]

 cat /proc/version
Linux version 5.15.24 (oe-user@oe-host) (arm-ostl-linux-gnueabi-gcc (GCC) 11.2.0, GNU ld (GNU Binutils) 2.38.20220313) #1 SMP PREEMPT Wed Feb 16 11:56:41 UTC 2022

Where:

Linux Kernel name
version 5.15.24 Kernel release
(xxxx@yyyy) Person (xxxx) who compiled the kernel, and machine (yyyy) where it happened
(arm-ostl-linux-gnueabi-gcc (GCC) 11.2.0 ) Version of the GCC compiler used to compile the kernel
#1 SMP PREEMPT Wed Feb 16 11:56:41 UTC 2022 Kernel version; type of kernel (SMP) and date and time of the kernel compilation

5.6.4 Printing the amount of disk space available on all mounted file systems[edit]

 df -h
Filesystem      Size  Used Avail Use% Mounted on
devtmpfs         116M     0  116M   0% /dev
/dev/mmcblk0p10  684M  453M  184M  72% /
tmpfs            195M  176K  195M   1% /dev/shm
tmpfs             78M  8.8M   70M  12% /run
tmpfs            4.0M     0  4.0M   0% /sys/fs/cgroup
tmpfs            195M   16K  195M   1% /tmp
/dev/mmcblk0p8    55M   39M   12M  77% /boot
/dev/mmcblk0p9    14M  5.9M  6.8M  47% /vendor
tmpfs            195M   96K  195M   1% /var/volatile
/dev/mmcblk0p11   14G   45M   13G   1% /usr/local
tmpfs             39M  4.0K   39M   1% /run/user/1000
tmpfs             39M     0   39M   0% /run/user/0

Where:

Filesystem Source of the mount point, usually a device
Size Total size in human readable format (e.g. 1K, 234M, 2G)
Used Used size in human readable format
Available Available size in human readable format
Use% Percentage of used size divided by the total size
Mounted on Mount point


Note: the user file system (userfs) and the boot file system (bootfs) are accessible respectively through the /usr/local mounting point, and the /boot mounting point (see Flash partitions for a description of the file systems).


<noinclude>

{{ApplicableFor
|MPUs list=STM32MP15x,STM32MP13x
|MPUs checklist=STM32MP15x,STM32MP13x
}}</noinclude>
<noinclude>

==Article purpose==
This article gathers the information that applies to any STM32MP1 board.

{{Warning|To start efficiently the board, it's recommended to go through the Starter Package article relative to your board: [[:Category:Starter Package]]}}

That's the reason why the steps 2, 3 and 6 referenced in this article depend on the considered board:{{UpdateNeededForNewBoard|Point to the steps of the new board Starter Package}}
<div class="mw-collapsible mw-collapsed">

* For {{MicroprocessorDevice | device=13}}<div class="mw-collapsible-content">

* <span id{{=}}"step2">'''Step 2'''</span> is either [[STM32MP13 Discovery kits - Starter Package#step2]]
* <span id{{=}}"step3">'''Step 3'''</span> is either [[STM32MP13 Discovery kits - Starter Package#step3]]
* <span id{{=}}"step6">'''Step 6'''</span> is either [[STM32MP13 Discovery kits - Starter Package#step6]]</div></div>
<div class="mw-collapsible mw-collapsed">

* For {{MicroprocessorDevice | device=15}}<div class="mw-collapsible-content">

* <span id{{=}}"step2">'''Step 2'''</span> is either [[STM32MP15 Evaluation boards - Starter Package#step2]] or [[STM32MP15 Discovery kits - Starter Package#step2]]
* <span id{{=}}"step3">'''Step 3'''</span> is either [[STM32MP15 Evaluation boards - Starter Package#step3]] or [[STM32MP15 Discovery kits - Starter Package#step3]]
* <span id{{=}}"step6">'''Step 6'''</span> is either [[STM32MP15 Evaluation boards - Starter Package#step6]] or [[STM32MP15 Discovery kits - Starter Package#step6]]</div></div>
</noinclude>


==Checking the boot sequence==
Assuming you have performed the optional [[#step6|step 6]] above, the information (coming successively from the TF-A, OP-TEE OS, U-Boot and the Linux operating system that is booting on the board), should be displayed on the host PC Terminal.
{{Info|The information displayed below might differ from that on your own application, and should just be considered as an example.}}

[[File: STM32MP15_boot_information_1.png|thumb|upright=4|center|link=|First information scrolled on the remote Terminal during boot]]
[[File: STM32MP15_boot_information_2.png|thumb|upright=4|center|link=|Last information scrolled on the remote Terminal during boot]]

In parallel, a U-Boot splash screen picture is displayed on the DSI display (if one is connected to the board).[[File:DSI_U-Boot_splash_screen.png|link=]]

A user space graphical boot splash screen (PSplash) picture is then briefly displayed on the HDMI monitor if one is connected to the board, or otherwise on the DSI display (if one is connected to the board).[[File:DSI_user_splash_screen.png|link=]]

When the boot process is complete, the launcher application is shown on the HDMI monitor if one is connected to the board, or otherwise on the DSI display (if one is connected to the board).

More detail about this launcher application in [[GTK demo launcher]] page.

==Mouse, keyboard and Ethernet hot-plugs==
Let's assume that the optional [[#step2|step 2]] and [[#step3|step 3]] were not achieved when setting up the system above.

When connecting a USB mouse, the following information is displayed by the Terminal program:
 [  926.786326] usb 2-1.1: new low-speed USB device number 3 using ehci-platform
 [  926.961413] input: Logitech Optical USB Mouse as /devices/platform/soc/5800d000.usbh-ehci/usb2/2-1/2-1.1/2-1.1:1.0/0003:046D:C016.0001/input/input2
 [  926.975098] hid-generic 0003:046D:C016.0001: input: USB HID v1.10 Mouse [Logitech Optical USB Mouse] on usb-5800d000.usbh-ehci-1.1/input0
<br>

When connecting a USB keyboard, the following information is displayed by the Terminal program:
 [ 1009.026567] usb 2-1.3: new low-speed USB device number 4 using ehci-platform
 [ 1009.193990] input: Dell Dell USB Keyboard as /devices/platform/soc/5800d000.usbh-ehci/usb2/2-1/2-1.3/2-1.3:1.0/0003:413C:2003.0002/input/input3
 [ 1009.280101] hid-generic 0003:413C:2003.0002: input: USB HID v1.10 Keyboard [Dell Dell USB Keyboard] on usb-5800d000.usbh-ehci-1.3/input0
<br>

When connecting an Ethernet cable, the following information is displayed by the Terminal program:
 [ 1215.356377] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
 [ 1215.363377] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
 [ 1215.391068] Link is Up - 1000/Half

or on {{MicroprocessorDevice | device=13}} for the second Ethernet interface
 [  117.370989] stm32-dwmac 5800e000.eth2 eth1: Link is Up - 100Mbps/Full - flow control rx/tx
 [  117.377950] IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready

==Remote and local Terminal programs==
As already explained in the [[#step6|step 6]] above, a '''remote Terminal''' program can be installed and configured on your host PC in order to communicate with the board through a serial link or an Ethernet link: see [[How to get Terminal]].

The remote Terminal on your host PC can be used to enter command lines, as shown below with the ''ifconfig'' command to query the network interface parameters:

[[File: STM32MP15_example_command_remote_terminal.png|thumb|upright=4|center|link=|Example of command (''ifconfig'') executed on the remote Terminal program]]<br>


A '''local Terminal''' program can be launched directly on the board. Click on the small icon at the top left corner of the display (see the red arrow on the figure below):

[[File: STM32MP15_local_terminal_icon.png|thumb|upright=4|center|link=|Icon to launch a local Terminal program]]
[[File: STM32MP15_wayland_terminal.png|thumb|upright=4|center|link=|Wayland Terminal program]]<br>


Then the on-board Wayland Terminal can be used to directly enter command lines as shown below, still with the ''ip addr'' command to query the network interface parameters:

[[File: STM32MP15_example_command_local_terminal.png|thumb|upright=4|center|link=|Example of command (''ip addr'') executed on the Wayland Terminal program]]<br>


Consequently, unless an explicit restriction is mentioned, command lines can be run from both Terminals. 

Note: in this article, any command executed on the board (through the remote Terminal or the Wayland Terminal) starts with {{Board$}}, while any command executed on the host PC starts with {{PC$}}.

==Executing basic commands==
{{Info|The outputs of the commands executed below are examples; the outputs obtained might differ.}}

===Having a look at the OpenSTLinux directory structure===
The directory structure and directory contents in the OpenSTLinux distribution is standard. Some details are available in the [[OpenSTLinux directory structure]] article.

===Identifying the software running on board===

{{Info|Obviously, what you obtain might differ from what is displayed on the ''Output example'' column.}} {{UpdateNeededForNewRelease|The "Output example" column below shall be updated periodically, even if the information banner specifies that this column might not be up-to-date}}

====For {{EcosystemRelease | revision=4.0.0 }}====
{| class="st-table"
! style="text-align:center;" |Software !! style="text-align:center;" |How to get its version !! style="text-align:center;" |Output example
|-
| TF-A || [[How to debug TF-A BL2#TF-A Version number|TF-A Version number]] ||
NOTICE:  BL2: v2.6-stm32mp1-r1.0(debug):{{Highlight|v2.6-dirty}}
|-
| U-Boot || See the version displayed in the console ||
{{Highlight|2021.10-stm32mp-r1}} [...]
|-
| Linux kernel ||
 {{Board$}} cat /proc/version
||
{{Highlight|Linux version 5.15.24}} (xxxx@yyyy) (arm-ostl-linux-gnueabi-gcc (GCC) 11.2.0 ) [...]
|-
| GCC ||
 {{Board$}} cat /proc/version
||
Linux version 5.15.24 (xxxx@yyyy) ({{Highlight|arm-ostl-linux-gnueabi-gcc (GCC) 11.2.0}}) [...]
|-
| Yocto Project ||
 {{Board$}} grep DISTRO_CODENAME /etc/build
||
DISTRO_CODENAME = {{Highlight|kirkstone}}
|-
| Weston ||
 {{Board$}} weston --version
||
{{Highlight|weston 10.0.0}}
|-
| GStreamer ||
 {{Board$}} gst-play-1.0 --version
||
{{Highlight|GStreamer 1.20.1}}
|-
| GPU (only on {{MicroprocessorDevice | device=15}}) ||
 {{Board$}} cat /sys/kernel/debug/gc/version
||
{{Highlight|6.4.7.365873}} built [...]
|}

===Configuration tips===
* [[Wayland Weston overview#Configuration|Configure the keyboard layout (qwerty, azerty...)]]

===Getting board IP address===
Prerequisite: your board is connected to your local network through the Ethernet connector (see [[#step3|step 3]]).

* Get the IP address of your board with the [[IP Linux command line|''ip'' Linux command line]] ({{highlight|recommended method}}):
 {{Board$}} ip addr show eth0                                                                           
 3: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000
     link/ether xx:xx:xx:xx:xx:xx brd ff:ff:ff:ff:ff:ff
     inet {{highlight|xx.xx.xx.xx}}/xx brd xx.xx.xx.xx scope global dynamic eth0
        valid_lft 159045sec preferred_lft 159045sec
     inet6 xxxx::xx:xx:xx:xx/xx scope link 
        valid_lft forever preferred_lft forever

* Get the IP address of your board with the [[Ifconfig|''ifconfig'']] Linux command line (a deprecated but well-known command):
 {{Board$}} ifconfig eth0
 eth0      Link encap:Ethernet  HWaddr xx:xx:xx:xx:xx:xx
           inet addr:{{highlight|xx.xx.xx.xx}}  Bcast:xx.xx.xx.xx  Mask:255.255.252.0
           inet6 addr: xxxx::xx:xx:xx:xx/xx Scope:Link
           UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
           RX packets:2619 errors:0 dropped:0 overruns:0 frame:0
           TX packets:1311 errors:0 dropped:0 overruns:0 carrier:0
           collisions:0 txqueuelen:1000
           RX bytes:353250 (344.9 KiB)  TX bytes:118305 (115.5 KiB)
           Interrupt:247

===Copying a file from your host PC to your board (and reciprocally)===
* [[How to transfer a file over network]] ({{highlight|recommended method}})

* [[How to transfer a file over serial console]]

===Miscellaneous commands===
{{Info|The outputs of the commands executed below are examples; the outputs that you obtain might differ.}}{{UpdateNeededForNewRelease|The outputs of the commands below shall be updated periodically, even if the information banner specifies that these outputs might not be up-to-date}}

====Printing distribution specific information====
 {{Board$}} cat /etc/os-release 
 ID=openstlinux-weston
 NAME="ST OpenSTLinux - Weston - (A Yocto Project Based Distro)"
 VERSION="4.0.1-openstlinux-22-06-15 (kirkstone)"
 VERSION_ID=4.0.1-openstlinux-22-06-15 
 PRETTY_NAME="ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 4.0.1-openstlinux-22-06-15 (kirkstone)"
 DISTRO_CODENAME="kirkstone"

Where:
{|
| ID || A lower-case string identifying the operating system
|-
| NAME || A string identifying the operating system
|-
| VERSION || A string identifying the operating system version, including a release code name
|-
| VERSION_ID || A lower case string identifying the operating system version
|-
| PRETTY_NAME || A full pretty name of the release
|}

====Printing system information====
 {{Board$}} uname -a
 Linux stm32mp1 5.15.24 #1 SMP PREEMPT Wed Feb 16 11:56:41 UTC 2022 armv7l armv7l armv7l GNU/Linux

Where:
{|
| Linux || Kernel name
|-
| stm32mp1 || Network node hostname
|-
| 5.15.24 || Kernel release
|-
| &#35;1 SMP PREEMPT Wed Feb 16 11:56:41 UTC 2022 || Kernel version
|-
| armv7l || Machine hardware name
|-
| GNU/Linux || Operating system 
|}

====Printing Linux kernel and GCC versions====
 {{Board$}} cat /proc/version
 Linux version 5.15.24 (oe-user@oe-host) (arm-ostl-linux-gnueabi-gcc (GCC) 11.2.0, GNU ld (GNU Binutils) 2.38.20220313) #1 SMP PREEMPT Wed Feb 16 11:56:41 UTC 2022

Where:
{|
| Linux || Kernel name
|-
| version 5.15.24 ||Kernel release
|-
| (xxxx@yyyy) || Person (xxxx) who compiled the kernel, and machine (yyyy) where it happened
|-
| (arm-ostl-linux-gnueabi-gcc (GCC) 11.2.0 ) || Version of the GCC compiler used to compile the kernel
|-
| &#35;1 SMP PREEMPT Wed Feb 16 11:56:41 UTC 2022 || Kernel version; type of kernel (SMP) and date and time of the kernel compilation
|}

====Printing the amount of disk space available on all mounted file systems====
 {{Board$}} df -h
 Filesystem      Size  Used Avail Use% Mounted on
 devtmpfs         116M     0  116M   0% /dev
 /dev/mmcblk0p10  684M  453M  184M  72% /
 tmpfs            195M  176K  195M   1% /dev/shm
 tmpfs             78M  8.8M   70M  12% /run
 tmpfs            4.0M     0  4.0M   0% /sys/fs/cgroup
 tmpfs            195M   16K  195M   1% /tmp
 /dev/mmcblk0p8    55M   39M   12M  77% /boot
 /dev/mmcblk0p9    14M  5.9M  6.8M  47% /vendor
 tmpfs            195M   96K  195M   1% /var/volatile
 /dev/mmcblk0p11   14G   45M   13G   1% /usr/local
 tmpfs             39M  4.0K   39M   1% /run/user/1000
 tmpfs             39M     0   39M   0% /run/user/0

Where:
{|
| Filesystem || Source of the mount point, usually a device
|-
| Size || Total size in human readable format (e.g. 1K, 234M, 2G)
|-
| Used ||Used size in human readable format
|-
| Available || Available size in human readable format
|-
| Use% ||Percentage of used size divided by the total size
|-
| Mounted on || Mount point
|}
<br>

Note: the user file system (userfs) and the boot file system (bootfs) are accessible respectively through the ''/usr/local'' mounting point, and the ''/boot'' mounting point (see [[STM32 MPU Flash mapping#Flash partitions|Flash partitions]] for a description of the file systems).
<noinclude>

{{NoIndex}}
[[Category:Sub-articles]]
{{PublicationRequestId | No TLMS yet | 2022-08-29 | TLMS to be entered by NSA24661 | 2022-09-26 |}}</noinclude>
Line 271: Line 271:
 
{{NoIndex}}
 
{{NoIndex}}
 
[[Category:Sub-articles]]
 
[[Category:Sub-articles]]
{{PublicationRequestId | No TLMS yet | 2022-08-29 | TLMS to be entered by NSA}}
+
{{PublicationRequestId | 24661 | 2022-09-26 |}}
 
</noinclude>
 
</noinclude>