Standard SDK directory structure

Stable: 23.02.2023 - 15:34 / Revision: 23.02.2023 - 15:33

I am here to prevent the first-page-empty bug!

This article describes the structure of the OpenSTLinux standard SDK installation directory:

SDK
├── environment-setup-<target>-<distro>-linux-gnueabi  Environment setup script
├── site-config-<target>-<distro>-linux-gnueabi        Configuration file for the target
├── sysroots                                           Root file systems
│   ├── <target>-<distro>-linux-gnueabi                Target sysroot (libraries, headers, and symbols)
│   │   ├── bin
│   │   ├── boot
│   │   ├── config
│   │   ├── dev
│   │   ├── etc
│   │   ├── home
│   │   ├── lib
│   │   ├── media
│   │   ├── mnt
│   │   ├── proc
│   │   ├── run
│   │   ├── sbin
│   │   ├── sys
│   │   ├── tmp
│   │   ├── usr
│   │   └── var
│   └── <host machine>-<distro>_sdk-linux              Native sysroot (libraries, headers, and symbols)
│       ├── bin
│       ├── environment-setup.d
│       ├── etc
│       ├── lib
│       ├── sbin
│       ├── usr
│       └── var
└── version-<target>-<distro>-linux-gnueabi            Version file for the target

Where:

<target> Target architecture for cross-toolchain; examples (non exhaustive list):
  • cortexa7hf-neon-vfpv4
<distro> Distribution; examples (non-exhaustive list):
  • openstlinux_weston
<host machine> Host machine on which the SDK is installed; examples (non-exhaustive list):
  • x86_64 (64-bit host machine)

The installed SDK consists of:

  • an environment setup script for the SDK
  • a configuration file for the target
  • a version file for the target
  • the root file systems (sysroots) needed to develop objects for the target system


IMPORTANT NOTICE – READ CAREFULLY
STMicroelectronics NV and its subsidiaries ("ST") reserve the right to make changes, corrections, enhancements, modifications, and improvements to ST products and/or to this document at any time without notice. Purchasers should obtain the latest relevant information on ST products before placing orders. ST products are sold pursuant to ST’s terms and conditions of sale in place at the time of order acknowledgment.

Purchasers are solely responsible for the choice, selection, and use of ST products and ST assumes no liability for application assistance or the design of purchasers’ products.

No license, express or implied, to any intellectual property right is granted by ST herein.

Resale of ST products with provisions different from the information set forth herein shall void any warranty granted by ST for such product.

ST and the ST logo are trademarks of ST. For additional information about ST trademarks, refer to www.st.com/trademarks. All other product or service names are the property of their respective owners.

Information in this document supersedes and replaces information previously supplied in any prior versions of this document.