- Last edited one year ago ago
How to play audio
Contents
1 Article purpose[edit]
This article explains how to play audio through the ALSA audio framework in Linux® OS context. The examples below, show how to play audio on the different audio hardware interfaces of the STM32MPU boards.
2 Audio playback overview[edit]
The ALSA framework exposes audio devices associated to the board audio hardware interfaces.
The application audio streams are routed by default through the PulseAudio sound server. PulseAudio exposes audio profiles which are mapped on the ALSA sound card audio devices. The PulseAudio server provides a command line interface which allows to list audio profiles and to select a profile, to play on a specific audio interface.
The audio playback examples in following sections are given for ALSA utilities. However, the audio playbacks can be launched by other applications, such as gstreamer multimedia framework.
3 Examples[edit]
3.1 Audio playback on headset output[edit]
3.1.1 Playback on ALSA device[edit]
Run audio playback on 'playback_codec' ALSA device:
aplay -D playback_codec /usr/share/sounds/alsa/Front_Left.wav
3.1.2 Playback via PulseAudio[edit]
- Configure Pulseaudio
Change the Pulseaudio active profile of the sound card, to 'analog-stereo' profile:
pacmd set-card-profile 0 output:analog-stereo+input:analog-stereo
- Run audio playback:
aplay /usr/share/sounds/alsa/Front_Left.wav
3.2 Audio playback on HDMI output[edit]
3.2.1 Playback on ALSA device[edit]
Run audio playback on 'playback_hdmi' ALSA device:
aplay -D playback_hdmi /usr/share/sounds/alsa/Front_Left.wav
3.2.2 Playback via PulseAudio[edit]
- Configure Pulseaudio
Change the Pulseaudio active profile of the sound card, to 'hdmi-stereo' profile:
pacmd set-card-profile 0 output:hdmi-stereo
- Run audio playback:
aplay /usr/share/sounds/alsa/Front_Left.wav
3.3 Audio playback on S/PDIF output[edit]
3.3.1 Set IEC958 status bits[edit]
Example: set IEC958 mode bit.
iecset -c STM32MP1EV -n device=0 pro on
3.3.2 Playback on ALSA device[edit]
Run audio playback on 'playback_spdif' ALSA device:
speaker-test -D playback_spdif -c 2 -F S32_LE -f 440 -t sine -l 1
3.3.3 Playback via PulseAudio[edit]
- Configure Pulseaudio
Change the sound card active profile, to S/PDIF 'iec958-stereo' profile.
pacmd set-card-profile 0 output:iec958-stereo
- Run audio playback:
speaker-test -c 2 -F S32_LE -f 440 -t sine -l 1