STM32MPU Embedded Software architecture overview

Stable: 14.02.2023 - 09:56 / Revision: 14.02.2023 - 09:55

I am here to prevent the first-page-empty bug!

Template:ToBeReviewedByProductMarketing Template:ArticleMainWriter Template:ArticleApprovedVersion


1 STM32MPU Embedded Software overview

The diagram below shows STM32MPU Embedded Software distribution main components:

  • The OpenSTLinux distribution, running on the Arm®Cortex®-A, including:
    • The OpenSTLinux BSP with:
      • The boot chain based on TF-A and U-Boot.
      • The OP-TEE secure OS running on the Arm®Cortex®-A in secure mode.
      • The Linux® kernel running on the Arm®Cortex®-A in non-secure mode.
    • The application frameworks are composed of middlewares relying on the BSP and providing API:
      • on the OP-TEE side to run Trusted Applications (TA) that allow to manipulate secrets (not visible from the Linux and STM32Cube MPU Package)
      • on the Linux side to run Applications that typically interact with the user via the display, the touchscreen, etc.
  • The STM32Cube MPU Package is running on the Arm®Cortex®-M: it is based on HAL drivers and middlewares, like other STM32 microcontrollers, completed with coprocessor management.

The figure below is clickable so that the user can directly jump to one of the sub-levels listed above.

STM32CubeMP1 architecture OP-TEE overview OP-TEE overview TF-A overview U-Boot overview STM32MP15 Linux kernel overview Boot chains overview Linux application frameworks overview OpenSTLinux BSP architecture overview OpenSTLinux architecture overview Category:Platform configuration Security overview
STM32MPU Embedded Software architecture overview...

Template:WarningImageMapOverlay
OpenSTLinux OE legend.png


2 Open Source Software (OSS) philosophy

The Open source software source code is released under a license in which the copyright holder grants users the rights to study, change and distribute the software to anyone and for any purpose[1].
STMicroelectronics maximizes the using of open source software and contributes to those communities. Notice that, due to the software review life cycle, it can take some time before getting all developments accepted in the communities, so STMicroelectronics can also temporarily provide some source code on github[2], until it is merged in the targeted repository.

3 References

IMPORTANT NOTICE – READ CAREFULLY
STMicroelectronics NV and its subsidiaries ("ST") reserve the right to make changes, corrections, enhancements, modifications, and improvements to ST products and/or to this document at any time without notice. Purchasers should obtain the latest relevant information on ST products before placing orders. ST products are sold pursuant to ST’s terms and conditions of sale in place at the time of order acknowledgment.

Purchasers are solely responsible for the choice, selection, and use of ST products and ST assumes no liability for application assistance or the design of purchasers’ products.

No license, express or implied, to any intellectual property right is granted by ST herein.

Resale of ST products with provisions different from the information set forth herein shall void any warranty granted by ST for such product.

ST and the ST logo are trademarks of ST. For additional information about ST trademarks, refer to www.st.com/trademarks. All other product or service names are the property of their respective owners.

Information in this document supersedes and replaces information previously supplied in any prior versions of this document.