SPDIFRX Linux driver
Stable: 12.07.2023 - 10:24 / Revision: 12.07.2023 - 10:23
Template:ArticleMainWriter
Template:ArticleApprovedVersion
Contents
1 Article purpose
This article introduces the SPDIFRX Linux® driver for the SPDIFRX internal peripheral.
2 Short Description
The SPDIFRX[1]Linux driver is an ASoC CPU DAI driver implemented in the Linux ALSA framework.
3 Configuration
3.1 Kernel Configuration
Activate the SPDIFRX[1]Linux driver in the kernel configuration using the Linux Menuconfig tool: Menuconfig or how to configure kernel
[*] Device Drivers [*] Sound card support [*] Advanced Linux Sound Architecture [*] ALSA for SoC audio support STMicroelectronics STM32 SOC audio support [*] STM32 S/PDIF receiver (SPDIFRX) support
3.2 Device tree
Refer to the SPDIFRX device tree configuration article when configuring the SPDIFRX Linux kernel driver.
4 How to use
The SAI driver is accessed from userland through an ALSA device. Refer to ALSA overview to see how to list and use ALSA devices.
5 How to debug
The debugfs and procfs file systems can be checked to get information about the SPDFIRX driver and the resources it uses. A none exhaustive list of these file system entries is provided below. Refer to ALSA overview to get more details about debugging tools.
- debugfs entries:
- asoc: refer to ALSA_overview#How_to_monitor
- clk: refer to Clock_overview#How_to_monitor_with_debugfs to get information on clocks.
- pinctrl: refer to Pinctrl_overview#How_to_monitor to get information on pins.
- regmap: allow to monitor SPDIFRX peripheral registers.
$ cat /sys/kernel/debug/regmap/xxx.audio-controller/registers
- procfs entries:
- asound: refer to ALSA_overview#How_to_debug
- interrupts: allow to check interrupts.
$ cat /proc/interrupts
6 Source code location
sound/soc/stm/stm32_spdifrx.c : implements the SPDIFRX driver.