OTG internal peripheral

Stable: 12.07.2023 - 15:49 / Revision: 12.07.2023 - 15:49

I am here to prevent the first-page-empty bug!


Template:ArticleMainWriter Template:ArticleApprovedVersion


1 Article purpose

The purpose of this article is to

  • briefly introduce the OTG peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how it can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain, when needed, how to configure the OTG peripheral.

2 Peripheral overview

The OTG peripheral is used to interconnect other systems with STM32 MPU devices, using USB standard.

2.1 Features

The OTG peripheral is a USB Dual-Role Device (DRD) controller that supports both device and host functions.
In Host mode, it supports high-speed (480 Mbit/s), full-speed (12 Mbit/s) and low-speed (1.5 Mbit/s).
In Peripheral mode, high-speed and full-speed are supported, not low-speed.
The OTG peripheral embeds a full-speed PHY and supports a UTMI interface connected to internal HS PHY.

The OTG peripheral is fully compliant with

  • On-The-Go and Embedded Host Supplement to the USB Revision 2.0 Specification[1], Revision 2.0, May 8, 2009
  • Universal Serial Bus Revision 2.0 Specification[2], Revision 2.0, April 27, 2000
  • USB 2.0 Link Power Management Addendum Engineering Change Notice to the USB 2.0 specification[3], July 16, 2007
  • USB 2.0 Transceiver Macrocell Interface (UTMI) Specification[4], Version 1.05, March 29, 2001
  • UTMI+ Specification[5], Revision 1.0, February 25, 2004

Refer to STM32MP15 reference manuals for the complete hardware feature list, and to the software components (introduced below) to know which features are supported.

2.2 Security support

The OTG peripheral is a non-secure peripheral.

3 Peripheral usage and associated software

3.1 Boot time

The OTG peripheral is used by ROM code, FSBL and SSBL in device mode (DFU) to support serial boot for flash programming with STM32CubeProgrammer.
The SSBL can use it in host mode (mass storage), for instance to boot on a kernel stored on a USB key, or after a kernel panic to perform the crash dump saving to the USB key.

3.2 Runtime

3.2.1 Overview

The OTG peripheral can be allocated to the Arm®Cortex®-A7 non-secure core to be used under Linux® with USB framework.

3.2.2 Software frameworks

Domain Peripheral Software frameworks Comment
Cortex-A7 S
(OP-TEE)
Cortex-A7 NS
(Linux)
Cortex-M4
(STM32Cube)
High speed interface OTG (USB OTG) Linux USB framework

3.2.3 Peripheral configuration

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration by itself can be performed via the STM32CubeMX tool for all internal peripherals. It can then be manually completed (especially for external peripherals) according to the information given in the corresponding software framework article.

For Linux kernel configuration, please refer to OTG device tree configuration.

3.2.4 Peripheral assignment

Internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

means that the peripheral can be assigned () to the given runtime context.
is used for system peripherals that cannot be unchecked because they are statically connected in the device.


Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7 S
(OP-TEE)
Cortex-A7 NS
(Linux)
Cortex-M4
(STM32Cube)
High speed interface OTG (USB OTG) OTG (USB OTG)

4 References

IMPORTANT NOTICE – READ CAREFULLY
STMicroelectronics NV and its subsidiaries ("ST") reserve the right to make changes, corrections, enhancements, modifications, and improvements to ST products and/or to this document at any time without notice. Purchasers should obtain the latest relevant information on ST products before placing orders. ST products are sold pursuant to ST’s terms and conditions of sale in place at the time of order acknowledgment.

Purchasers are solely responsible for the choice, selection, and use of ST products and ST assumes no liability for application assistance or the design of purchasers’ products.

No license, express or implied, to any intellectual property right is granted by ST herein.

Resale of ST products with provisions different from the information set forth herein shall void any warranty granted by ST for such product.

ST and the ST logo are trademarks of ST. For additional information about ST trademarks, refer to www.st.com/trademarks. All other product or service names are the property of their respective owners.

Information in this document supersedes and replaces information previously supplied in any prior versions of this document.