Install the SDK

Stable: 29.06.2023 - 14:47 / Revision: 29.06.2023 - 14:47

I am here to prevent the first-page-empty bug!

1 Overview

This stage explains how to install the SDK.
The SDK for OpenSTLinux distribution provides a stand-alone cross-development toolchain and libraries tailored to the contents of the specific image flashed in the board.

2 Host computer configuration

2.1 Install extra package

Additional Ubuntu packages must be installed to perform basic development tasks, basic cross-compilation (via Developer Package) or more complex cross-compilation such as OpenEmbedded does (via Distribution Package):

 sudo apt-get update
 sudo apt-get install gawk wget git diffstat unzip texinfo gcc-multilib  chrpath socat cpio python3 python3-pip python3-pexpect 
xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev pylint xterm bsdmainutils
 sudo apt-get install libssl-dev libgmp-dev libmpc-dev lz4 zstd
  • Packages needed for some "Developer Package" use cases:
 sudo apt-get install build-essential libncurses-dev libyaml-dev libssl-dev 
  • Package for repo (used to download the "Distribution Package" source code):
First set python3 as default:  sudo apt install python-is-python3

Then follow the installation instructions described in repo.
  • Useful tools:
 sudo apt-get install coreutils bsdmainutils sed curl bc lrzsz corkscrew cvs subversion mercurial nfs-common nfs-kernel-server libarchive-zip-perl dos2unix texi2html libxml2-utils


2.2 Additional configurations

  • Allow up to 16 partitions per mmc

By default, on Linux system, a maximum of 8 partitions are allowed on mmc. All Packages (Starter Package, ...) need more than 10 partitions for the storage device. In order to extend the number of partitions per device to 16, the following options must be added to modprobe:

 echo 'options mmc_block perdev_minors=16' > /tmp/mmc_block.conf
 sudo mv /tmp/mmc_block.conf /etc/modprobe.d/mmc_block.conf

3 Download the SDK

The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.

  • Download the [unknown revision /unknown revision Developer Package SDK] into the following directory: $HOME/STM32MPU_workspace/tmp
  • Uncompress the tarball file to get the SDK installation script
 cd $HOME/STM32MPU_workspace/tmp
 tar xvf unknown revision 

4 Run the SDK installation script

  • Create your STM32MP15 Developer Package SDK directory on your host computer
 mkdir -p $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Developer-Package/SDK
  • Change the permissions of the SDK installation script so that it is executable
 chmod +x unknown revision /unknown revision 
  • Execute the SDK installation script
 ./unknown revision /unknown revision  -d <working directory absolute path>/Developer-Package/SDK
  • A successful installation outputs the following log:
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 3.1-openstlinux-5.10-dunfell-mp1-21-03-31
========================================================================================================================
Enter target directory for SDK (default:  $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Developer-Package/SDK): 
You are about to install the SDK to "$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Developer-Package/SDK". Proceed [Y/n]? Y
Extracting SDK......................................................................................................................................................................................................................done
Setting it up...done
SDK has been successfully set up and is ready to be used.
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g.
 $ . /home/osboxes/MCD/DV3.0/Dev/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi

5 Starting up the SDK

Info white.png Information
The SDK environment setup script must be run once in each new working terminal in which you cross-compile
 cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Developer-Package 
 source SDK/unknown revision 

The following checks allow to ensure that the environment is correctly setup:

  • Check the target architecture
 echo $ARCH
arm
  • Check the toolchain binary prefix for the target tools
 echo $CROSS_COMPILE
arm-ostl-linux-gnueabi-

  • Check the C compiler version
 $CC --version
arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0  
Copyright (C) 2019 Free Software Foundation, Inc.
This is free software; see the source for copying conditions.  There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
  • Check that the SDK version is the expected one
 echo $OECORE_SDK_VERSION
3.1-unknown revision 

If any of these commands fails or does not return the expected result, please try to reinstall the SDK.


IMPORTANT NOTICE – READ CAREFULLY
STMicroelectronics NV and its subsidiaries ("ST") reserve the right to make changes, corrections, enhancements, modifications, and improvements to ST products and/or to this document at any time without notice. Purchasers should obtain the latest relevant information on ST products before placing orders. ST products are sold pursuant to ST’s terms and conditions of sale in place at the time of order acknowledgment.

Purchasers are solely responsible for the choice, selection, and use of ST products and ST assumes no liability for application assistance or the design of purchasers’ products.

No license, express or implied, to any intellectual property right is granted by ST herein.

Resale of ST products with provisions different from the information set forth herein shall void any warranty granted by ST for such product.

ST and the ST logo are trademarks of ST. For additional information about ST trademarks, refer to www.st.com/trademarks. All other product or service names are the property of their respective owners.

Information in this document supersedes and replaces information previously supplied in any prior versions of this document.