How to create your own machine

Stable: 25.02.2019 - 16:46 / Revision: 19.02.2019 - 16:54

I am here to prevent the first-page-empty bug!

Template:ArticleMainWriter Template:ArticleApprovedVersion


1 Introduction

For your own needs, you can add in the Yocto project a new machine reflecting your own board and your own features.
This article is reserved to Yocto experts or at least people who have already practiced with the Yocto environmment.

This section describes how to add and configure a machine that is similar to those that the OpenSTLinux Distribution Package already supports.
This customer machine is associated to STM32CubeMX tool which provides DeviceTree files per component (tf-a, u-boot and kernel).

We suppose here that all the material described below is done inside an existing STM32MP BSP layer 'addons'.
For reminder this addons layer is deployed here in our delivery : <path of OpenSTLinux distribution delivery>/meta-st/meta-st-stm32mp-addons/

2 Generate devicetree

The principle is that the user generates devicetree files from the STM32CubeMX tool.
With the STM32CubeMX tool, the user browses inside the OpenSTLinux distribution file system until “mx” folder located into STM32MP BSP layer addons : <path of OpenSTLinux distribution delivery>/meta-st/meta-st-stm32mp-addons/mx/

  • 3 sub-folders are created and populated with generated devicetree files :
    • <ProjectName>/kernel
    • <ProjectName>/u-boot
    • <ProjectName>/tf-a

Where <ProjectName> is the “STM32CubeMX user project name”

Each directory of <ProjectName> contains devicetree files associated to the component directory, here: kernel, u-boot and tf-a (Trusted Firmware-A).
Please refer to this page for more details on this tool and its usage :


3 Create a custom machine

Create a machine based on the one provided by ST and align some environment variables with the content of mx/<ProjectName> sub-folders

3.1 Create the new machine

  $> cd <path of OpenSTLinux distribution delivery>/meta-st/meta-st-stm32mp-addons/conf/machine
  $> cp stm32mp1-mx.conf stm32mp1-<ProjectName>.conf
  $> cd include
  $> cp stm32mp1-mx-config.inc stm32mp1-<ProjectName>-config.inc
  $> cp stm32mp1-mx-extlinux-config.inc stm32mp1-<ProjectName>-extlinux-config.inc

3.2 Edit the new machine file: stm32mp1-<ProjectName>.conf

Replace these 2 lines :

include conf/machine/include/stm32mp1-mx-config.inc
include conf/machine/include/stm32mp1-mx-extlinux-config.inc

By these ones :

include conf/machine/include/stm32mp1-<ProjectName>-config.inc
include conf/machine/include/stm32mp1-<ProjectName>-extlinux-config.inc

3.3 Edit the new machine config file: stm32mp1-<ProjectName>-config.inc

In this config file you can select :

* boot scheme (by default trusted is set)
* boot device  (by default sdcard is set)
* board (by default eval is set)
* name of CubeMX Board DeviceTree files (by default stm32mp157c-defaultmxconfig-mx is set)
* path of CubeMX Board DeviceTree files (by default STM32MP157C-EV1/Templates/DefaultMXConfig/DeviceTree/DefaultMXConfig is set)

To select one of each parameter you have just to comment and uncomment lines, and modify CUBEMX_DTB accordingly to the name of CubeMX Board DeviceTree files

4 Miscellaneous

4.1 MACHINEOVERRIDES regular expression

In each customer machine we retrieve this line:

MACHINEOVERRIDES .= ":stm32mpcommonmx"

A regular expression that resolves to one or more target machines with which a recipe is compatible.


The impact in the build environment is that recipes can now do things conditionally only on the builds for all mx specific machines: stm32mpcommonmx
It is very useful in some existing recipes to keep the compatibility for all stm32mp1-<ProjectName>.conf machines.
For instance use it like this (as it is done in the recipe <path of OpenSTLinux distribution delivery>/meta-st/meta-st-stm32mp-addons/recipes-bsp/alsa/alsa-state-stm32mp1.bbappend):

SRC_URI_append_stm32mpcommonmx

The append will be applied for all machines (all stm32mp1-<ProjectName>.conf) which include MACHINEOVERRIDES .= ":stm32mpcommonmx"

So it avoids to create an append file by customer machine.

4.2 STM32CubeMX class

A dedicated class is provided here :

<STM32MP BSP layer addons>/classes/cubemx-stm32mp.bbclass

The main goal of this class is to manage any change done by the customer in sub folders mx/<ProjectName>/...

So if a devicetree file is updated for one or more of components, this change will be taken into account automatically during the next compilation done in the Distribution Package.

5 Compile your image with the yocto build process

 $> cd <path of yocto delivery>
 (directory which contains meta-st, openembedded-core, meta-openembedded)
$> MACHINE=stm32mp1-<ProjectName> DISTRO=openstlinux-weston source meta-st/script/envsetup.sh Accept the term of EULA (if you agree with)
$> bitbake st-image-weston The generated images are available on build-openstlinuxweston-stm32mp1-<ProjectName>/tmp-glibc/deploy/images/stm32mp1-<ProjectName>
IMPORTANT NOTICE – READ CAREFULLY
STMicroelectronics NV and its subsidiaries ("ST") reserve the right to make changes, corrections, enhancements, modifications, and improvements to ST products and/or to this document at any time without notice. Purchasers should obtain the latest relevant information on ST products before placing orders. ST products are sold pursuant to ST’s terms and conditions of sale in place at the time of order acknowledgment.

Purchasers are solely responsible for the choice, selection, and use of ST products and ST assumes no liability for application assistance or the design of purchasers’ products.

No license, express or implied, to any intellectual property right is granted by ST herein.

Resale of ST products with provisions different from the information set forth herein shall void any warranty granted by ST for such product.

ST and the ST logo are trademarks of ST. For additional information about ST trademarks, refer to www.st.com/trademarks. All other product or service names are the property of their respective owners.

Information in this document supersedes and replaces information previously supplied in any prior versions of this document.