GIC internal peripheral

Stable: 15.02.2019 - 15:08 / Revision: 15.02.2019 - 15:07

I am here to prevent the first-page-empty bug!


Template:ArticleMainWriter Template:ArticleApprovedVersion



1 Article purpose

The purpose of this article is to

  • briefly introduce the GIC peripheral (generic interrupt controller) and its main features
  • indicate the level of security supported by this hardware block
  • explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain, when needed, how to configure the GIC peripheral.

2 Peripheral overview

The GIC peripheral is the Arm®Cortex®-A7 interrupt controller. It is consequently not accessible from the Arm®Cortex®-M4 core.

2.1 Features

Refer to STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to know which features are really implemented.

2.2 Security support

The GIC is a secure peripheral (under ETZPC control).

3 Peripheral usage and associated software

3.1 Boot time

The GIC is configured by the FSBL (see Boot chains overview), mainly to define the routing of each interrupt to the secure or non-secure context at runtime: this configuration is further described in STM32MP15 interrupts article.

3.2 Runtime

3.2.1 Overview

The GIC can be allocated:

  • to the Arm®Cortex®-A7 secure core to be used under OP-TEE with the GIC OP-TEE driver (or TF-A secure monitor if the OP-TEE is not present)
  • or to the Arm®Cortex®-A7 non-secure core to be used under Linux® with the interrupts framework

3.2.2 Software frameworks

Internal peripherals software table template

| Core/Interrupts
| GIC
| OP-TEE GIC driver
| Linux interrupt framework
| 
|
|-
|}

3.2.3 Peripheral configuration

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration by itself can be performed via the STM32CubeMX tool for all internal peripherals. It can then be manually completed (especially for external peripherals) according to the information given in the corresponding software framework article.

3.2.4 Peripheral assignment

Internal peripherals assignment table template

| rowspan="1" | Core/Interrupts
| rowspan="1" | GIC
| GIC
| 
| 
|
|
|-
|}
IMPORTANT NOTICE – READ CAREFULLY
STMicroelectronics NV and its subsidiaries ("ST") reserve the right to make changes, corrections, enhancements, modifications, and improvements to ST products and/or to this document at any time without notice. Purchasers should obtain the latest relevant information on ST products before placing orders. ST products are sold pursuant to ST’s terms and conditions of sale in place at the time of order acknowledgment.

Purchasers are solely responsible for the choice, selection, and use of ST products and ST assumes no liability for application assistance or the design of purchasers’ products.

No license, express or implied, to any intellectual property right is granted by ST herein.

Resale of ST products with provisions different from the information set forth herein shall void any warranty granted by ST for such product.

ST and the ST logo are trademarks of ST. For additional information about ST trademarks, refer to www.st.com/trademarks. All other product or service names are the property of their respective owners.

Information in this document supersedes and replaces information previously supplied in any prior versions of this document.