Ethtool

Stable: 11.02.2019 - 11:21 / Revision: 10.01.2019 - 09:56

I am here to prevent the first-page-empty bug!


Template:ArticleMainWriter

Template:ArticleApprovedVersion


1 Article purpose

This article provides the basic information needed to start using the Linux® command tool: ethtool [1].

2 Introduction

The following table provides a brief description of the tool, as well as its availability depending on the software packages:

Yes: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.

No: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.

Tool STM32MPU Embedded Software distribution STM32MPU Embedded Software distribution for Android™
Warning white.png Warning
STM32MPU Embedded Software distribution for Android™ is no more supported by ST. You can contact our ST partner, Witekio, who can help you to port and maintain it on STM32MP15 platform.
Name Category Purpose Starter Package Developer Package Distribution Package Starter Package Developer Package Distribution Package
ethtool Monitoring tools ethtool[1] allows to query or control network driver and hardware settings, in particular for wired Ethernet devices. Yes Yes Yes
Under construction.png Coming soon

3 Installing the trace and debug tool on your target board

3.1 Using the STM32MPU Embedded Software distribution

ethtool is installed by default and ready to be used with all STM32MPU Embedded Software Packages.

 which ethtool
/usr/sbin/ethtool

It is integrated in weston image distribution through the meta-st package: meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bb.

RDEPENDS_packagegroup-framework-tools-network-base = "\
   ethtool         \
   iproute2        \
   "

3.2 Using the STM32MPU Embedded Software distribution for Android™

Under construction.png Coming soon

4 Getting started

The ethernet links available on your board can be listed by using the IP Linux command line:

 ip link | grep eth
3: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP mode DEFAULT group default qlen 1000
   link/ether 00:80:e1:42:43:65 brd ff:ff:ff:ff:ff:ff
  • Get information about the eth0 network device:
 ethtool eth0
Settings for eth0:
	Supported ports: [ TP AUI BNC MII FIBRE ]
	Supported link modes:   10baseT/Half 10baseT/Full 
	                        100baseT/Half 100baseT/Full 
	                        1000baseT/Half 1000baseT/Full 
	Supported pause frame use: Symmetric Receive-only
	Supports auto-negotiation: Yes
	Advertised link modes:  10baseT/Half 10baseT/Full 
	                        100baseT/Half 100baseT/Full 
	                        1000baseT/Half 1000baseT/Full 
	Advertised pause frame use: No
	Advertised auto-negotiation: Yes
	Link partner advertised link modes:  10baseT/Half 10baseT/Full 
	                                     100baseT/Half 100baseT/Full 
	                                     1000baseT/Full 
	Link partner advertised pause frame use: Symmetric
	Link partner advertised auto-negotiation: Yes
	Speed: 1000Mb/s
	Duplex: Full
	Port: MII
	PHYAD: 0
	Transceiver: internal
	Auto-negotiation: on
	Supports Wake-on: ug
	Wake-on: d
	Current message level: 0x0000003f (63)
			       drv probe link timer ifdown ifup
	Link detected: yes
  • Display Ethernet driver settings for eth0
 ethtool -i eth0
driver: st_gmac
version: Jan_2016
firmware-version: 
expansion-rom-version: 
bus-info: 
supports-statistics: yes
supports-test: no
supports-eeprom-access: no
supports-register-dump: yes
supports-priv-flags: no
  • Display network statistics for eth0:
 ethtool -S eth0
NIC statistics:
     mmc_tx_octetcount_gb: 0
     mmc_tx_framecount_gb: 0
     mmc_tx_broadcastframe_g: 0
     mmc_tx_multicastframe_g: 0
     mmc_tx_64_octets_gb: 0
     mmc_tx_65_to_127_octets_gb: 0
     mmc_tx_128_to_255_octets_gb: 0
     mmc_tx_256_to_511_octets_gb: 0
     mmc_tx_512_to_1023_octets_gb: 0
     mmc_tx_1024_to_max_octets_gb: 0
     mmc_tx_unicast_gb: 0
     mmc_tx_multicast_gb: 0
     mmc_tx_broadcast_gb: 0
     mmc_tx_underflow_error: 0
     mmc_tx_singlecol_g: 0
     mmc_tx_multicol_g: 0
     mmc_tx_deferred: 0
     mmc_tx_latecol: 0
     mmc_tx_exesscol: 0
     mmc_tx_carrier_error: 0
     mmc_tx_octetcount_g: 0
     mmc_tx_framecount_g: 1809
     mmc_tx_excessdef: 0
     mmc_tx_pause_frame: 0
     mmc_tx_vlan_frame_g: 0
     mmc_rx_framecount_gb: 0
     mmc_rx_octetcount_gb: 0
     mmc_rx_octetcount_g: 0
     mmc_rx_broadcastframe_g: 0
     mmc_rx_multicastframe_g: 0
     mmc_rx_crc_error: 0
     mmc_rx_align_error: 0
     mmc_rx_run_error: 0
     mmc_rx_jabber_error: 0
     mmc_rx_undersize_g: 0
     mmc_rx_oversize_g: 0
     mmc_rx_64_octets_gb: 0
     mmc_rx_65_to_127_octets_gb: 0
     mmc_rx_128_to_255_octets_gb: 0
     mmc_rx_256_to_511_octets_gb: 0
     mmc_rx_512_to_1023_octets_gb: 0
     mmc_rx_1024_to_max_octets_gb: 0
     mmc_rx_unicast_g: 1514
     mmc_rx_length_error: 0
     mmc_rx_autofrangetype: 0
     mmc_rx_pause_frames: 0
     mmc_rx_fifo_overflow: 0
     mmc_rx_vlan_frames_gb: 0
     mmc_rx_watchdog_error: 0
     mmc_rx_ipc_intr_mask: 0
     mmc_rx_ipc_intr: 0
     mmc_rx_ipv4_gd: 0
     mmc_rx_ipv4_hderr: 0
     mmc_rx_ipv4_nopay: 0
     mmc_rx_ipv4_frag: 0
     mmc_rx_ipv4_udsbl: 0
     mmc_rx_ipv4_gd_octets: 0
     mmc_rx_ipv4_hderr_octets: 0
     mmc_rx_ipv4_nopay_octets: 0
     mmc_rx_ipv4_frag_octets: 0
     mmc_rx_ipv4_udsbl_octets: 0
     mmc_rx_ipv6_gd_octets: 0
     mmc_rx_ipv6_hderr_octets: 0
     mmc_rx_ipv6_nopay_octets: 0
     mmc_rx_ipv6_gd: 0
     mmc_rx_ipv6_hderr: 0
     mmc_rx_ipv6_nopay: 0
     mmc_rx_udp_gd: 0
     mmc_rx_udp_err: 0
     mmc_rx_tcp_gd: 0
     mmc_rx_tcp_err: 0
     mmc_rx_icmp_gd: 0
     mmc_rx_icmp_err: 0
     mmc_rx_udp_gd_octets: 0
     mmc_rx_udp_err_octets: 0
     mmc_rx_tcp_gd_octets: 0
     mmc_rx_tcp_err_octets: 0
     mmc_rx_icmp_gd_octets: 0
     mmc_rx_icmp_err_octets: 0
     tx_underflow: 0
     tx_carrier: 0
     tx_losscarrier: 0
     vlan_tag: 0
     tx_deferred: 0
     tx_vlan: 0
     tx_jabber: 0
     tx_frame_flushed: 0
     tx_payload_error: 0
     tx_ip_header_error: 0
     rx_desc: 0
     sa_filter_fail: 0
     overflow_error: 0
     ipc_csum_error: 0
     rx_collision: 0
     rx_crc_errors: 0
     dribbling_bit: 0
     rx_length: 0
     rx_mii: 0
     rx_multicast: 0
     rx_gmac_overflow: 0
     rx_watchdog: 0
     da_rx_filter_fail: 0
     sa_rx_filter_fail: 0
     rx_missed_cntr: 0
     rx_overflow_cntr: 0
     rx_vlan: 0
     tx_undeflow_irq: 0
     tx_process_stopped_irq: 0
     tx_jabber_irq: 0
     rx_overflow_irq: 0
     rx_buf_unav_irq: 0
     rx_process_stopped_irq: 0
     rx_watchdog_irq: 0
     tx_early_irq: 0
     fatal_bus_error_irq: 0
     rx_early_irq: 0
     threshold: 1
     tx_pkt_n: 1809
     rx_pkt_n: 12682
     normal_irq_n: 11110
     rx_normal_irq_n: 11082
     napi_poll: 11118
     tx_normal_irq_n: 28
     tx_clean: 11641
     tx_set_ic_bit: 28
     irq_receive_pmt_irq_n: 0
     mmc_tx_irq_n: 0
     mmc_rx_irq_n: 0
     mmc_rx_csum_offload_irq_n: 0
     irq_tx_path_in_lpi_mode_n: 0
     irq_tx_path_exit_lpi_mode_n: 0
     irq_rx_path_in_lpi_mode_n: 0
     irq_rx_path_exit_lpi_mode_n: 0
     phy_eee_wakeup_error_n: 0
     ip_hdr_err: 0
     ip_payload_err: 0
     ip_csum_bypassed: 544
     ipv4_pkt_rcvd: 9189
     ipv6_pkt_rcvd: 1948
     no_ptp_rx_msg_type_ext: 12682
     ptp_rx_msg_type_sync: 0
     ptp_rx_msg_type_follow_up: 0
     ptp_rx_msg_type_delay_req: 0
     ptp_rx_msg_type_delay_resp: 0
     ptp_rx_msg_type_pdelay_req: 0
     ptp_rx_msg_type_pdelay_resp: 0
     ptp_rx_msg_type_pdelay_follow_up: 0
     ptp_rx_msg_type_announce: 0
     ptp_rx_msg_type_management: 0
     ptp_rx_msg_pkt_reserved_type: 0
     ptp_frame_type: 0
     ptp_ver: 0
     timestamp_dropped: 0
     av_pkt_rcvd: 0
     av_tagged_pkt_rcvd: 0
     vlan_tag_priority_val: 0
     l3_filter_match: 0
     l4_filter_match: 0
     l3_l4_filter_no_match: 0
     irq_pcs_ane_n: 0
     irq_pcs_link_n: 0
     irq_rgmii_n: 1
     mtl_tx_status_fifo_full: 0
     mtl_tx_fifo_not_empty: 0
     mmtl_fifo_ctrl: 0
     mtl_tx_fifo_read_ctrl_write: 0
     mtl_tx_fifo_read_ctrl_wait: 0
     mtl_tx_fifo_read_ctrl_read: 0
     mtl_tx_fifo_read_ctrl_idle: 0
     mac_tx_in_pause: 0
     mac_tx_frame_ctrl_xfer: 0
     mac_tx_frame_ctrl_idle: 0
     mac_tx_frame_ctrl_wait: 0
     mac_tx_frame_ctrl_pause: 0
     mac_gmii_tx_proto_engine: 0
     mtl_rx_fifo_fill_level_full: 0
     mtl_rx_fifo_fill_above_thresh: 0
     mtl_rx_fifo_fill_below_thresh: 0
     mtl_rx_fifo_fill_level_empty: 0
     mtl_rx_fifo_read_ctrl_flush: 0
     mtl_rx_fifo_read_ctrl_read_data: 0
     mtl_rx_fifo_read_ctrl_status: 0
     mtl_rx_fifo_read_ctrl_idle: 0
     mtl_rx_fifo_ctrl_active: 0
     mac_rx_frame_ctrl_fifo: 0
     mac_gmii_rx_proto_engine: 0
     tx_tso_frames: 0
     tx_tso_nfrags: 0

5 To go further

Lots of documentation exists on Internet about ethtool.

Refer to ethtool man page[1] for more details on command options.

6 References


  • Useful external links
Document link Document Type Description
ethtool Standard Wikipedia article
ethtool-command User guide thegeekstuff web page
IMPORTANT NOTICE – READ CAREFULLY
STMicroelectronics NV and its subsidiaries ("ST") reserve the right to make changes, corrections, enhancements, modifications, and improvements to ST products and/or to this document at any time without notice. Purchasers should obtain the latest relevant information on ST products before placing orders. ST products are sold pursuant to ST’s terms and conditions of sale in place at the time of order acknowledgment.

Purchasers are solely responsible for the choice, selection, and use of ST products and ST assumes no liability for application assistance or the design of purchasers’ products.

No license, express or implied, to any intellectual property right is granted by ST herein.

Resale of ST products with provisions different from the information set forth herein shall void any warranty granted by ST for such product.

ST and the ST logo are trademarks of ST. For additional information about ST trademarks, refer to www.st.com/trademarks. All other product or service names are the property of their respective owners.

Information in this document supersedes and replaces information previously supplied in any prior versions of this document.