CEC overview

Stable: 04.11.2022 - 09:46 / Revision: 04.11.2022 - 09:45

I am here to prevent the first-page-empty bug!

CEC (Consumer Electronics Control) provides enhanced functions to control devices connected through HDMI.

As an example, it allows the control of a recorder through TV remote control.

The CEC protocol is defined in the HDMI specification. This article gives information about the Linux®CEC framework.

1 Purpose

The purpose of this article is to introduce the CEC framework:

  • General information
  • Main components/stakeholders
  • How to use the CEC framework
  • Use cases

CEC is an HDMI feature designed to command and control devices connected through HDMI by using only one remote control. As an example, the remote control of a television set can be used to control a set-top box and a DVD player. Up to 15 devices can be controlled. CEC also allows individual CEC-enabled devices to command and control each other without user intervention.[1]

2 CEC overview

CECOverview.png


2.1 Description of the main components

From user space to hardware

  • CEC tools (User space)

This component contains a set of useful tools to configure CEC features. It is hosted in v4l-utils [2].

  • CEC core (Kernel space)

CEC core is the standard Linux kernel CEC framework. It manages the CEC protocol.

  • stm32-cec (Kernel space)

This is the ST CEC Linux driver that handles the CEC hardware block.

  • CEC (Hardware)

This is ST microprocessor CEC hardware block.

2.2 Description of the APIs

The CEC kernel API is documented in the 'CEC kernel support' section of the Linux Kernel documentation[3].

The CEC Userland API is documented in the 'Consumer Electronics Control API of v4l-utils documentation[4].

3 Configuration

By default, CEC is deactivated in ST deliveries. However, you can use Linux Menuconfig tool if a specific configuration is required: Menuconfig or how to configure kernel then select:

[*] Device Drivers --->
    [*] Multimedia support --->
        [*] HDMI-CEC support
        [*] CEC platform devices --->
            [*] STMicroelectronics STM32 HDMI-CEC driver

4 How to use CEC framework

cec-ctl and cec-compliance tools are hosted in CEC tools use space.

To register a CEC device on CEC bus, set its type and physical address:

{{Board$}} cec-ctl --tuner -p 1.0.0.0
Driver Info:
        Driver Name                : stm32-cec
        Adapter Name               : stm32-cec
        Capabilities               : 0x000000ef
                Physical Address
                Logical Addresses
                Transmit
                Passthrough
                Monitor All
        Driver version             : 4.19.9
        Available Logical Addresses: 4
        Physical Address           : 1.0.0.0
        Logical Address Mask       : 0x0008
        CEC Version                : 2.0
        Vendor ID                  : 0x000c03 (HDMI)
        OSD Name                   : 'Tuner'
        Logical Addresses          : 1 (Allow RC Passthrough)

          Logical Address          : 3 (Tuner 1)
            Primary Device Type    : Tuner
            Logical Address Type   : Tuner
            All Device Types       : Tuner
            RC TV Profile          : None
            Device Features        :
                None

To debug and monitor CEC messages on bus, use the following command line:

{{Board$}} cec-ctl -M
Driver Info:
        Driver Name                : stm32-cec
        Adapter Name               : stm32-cec
        Capabilities               : 0x000000ef
                Physical Address
                Logical Addresses
                Transmit
                Passthrough
                Monitor All
        Driver version             : 4.19.9
        Available Logical Addresses: 4
        Physical Address           : 1.0.0.0
        Logical Address Mask       : 0x0008
        CEC Version                : 2.0
        Vendor ID                  : 0x000c03 (HDMI)
        OSD Name                   : 'Tuner'
        Logical Addresses          : 1 (Allow RC Passthrough)

          Logical Address          : 3 (Tuner 1)
            Primary Device Type    : Tuner
            Logical Address Type   : Tuner
            All Device Types       : Tuner
            RC TV Profile          : None
            Device Features        :
                None



Initial Event: State Change: PA: 1.0.0.0, LA mask: 0x000

Run CEC compliance to check CEC bus typology:

{{Board$}} cec-compliance -A
cec-compliance SHA                 : not available

Driver Info:
        Driver Name                : stm32-cec
        Adapter Name               : stm32-cec
        Capabilities               : 0x000000ef
                Physical Address
                Logical Addresses
                Transmit
                Passthrough
                Monitor All
        Driver version             : 4.19.9
        Available Logical Addresses: 4
        Physical Address           : 1.0.0.0
        Logical Address Mask       : 0x0008
        CEC Version                : 2.0
        Vendor ID                  : 0x000c03
        Logical Addresses          : 1 (Allow RC Passthrough)

          Logical Address          : 3
            Primary Device Type    : Tuner
            Logical Address Type   : Tuner
            All Device Types       : Tuner
            RC TV Profile          : None
            Device Features        :
                None

Compliance test for device /dev/cec0:

    The test results mean the following:
        OK                  Supported correctly by the device.
        OK (Not Supported)  Not supported and not mandatory for the device.
        OK (Presumed)       Presumably supported.  Manually check to confirm.
        OK (Unexpected)     Supported correctly but is not expected to be supported for this device.
        OK (Refused)        Supported by the device, but was refused.
        FAIL                Failed and was expected to be supported by this device.

Find remote devices:
        Polling: OK

CEC API:
        CEC_ADAP_G_CAPS: OK
        CEC_DQEVENT: OK
        CEC_ADAP_G/S_PHYS_ADDR: OK
        CEC_ADAP_G/S_LOG_ADDRS: OK
        CEC_TRANSMIT: OK
        CEC_RECEIVE: OK
        CEC_TRANSMIT/RECEIVE (non-blocking): OK (Presumed)
        CEC_G/S_MODE: OK
        CEC_EVENT_LOST_MSGS: OK

Network topology:
        System Information for device 0 (TV) from device 3 (Tuner 1):
                CEC Version                : 1.4
                Physical Address           : 0.0.0.0
                Primary Device Type        : TV
                Vendor ID                  : 0x00903e
                OSD Name                   : 'TV'
                Menu Language              : fre
                Power Status               : On

Total: 10, Succeeded: 10, Failed: 0, Warnings: 0

Send a string to OSD:

{{Board$}} cec-ctl --set-osd-string=disp-ctl=0x00,osd="hello" --to tv
Driver Info:
        Driver Name                : stm32-cec
        Adapter Name               : stm32-cec
        Capabilities               : 0x000000ef
                Physical Address
                Logical Addresses
                Transmit
                Passthrough
                Monitor All
        Driver version             : 4.19.9
        Available Logical Addresses: 4
        Physical Address           : 1.0.0.0
        Logical Address Mask       : 0x0008
        CEC Version                : 2.0
        Vendor ID                  : 0x000c03 (HDMI)
        OSD Name                   : 'Tuner'
        Logical Addresses          : 1 (Allow RC Passthrough)

          Logical Address          : 3 (Tuner 1)
            Primary Device Type    : Tuner
            Logical Address Type   : Tuner
            All Device Types       : Tuner
            RC TV Profile          : None
            Device Features        :
                None


Transmit from Tuner 1 to TV (3 to 0):
CEC_MSG_SET_OSD_STRING (0x64):
        disp-ctl: default (0x00)
        osd: hello
        Sequence: 347 Tx Timestamp: 2626.350s

Get topology:

{{Board$}} cec-ctl -S
Driver Info:
        Driver Name                : stm32-cec
        Adapter Name               : stm32-cec
        Capabilities               : 0x000000ef
                Physical Address
                Logical Addresses
                Transmit
                Passthrough
                Monitor All
        Driver version             : 4.19.9
        Available Logical Addresses: 4
        Physical Address           : 1.0.0.0
        Logical Address Mask       : 0x0008
        CEC Version                : 2.0
        Vendor ID                  : 0x000c03 (HDMI)
        OSD Name                   : 'Tuner'
        Logical Addresses          : 1 (Allow RC Passthrough)

          Logical Address          : 3 (Tuner 1)
            Primary Device Type    : Tuner
            Logical Address Type   : Tuner
            All Device Types       : Tuner
            RC TV Profile          : None
            Device Features        :
                None

        System Information for device 0 (TV) from device 3 (Tuner 1):
                CEC Version                : 1.4
                Physical Address           : 0.0.0.0
                Primary Device Type        : TV
                Vendor ID                  : 0x00903e (Philips)
                OSD Name                   : TV
                Menu Language              : fre
                Power Status               : On

        Topology:

        0.0.0.0: TV
            1.0.0.0: Tuner 1

Send a standby message to a tv:

{{Board$}} cec-ctl --standby --to tv
Driver Info:
        Driver Name                : stm32-cec
        Adapter Name               : stm32-cec
        Capabilities               : 0x000000ef
                Physical Address
                Logical Addresses
                Transmit
                Passthrough
                Monitor All
        Driver version             : 4.19.9
        Available Logical Addresses: 4
        Physical Address           : 1.0.0.0
        Logical Address Mask       : 0x0008
        CEC Version                : 2.0
        Vendor ID                  : 0x000c03 (HDMI)
        OSD Name                   : 'Tuner'
        Logical Addresses          : 1 (Allow RC Passthrough)

          Logical Address          : 3 (Tuner 1)
            Primary Device Type    : Tuner
            Logical Address Type   : Tuner
            All Device Types       : Tuner
            RC TV Profile          : None
            Device Features        :
                None


Transmit from Tuner 1 to TV (3 to 0):
CEC_MSG_STANDBY (0x36)
        Sequence: 371 Tx Timestamp: 2747.236s

5 Use cases

Appplications must be added/developped in userland to support all the use cases related to CEC (eg recorder controled by TV remote control) .


6 Generic source code location

7 References




IMPORTANT NOTICE – READ CAREFULLY
STMicroelectronics NV and its subsidiaries ("ST") reserve the right to make changes, corrections, enhancements, modifications, and improvements to ST products and/or to this document at any time without notice. Purchasers should obtain the latest relevant information on ST products before placing orders. ST products are sold pursuant to ST’s terms and conditions of sale in place at the time of order acknowledgment.

Purchasers are solely responsible for the choice, selection, and use of ST products and ST assumes no liability for application assistance or the design of purchasers’ products.

No license, express or implied, to any intellectual property right is granted by ST herein.

Resale of ST products with provisions different from the information set forth herein shall void any warranty granted by ST for such product.

ST and the ST logo are trademarks of ST. For additional information about ST trademarks, refer to www.st.com/trademarks. All other product or service names are the property of their respective owners.

Information in this document supersedes and replaces information previously supplied in any prior versions of this document.